Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Measuring low resistances with Arduino
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 340 subscribers
  • Views 3843 views
  • Users 0 members are here
  • resistance
  • ohms
  • resistor
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Measuring low resistances with Arduino

e14 Contributor
e14 Contributor over 10 years ago

Hi,

 

I want to measure a resistance of about 0.4-1.6 ohms with an Arduino. I'm guessing this can't be done by a simple voltage divider because of the low resistances.

 

How could I achieve this? The measurement doesn't have to be very accurate. The question is pretty much about "is it less than or more than 1 ohm?".

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom +1
    Haven't tried anything in circuit yet. The only thing that came to mind was a voltage divider circuit, but with a bit of googling I came to the conclusion that the Arduino doesn't have enough resolution…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The reason I ask is that in the following circuit, the resistor in the middle is the resistance you are measuring from whatever source it may be. The other 2 allow us to create potential dividers with 2 seperate outputs. The output between the middle resistor and the lower resistor can be seen as a virtual ground that we can reference as a ground. The output between the middle resistor and the top resistor can be seen as a potential difference.

     

    If we measure the voltage between this new ground reference and the potential difference that we created, it should change whenever the resistance in the center changes, in this configuration the potential between those two points becomes 0.13V at 0.4ohm and 0.48V at 1.6ohm, a very much increased range and easier to measure.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The reason I ask is that in the following circuit, the resistor in the middle is the resistance you are measuring from whatever source it may be. The other 2 allow us to create potential dividers with 2 seperate outputs. The output between the middle resistor and the lower resistor can be seen as a virtual ground that we can reference as a ground. The output between the middle resistor and the top resistor can be seen as a potential difference.

     

    If we measure the voltage between this new ground reference and the potential difference that we created, it should change whenever the resistance in the center changes, in this configuration the potential between those two points becomes 0.13V at 0.4ohm and 0.48V at 1.6ohm, a very much increased range and easier to measure.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer