Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum I am looking for substitute for a 9564gm mosfet.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 339 subscribers
  • Views 1113 views
  • Users 0 members are here
  • mosfet
  • p-channel
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

I am looking for substitute for a 9564gm mosfet.

e14 Contributor
e14 Contributor over 10 years ago

My question is in the title.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +2
    Check the datasheet for Fairchild FDS4685 to see if it is close enough. Doug
Parents
  • dougw
    0 dougw over 10 years ago

    Check the datasheet for Fairchild  FDS4685 to see if it is close enough.

    Doug

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dougw

    Hello.

     

    I have an older chassis that rides on a trailer so it goes through shock and vibration. It only has one EM relay that activates when 120VAC is applied. It is a DPDT. The contacts only select 5VDC or Gnd as sense lines into a computer interface so current is not a big issue.

     

    Current relay is a plugin Potter & Brumfield KRP11AG120

     

    So, I'm looking to replace this relay with a SSR. 120VAC and DPDT for the two sense lines.

     

    Can you help me select a replacement? I'm sure back when this was designed they only used the EM relay because the used it to power up the DC supplies from the 120VAC main input.

     

    Thanks a lot.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dougw

    Hello.

     

    I have an older chassis that rides on a trailer so it goes through shock and vibration. It only has one EM relay that activates when 120VAC is applied. It is a DPDT. The contacts only select 5VDC or Gnd as sense lines into a computer interface so current is not a big issue.

     

    Current relay is a plugin Potter & Brumfield KRP11AG120

     

    So, I'm looking to replace this relay with a SSR. 120VAC and DPDT for the two sense lines.

     

    Can you help me select a replacement? I'm sure back when this was designed they only used the EM relay because the used it to power up the DC supplies from the 120VAC main input.

     

    Thanks a lot.

     

    Mike