Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Voltage regulator questions - capacitor on the input, difference between different regulators
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 314 subscribers
  • Views 3148 views
  • Users 0 members are here
  • voltage_regulation
  • voltage regulator
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Voltage regulator questions - capacitor on the input, difference between different regulators

sawik123
sawik123 over 9 years ago

Hello everyone,

 

I have some questions about voltage regulators (it's the first time I'm dealing with them, so the question are *really* basic - but I wasn't able to find answers anywhere, so I've figured I'll ask).

 

I have a 6 AA battery pack that I want to get 5 volts out of. First I got this voltage regulator and it seems to be working: https://www.adafruit.com/products/2164

However, it's dropdown can be as high as 2.5V, meaning that once the batteries go below 1.25 V each (which as far as I know is not the end of their lifetime) it may stop working (if I understand correctly. Or will this one do fine?).

 

Anyway, I've decided to get a regulator with a lower dropdown. I got these two (I expect the output current to be around 1A, so I got ones that support >= 1.5A just in case)

MIC29150-5.0WT - MICREL SEMICONDUCTOR - LDO VOLTAGE REGULATOR, 5V, 1.5A, TO-220 | Newark element14

MIC29300-5.0WT - MICREL SEMICONDUCTOR - Fixed LDO Voltage Regulator, 2.5V to 26V, 370mV Dropout, 5Vout, 3Aout, TO-220-3 …

 

Now basically my questions are:

  1. what capacitor should I use on the input? The spec doesn't really specify that. It only marks it as "C In". Does the value of that really matter? Will 10uF work fine (so I'd have 10uF on both input & output)?
  2. just out of curiosity - what really is the difference between them? Seems like the second one supports higher current and has slightly higher dropdown. Is that really the only thing? Will they pretty much operate the same, or will the second one like get more warm or something? Basically what I'm trying ot ask is - why would anyone want to use the first one over the second one?

 

Thanks,

Tom

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +2 suggested
    Hi Tom, The spec does specify that you may need a 100nF cap on the input (see page 20), you can additionally add the 10uF if you find you need it (it depends on what the impedance of your source is; there…
  • shabaz
    shabaz over 9 years ago in reply to sawik123 +2 verified
    Hi Tom, The 100nF and 10uF are used together, the reason is that they perform differently due to the material used in their construction (ceramic vs electrolytic). Both are advised. Figure 1 in this PDF…
  • jw0752
    jw0752 over 9 years ago +2 suggested
    Here is a link to Recom's DC to DC Book of Knowledge just in case you want more information on using switchers for converting voltages and some other really neat things. http://www.recom-power.com/de/americas…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Tom,

     

    The spec does specify that you may need a 100nF cap on the input (see page 20), you can additionally add the 10uF if you find you need it (it depends on what the impedance of your source is; there is no harm in adding a small amount of capacitance such as 10uF and the 100nF. To know why you're best picking up a book, because there is some theory including Ohm's Law and reactance that would need to be covered to do it justice - see here  I Want to Do Electronics!  Where do I start?

    But in summary you can use 10uF on the input (and 100nF) and 10uF on the output with that particular device because that is what page 20 text and the diagram on page 21 show. If they start mentioning ESR and capacitor type then that is important too.

     

    Regarding your second question, the 3A part is a similar part in the same family, rated for higher current. It may cost slightly more.

    As for if it will get hot - this is all down to the Power equation and Ohm's Law. You'll find that the amount of power dissipated as heat depends on your source voltage (e.g. 9V), and the output voltage (e.g. 5V) and the current through the voltage regulator and current through your load. You can calculate the power being dissipated as heat using Ohm's Law and the Power Equation, i.e. V=IR and P=IV.

    If your circuit is consuming 1A then the power dissipated by the voltage regulator as heat is approximately (first level approximation):

    V=9-5 = 4

    P=IV = 1*4 = 4W

    So your regulator would dissipate 4W and would be very hot and would need a heat sink. That answer is the same for both of the regulators.

    I strongly recommend you checking out that link, because it will help with these types of questions.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sawik123
    0 sawik123 over 9 years ago in reply to shabaz

    Thanks! That's very helpful. Yeah I guess I'll have to pick up some book...

    Until then, just to make sure - if I need a 100nF capacitor on the input, and you're saying I can add 10uF as well, I should be able to just drop the smaller one and just go with 10uF only? That should be ok, right?

    And in terms of heat - yeah, I'm planning to add the heat sink and some holes in the case for my thing to allow air circulation and stuff. Hopefully it won't melt image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to sawik123

    Hi Tom,

     

    The 100nF and 10uF are used together, the reason is that they perform differently due to the material used in their construction (ceramic vs electrolytic). Both are advised. Figure 1 in this PDF highlights the difference http://rohmfs.rohm.com/en/products/databook/applinote/ic/power/switching_regulator/cera_cap_appli-e.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago in reply to sawik123

    Hi Tom,

     

    The 100nF and 10uF are used together, the reason is that they perform differently due to the material used in their construction (ceramic vs electrolytic). Both are advised. Figure 1 in this PDF highlights the difference http://rohmfs.rohm.com/en/products/databook/applinote/ic/power/switching_regulator/cera_cap_appli-e.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer