Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Supercapacitor Balancing Questions
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 338 subscribers
  • Views 2659 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Supercapacitor Balancing Questions

e14 Contributor
e14 Contributor over 10 years ago

Hello,

     I have been doing some research for a couple months now on how to best balance supercapacitors in series. Now I'm just a hobbyist with only a college physics class and what I've read in my free time for an electronics background so I'm pretty limited. This in NOT a homework problem, Yay!

     The attached circuit is what I came up with for balancing. It’s basically an active Zener shunt regulator across each bank of capacitors (all 2.5V 630F parallel and series for 5V 630F total). The hope is that if the capacitors reach 2.5V (or a little less just to be safe) the Zener diodes would start conducting, opening the NPN transistors, and shunt power to the capacitors with the lower voltage or stop charging them altogether. It will be powered via USB (5V, 2.1A) and will power USB up to 1A so I think the components will have to be pretty beefy.

image

 

     Ok for D1 I have a T6A100L 1kV 6A rectifier diode (probably overkill but it’s what I had) in series with a 18Ω, 5W resistor (R1) to limit current draw to the USB supply. For the bipolar NPN transistors Q1 and Q2, I’m thinking of using BUJ403A,127 transistors (550V, 6A, 100W) attached to heat sinks. Now for the problem(s). If I am to expect a 0.7V drop across the transistors, should I use Zener diodes with a Zener Voltage of 1.8V or 3.2V if I’m looking to limit the voltage to 2.5V. I’m also wondering if I need resistors at R2 and R3 to drop the voltage by 2.5V to make it safe for the capacitors in the other bank and pull current away from Zener diodes. If so, how would I go about determining the necessary values of R2 and R3? I included current limiting resistors R4 and R5 in series with each of the Zener diodes, but I don’t know if these are necessary or what value they should be to get the current to below 100mA. If resistors R4 and R5 are included would that change what Zener voltage I would need to use?

     I also thought about putting all of the supercaps in parallel and using a buck converter to step the voltage from 5V to around 2.4V and ditch the balancing circuitry. The problem there is that the boosting the voltage back up to 5V. I’m using an Adafruit PowerBoost 1000 Basic to provide USB out but it only is operable down to 1.8V leaving me with only 3793J of useable energy instead of 6855J with the proposed setup. As this is meant for a mobile application that’s not a great option. I also looked at using the “ALD810024 Supercapacitor Auto Balancing (SAB) MOSFET” in a parallel configuration across the capacitors. However, this system is limited to around 80mA of current through it which seems insufficient to effectively drain these supercapacitors. Also it is in a surface mount SOIC-16 Package which even with a through hole adapter would stretch my soldering abilities. I currently have 20kΩ worth of resistors in parallel with the capacitor sets, however this doesn’t balance them very well and runs them down within a few days. I also looked at putting 3 rectifier diodes in series across the terminals of the capacitors; however, this is also limited in how much current can pass through it and I don’t know if it would be sufficient since I’m pushing 10.5W into these caps with the USB charger. Hopefully I covered everything. If you want to shoot some equations my way it would be much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • bnebeker
    bnebeker over 7 years ago +1 suggested
    This circuit has several issues and you have made some assumptions that are leading you in the wrong direction. The first issue is that balancing capacitors is not about switching large currents. The 80…
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I have just seen your question and I hope is not too late to answer.

    I think your circuit could work if you change the position of the resistors R2 and R3, placing them connected to the collector, instead of the emitter, of the transistors Q1 and Q2. Where these resistors are now they will increase the voltage limit that you are trying to get by the voltage drop in them. With the change that I am proposing I think that you get your intended voltage limiting function at a voltage that is equal to the zener voltage plus about 0.,6V for the base emitter drop.

    I have also been looking recently for balancing options. Your circuit with the proposed modification is, I think, a good one. With a 2.0V zener I could get a 2.6V voltage limit. The only difficulty that I see is that the required zener voltage, 2.0v, doesn't seem very common and it may be expensive or difficult to get. If you used instead an OA (Operational Amplifier) you could easily use a common voltage zener and adjust the exact voltage limit with a voltage divider (two resistors in series).

    Godd luck with your project!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bnebeker
    0 bnebeker over 7 years ago

    This circuit has several issues and you have made some assumptions that are leading you in the wrong direction.

    The first issue is that balancing capacitors is not about switching large currents. The 80 mA current limit of the SAB series is more that what should be needed to balance capacitors. Balancing is needed because the leakage of the capacitors will not perfectly match however the leakage should be well below 50 mA overwise the capacitors are going to self discharge quickly. The use of zener diodes for voltage limiting will not work because zener diodes have two characteristics that work against you. First off they have a tolerance of at best 5% or typically 10%. The also have a high reverse leakage current and require current to flow through them reversed biased to perform there voltage drop function.The lower the zener voltage the more reverse current required and the more drift will be present in the zener diode. This means that power will be constantly wasted and you will need to set the limit voltage to around 2.1 volts maximum to account for drift and component tolerances.

     

    The second part of the problem is that the capacitor is going to discharge down from its fully charged voltage very quickly giving you a very short discharge curve. By using a boost converter you could discharge the capacitors down two around 2.5 volts across both capacitors. However stacking all four capacitors and charging then to around 9.4 volts using a boost converter would give you a discharge curve of 9.4 to 2.5 using a buck-boost converter instead of 5 to 2.5v as in your current design.

     

    Solder surface mounted components can be a challenge but low pin count surface mounted components are not that hard to deal with by using a few cheating methods.

     

    Method 1. Solder then on using a regular solder iron using fine solder. Solder one corner of the chip and don't worry if you get two pins at the same time. Just work on getting the chip aligned with just solder on one corner. Once you have one or two pins soldered and the chip aligned to the pads you can solder the opposite corner. This is keep the chip in place while to finish soldering. Take your time between solder pins to let the chip cool down and just solder a pin or two at a time. Don't worry about getting more than 1 pin at a time. The trick is to use de-soldering wick to remove the extra solder that is bridging the pins. SOIC packages are not that difficult as the gap between the pins is large enough to soaking up the solder easily.

     

    Method 2. Hot air soldering. This method requires spending around $100 for a cheap hot air soldering station but make mounting surface mounted component very easy. It also require purchasing soldering paste which is another $15. This method does not take long to learn and it provides a clean solder joint. This method works by just applying a thin coat of solder paste on the PCB pattern for the chip and then putting the chip on top of the solder paste. The exact amount of paste of not critical and the placement of the chip is not critical. You then heat the solder using the hot air slowly moving the air gun around to evenly heat the solder. Turn the air flow down to minimum and the temperature up to 40 degrees higher than the melting temperature of the paste. The package the paste comes in will tell you the melting temperature. This will  caused the flux in the paste to melt and will them lift the chip up from the board a little. As the flux evaporates the chip will align itself with the PCB pattern. Keep applying heat until the flux is gone and the solder because shiny on all of the pins. Take the heat away and let it cool, all done. If you find the alignment is not right apply the heat again to melt the solder and nudge the chip into alignment using something small like a paper clip.

     

    If you used too much solder paste you can use solder wick to remove the excess solder. If some pins don't seem to making contact you can use the solder wick with some solder in it to fix the problem. Put the solder wick over pin and heat with a soldering iron. This will wick some of the solder from the wick onto the board making a thin but solid connection.

     

    One of the keys in circuit design is to consider that all components are not perfect and you should never push them to the limit. The 2.5V capacitor should not seen more than 2.4V unless you want it to fail quickly. The capacitor itself may not properly withstand the voltage and the voltage you are measuring may not be are accurate as you thought it should be. Super capacitors are a special case as the only work are low voltages and thus require working near the stated voltage. Other capacitors should be derated by 20-30% and sometimes more if they are subjected to heat or surge voltages.

     

    A second key is that heat it the enemy. Most capacitors will live around twice as long by running at 10 degrees C cooler. Many components have a much longer lifetime but keeping the temperatures down to a reasonable level. Some components by nature must be run at higher temperatures to do there job but keeping other components from being heated by the hot component will help tremendously. As simple example of applying this would be to swap R1 and D1. The diode will not heat much at the current levels it will experience but the resistor will heat considerably when the capacitors are discharged. By connect the diode in the circuit to the capacitors instead of the resistor the heat from the resistor will not as easily couple to the first capacitor. While using a 5W resistor in this case is overkill it does have the advantage of dissipating heat faster thus running cooler.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BillyVelasquez
    0 BillyVelasquez 21 days ago

    This is an interesting discussion. One thing I learned when working with supercapacitors is that balancing becomes much more important than many people expect, especially when capacitors are connected in series. I like that you're considering several approaches instead of just relying on resistor balancing. The trade-off between efficiency, complexity, and long-term reliability is always the tricky part with these designs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett 21 days ago in reply to BillyVelasquez

     @  

    Did you notice that the question is 10 years old and the last answer is seven.

    I've been working on a super-capacitor buffered power supply with 10 x 400F caps in series. It has a micro to control balancing with up to about 3A current and measures the voltage across each cap.

    Have you got a supercap project on the go ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer