Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Beginner here. Designed a PC Arcade Controller, trying to figure out how to make it work.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 10 answers
  • Subscribers 320 subscribers
  • Views 4880 views
  • Users 0 members are here
  • custom arcade stick
  • teensy
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Beginner here. Designed a PC Arcade Controller, trying to figure out how to make it work.

lyndan
lyndan over 8 years ago

Over the past month or so I've been working on a design for my ideal PC game controller and I'm getting closer to figuring it all out.. And I was wondering if I could run it by the experts here for some help in understanding it all.

Here is the latest version of my design!

image

 

It started as my ideal handheld controller and evolved into an arcade stick. The stick I plan to build has two analog sticks; the leftmost analog stick being Ultimarc's Ultrastik 360 (or U360) and the rightmost being a thumbstick. Also on my design are 12 pushbuttons.

So I've been doing a lot of searching and learning about interfaces and such, but I still feel very in the dark. At this point, I believe it's a Teensy board that I'll need in order to convert these signals to digital so my PC can recognize my arcade controller as a HID. So as far as I understand, the voltage of the Interface I use will need to support the highest voltage of any of my switches, right? The U360 has it's own interface that you can hook to buttons and plug and play, but it only supports eight buttons, and my project incorporates 12 plus an additional analog stick. The U360 can also work in output mode, with 2 of it's eight pins outputting raw analog signal. Also note the stick can output digital 100% signals, but that is not what I want to use. I need the analog signals.

Here's the info on the U360: http://www.ultimarc.com/ultrastik_inst.html

So it shows the pin for powering the U360 is 5V.

Sorry for getting off topic a bit, but it says on the raw analog signals "not used at present".. Does this mean I wouldn't be able to use it? I contacted Andy at Ultimarc and he said it can output raw analog, but he seemed to want me to also buy his I-PAC for my extra buttons, which doesn't support analog, and just make my project act as two separate devices: one for the ultrastick and one for the buttons. That still doesn't let me use my extra analog stick and is too... messy for what I want. I want it to be clean and simple.

 

Anyway, as far as I can understand, I'll need a Teensy board that can power 5V, connect the two raw analog pins of the U360 to the Teensy's analog inputs and it should work fine, right?

Here is the analog stick from Adafruit I plan to pair with it: https://www.adafruit.com/product/512  "Usable with any voltage up to 5V, 2 analog outputs. 1 milliamp draw when used with 5V"

So the two analog sticks would take up four analog pins on a board, right? Then all that's left are the buttons which I can't find the voltage for.. it doesn't say on any of the sites for ordering them. I guess that's not something you have to worry about?

With all this information, if you notice something I'm missing, please let me know.

 

I guess the main questions I'm asking are: is this going to work with this U360 analog stick wired to a Teensy board, and which board should I buy for this project?

Thank you so much for your time.

  • Sign in to reply
  • Cancel

Top Replies

  • jeremy.f.medlin
    jeremy.f.medlin over 8 years ago in reply to lyndan +2 suggested
    Maybe this will help. Arduino is on the left. Each one of those lines represents a wire going somewhere. That +5V which is your power rail will connect to one side of your switch. Then an input pin wire…
  • Sean_Miller
    Sean_Miller over 8 years ago +1 suggested
    Good discussion. Your thumbstick is probably just two mechanically driven potentiometers that center on Vcc/2. So, not counting power and ground, you will consume two pins per stick. Get you the prototyping…
  • jeremy.f.medlin
    jeremy.f.medlin over 8 years ago in reply to lyndan +1 suggested
    Ah okay! Yep, definitely a way to get the joystick info. Hall effect sensors use voltage to determine direction, so you would read the voltage at the pins in order to find the direction and distance the…
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to lyndan

    the internal pull-up works the same as an external pull-up. it's just located inside the MCU device as opposed to externally.

     

    your diagram is correct. if you want, you can draw the pull-up resistor inside the UNO between the input and the internal +5v supply.

    e.g.:

    http://digitalmedia.risd.edu/pbadger/physcomp/uploads/Devices/MomentaryPullup2.png

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago

    I spotted this application note today and thought that it may be of some interest to you.

     

     

    Atmel AT01095: Joystick Game Controller Reference Design

     

    http://ww1.microchip.com/downloads/en/appnotes/atmel-42059-joystick-game-controller-reference-design_application%20note_…

     

    Note that it is based on the ATxmega32A4U microcontroller, as opposed to the ATmega328P as found in the Arduino UNO.

     

    Whilst you are there you may be interested in taking a look at page 97 of the ATmega328P data sheet.

     

     

    Ports as General Digital I/O

     

    http://ww1.microchip.com/downloads/en/DeviceDoc/Atmel-42735-8-bit-AVR-Microcontroller-ATmega328-328P_Datasheet.pdf#page=…

     

    which shows you the internal pull up resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lyndan
    0 lyndan over 8 years ago in reply to beacon_dave

    "All I/O pins have protection diodes to both Vcc and Ground as

    indicated in the following figure."

     

    Wait does that mean I don't have to ground all my buttons??

     

    EDIT: Wait that doesn't make any sense. How else could it sense the button is being pressed? lol

     

    I think I have it all figured out, but I have another question about my build: I need to supply 5V to both my analog sticks, but there's only one 5V pin on the Uno. So can I daisy chain my 5V to both the analog sticks?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to lyndan

    No, it means that the input pins have internal input protection clamping diodes...

     

    You may want to move your digital inputs away from D0 and D1 over to D12 and D13 so as to retain use of the serial comms on D0 and D1 for communicating with the host PC for programming/debugging. (You can also use A4 and A5 for digital IO if you don't need them for analogue input.)

     

    The +5v could come from the +5v pin on the UNO but be careful of how much current the funky joystick you are planning on using consumes. If you plan to power the UNO via the DC coaxial  connector, then the on-board voltage regulator has to power the UNO plus anything attached to that +5v power pin. The on-board regulator is rated at around 1A output. If you plan to power it off the USB connector, then there is an in-line 500mA polyfuse.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lyndan
    0 lyndan over 8 years ago in reply to beacon_dave

    Oh cool. So I could add more buttons if I wanted to. haha I think I'll stick with what I have here for now.

     

    There's no info on the draw of the Ultrastik, only that it uses 5V.

    I wasn't planning on powering the Uno by the DC Coaxial; just the USB. So is there some sort of precaution I can take to ensure it's safe?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to lyndan

    Get an Arduino Mega 2560 and you have 54 digital IO pins to play with...

     

    Perhaps connect your joystick to a power supply via a multimeter and see just how much current it draws.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<