Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Measure the volume change of a battery cell
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 5 answers
  • Subscribers 338 subscribers
  • Views 1662 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Measure the volume change of a battery cell

zeyang
zeyang over 8 years ago

Hello,

 

I would like measure the volume change of a lithium ion pouch cell during charge and discharge. The volume change will mainly reflect on the thickness of the battery. When it is discharged it is about 7 mm and it will increase by about 10% when it is charged. I would like to track the changes during charging.

 

We find this component as below which is a linear motion potentiaometer. https://se.farnell.com/ab-elektronik/4114902470/sensor-linear-5-kohm-20-flange/dp/2311430

  • ±20% Selection tolerance
  • ± 2.0% Typical independent linearity
  • 10mm ± 0.5mm Effective travel

 

Does the 20% means the accuracy of the potentiometer?

 

Do you have any suggestions about other type of sensors that I could use for this kind of measurement?

 

Thanks a lot for the help!

 

Best Regards,

 

/Zeyang

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +4 suggested
    You could also try capacitance measurement. If you put a foil "plate" on the battery and measure the capacitance to a nearby metal plate, the distance between plates will be directly proportional to the…
  • michaelkellett
    michaelkellett over 8 years ago +4 suggested
    You could do the measuring with Mitutoyo 575123 (Farnell 1667327 £169) - it outputs data in Mitotyo format so you need an interface and neither Farnell nor RS seem to sell these ! You can buy the interface…
  • shabaz
    shabaz over 8 years ago +3 verified
    Hi Zeyang, I think you're right, it is likely the overall resistance tolerance. But I think the 750 gram needed to operate this sensor could be too high for your application maybe? I don't know how much…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Zeyang,

     

    I think you're right, it is likely the overall resistance tolerance. But I think the 750 gram needed to operate this sensor could be too high for your application maybe? I don't know how much force is allowed. I think I'd do it differently. There are many ways you could consider. If money was not a concern, then an electronic dial indicator could be used, because that is available in low force versions, and it will be already calibrated. It can have a digital output to your computer, although an interface could be needed. For example, see Mitotoyu products.

     

    Otherwise, at very low cost (but you would need to do some machining and your own calibration) you could consider inductive sensing, e.g. see here:

    Getting Started with the LDC1000 - Small Metal Detection!

     

    You could have the metal plate target spaced off the battery using (say) a plastic block, so that the metal of the battery is not part of the inductive sensing.

    For calibration, you could use some manual measurement or reference devices, e.g. calipers or a gauge, or reference thickness blocks aka parallels (expensive) or layers of sheet material (cheap, less accurate but maybe sufficient for your needs).

     

    I think the lowest cost (and easiest) could be to use electronic calipers and just measure manually at different intervals during the charge/discharge process. But many have a serial output, so you could rig something up to automate this.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to shabaz

    Hi Shabaz,

    As soon as I read Zeyang's question I thought about the LDC1000 that you introduced to us a while back. Here is perhaps a good application. It is good you remembered it as I might have had a bit of trouble finding it.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago in reply to shabaz

    Hi Shabaz,

    As soon as I read Zeyang's question I thought about the LDC1000 that you introduced to us a while back. Here is perhaps a good application. It is good you remembered it as I might have had a bit of trouble finding it.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer