Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Repair Challenge: XBOX ONE S! (Beep on then beep off)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 7 answers
  • Subscribers 352 subscribers
  • Views 45565 views
  • Users 0 members are here
  • xbox
  • helpme
  • repair
  • xbox one s
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Repair Challenge: XBOX ONE S! (Beep on then beep off)

lilithelotor
lilithelotor over 7 years ago

CLARIFICATION

YES, BEFORE STARTING WORK ON THIS OF COURSE I GOOGLED AND WATCHED SEVERAL VIDEOS (MOSTLY USELESS) AND READ RESOURCES ON COMMON XBOX ONE AND ONE S PROBLEMS.

 

  1. I tried the HDD in a PC, and it does show up as several NTFS partitions with files that all look fine.
  2. Blu Ray drive at least powers up and can insert and eject a disc.
  3. Tried the "cold mode hairdrier" trick to spin the fan manually. It's not the fan. The fan works.

All other components of the board seem to work. Just the system started up with a startup sound, and shut down with a shut down sound immediately after. Likely a protection being triggered.

 

Help meee!

 

Trying to figure out this XBOX One S issue: https://www.ifixit.com/Answers/View/523582/PSU+11... Any ideas?

 

It makes the start and then stop sound. Southbridge gets voltage. All 12V test points get voltage. Power rails to CPU suspiciously low resistance. Details in iFixit link.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


I have an XBOX ONE S that I bought as “for parts” on eBay and the owner says it was kept in a clean house, etc. It is indeed clean inside. No signs of water damage.

The PSU is also fine. The APU had a TON of thermal grease all over the surface mount capacitors. I didn’t remove that yet but I did re-apply some arctic silver and I used a more reasonable amount.

The symptoms I see:

Console when plugged in does a few quick pulses to the APU fan. Is it trying to init?

Console when eject is pressed makes the eject sound, then the shutdown sound immediately after.

Console when power is pressed makes startup beep and then shutdown beep immediately after.

I don’t know what kind of issue I’m getting yet. Is there a JTAG interface or some way to do further diagnosis on this thing?

11.94V sounds perfectly fine for a 12V rail. Should I simpy try plugging a PC power supply into the motherboard to see if it will boot?

Any links or info on diagnosis would be appreciated.

Thanks in advance!


later

Aha! In the image you can see the CPU filter capacitor is registering just 1 ohm! The others are pretty low too but I bet if I remove that one it’ll at least boot. I have a server motherboard with a broken socket that I can steal capacitors from. Might replace the whole row if necessary.

image


later still

Looks like I was wrong. That capacitor I removed still offers up almost exactly the uf value on the tin. So that was another dead end. Hmm... One weird thing, all of the test points register 60Hz but not 110V. So thankfully the PSU isn't pushing wall socket voltage through. But that frequency is weird. My multimeter needs a charge though so I'll measure that again after it has.

The entire power area for the APU offers almost no resistance to the ground plane which is worrying. Again, need to charge that multimeter and re-check.


later again

Power on with no heatsink, the processor doesn't even warm to the touch. CPU, GPU, and other test points around the board pulse to 1-2V and then turn off fast.

Can't help but think it's related to the very low impedance between ground and positive on the V rails for the CPU/GPU. Is that normal?

USB port is charging the multimeter image

So that 5V rail from the southbridge is working.

Lots of 12V test points are consistently 12V (11.94V)


So...

Does any one have a diagram of the test points around the motherboard? What voltages / values should I be seeing? What are some likely culprits?

Thanks in advance! You're all wonderful!

 

This is the original XBOX One. Similar, but not exactly what I need. I can still maybe work from it.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago in reply to lilithelotor +5 suggested
    Sorry - I've been quite busy and am at work ... supposing you didn't lift any traces or warp the board significantly, you might well be fine. However, that's not to say that the VRM didn't fail for other…
  • lilithelotor
    lilithelotor over 7 years ago in reply to Gough Lui +4 suggested
    You are so wonderful and I can't thank you enough. I will work patiently from now on and I have learned a lot from this process. It is actually the first time I have ever used my hot air rework station…
  • Gough Lui
    Gough Lui over 7 years ago +3 suggested
    Most of the time, VRM issues are blown MOSFETs which have become shorted - your low resistance measurement is suggestive that the MOSFET on that phase may have gone shorted. Short burst of voltage and…
Parents
  • Gough Lui
    0 Gough Lui over 7 years ago

    Most of the time, VRM issues are blown MOSFETs which have become shorted - your low resistance measurement is suggestive that the MOSFET on that phase may have gone shorted. Short burst of voltage and shut down may be the converter going into protection due to overcurrent detection or because the shorted MOSFET may have tripped an upstream over-current protection.

     

    There's no easy way to test the MOSFET in circuit (to my knowledge, at least), but I would suggest replacing it and seeing what happens. It seems unlikely that the CPU/GPU itself is shorted since the other phases seem to measure a more reasonable resistance.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 7 years ago in reply to Gough Lui

    That's what I suspected but it's great to hear you say so too! One weird thing. 2 of the bigger MOSFETs (I think, markings are 4C55N RFJ4F) are not letting current through but the middle one is. Full short. No resistance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 7 years ago in reply to lilithelotor

    Addendum: I think the voltage rails on the CPU are all tied together. I did try testing resistance on every component and they all yield seemingly identical values. So Gough is right, it's hard to test for a fault that's not visible on the MOSFETs while they're on the board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • lilithelotor
    0 lilithelotor over 7 years ago in reply to lilithelotor

    Addendum: I think the voltage rails on the CPU are all tied together. I did try testing resistance on every component and they all yield seemingly identical values. So Gough is right, it's hard to test for a fault that's not visible on the MOSFETs while they're on the board.