Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Repair Challenge: XBOX ONE S! (Beep on then beep off)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 7 answers
  • Subscribers 352 subscribers
  • Views 46031 views
  • Users 0 members are here
  • xbox
  • helpme
  • repair
  • xbox one s
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Repair Challenge: XBOX ONE S! (Beep on then beep off)

lilithelotor
lilithelotor over 7 years ago

CLARIFICATION

YES, BEFORE STARTING WORK ON THIS OF COURSE I GOOGLED AND WATCHED SEVERAL VIDEOS (MOSTLY USELESS) AND READ RESOURCES ON COMMON XBOX ONE AND ONE S PROBLEMS.

 

  1. I tried the HDD in a PC, and it does show up as several NTFS partitions with files that all look fine.
  2. Blu Ray drive at least powers up and can insert and eject a disc.
  3. Tried the "cold mode hairdrier" trick to spin the fan manually. It's not the fan. The fan works.

All other components of the board seem to work. Just the system started up with a startup sound, and shut down with a shut down sound immediately after. Likely a protection being triggered.

 

Help meee!

 

Trying to figure out this XBOX One S issue: https://www.ifixit.com/Answers/View/523582/PSU+11... Any ideas?

 

It makes the start and then stop sound. Southbridge gets voltage. All 12V test points get voltage. Power rails to CPU suspiciously low resistance. Details in iFixit link.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


I have an XBOX ONE S that I bought as “for parts” on eBay and the owner says it was kept in a clean house, etc. It is indeed clean inside. No signs of water damage.

The PSU is also fine. The APU had a TON of thermal grease all over the surface mount capacitors. I didn’t remove that yet but I did re-apply some arctic silver and I used a more reasonable amount.

The symptoms I see:

Console when plugged in does a few quick pulses to the APU fan. Is it trying to init?

Console when eject is pressed makes the eject sound, then the shutdown sound immediately after.

Console when power is pressed makes startup beep and then shutdown beep immediately after.

I don’t know what kind of issue I’m getting yet. Is there a JTAG interface or some way to do further diagnosis on this thing?

11.94V sounds perfectly fine for a 12V rail. Should I simpy try plugging a PC power supply into the motherboard to see if it will boot?

Any links or info on diagnosis would be appreciated.

Thanks in advance!


later

Aha! In the image you can see the CPU filter capacitor is registering just 1 ohm! The others are pretty low too but I bet if I remove that one it’ll at least boot. I have a server motherboard with a broken socket that I can steal capacitors from. Might replace the whole row if necessary.

image


later still

Looks like I was wrong. That capacitor I removed still offers up almost exactly the uf value on the tin. So that was another dead end. Hmm... One weird thing, all of the test points register 60Hz but not 110V. So thankfully the PSU isn't pushing wall socket voltage through. But that frequency is weird. My multimeter needs a charge though so I'll measure that again after it has.

The entire power area for the APU offers almost no resistance to the ground plane which is worrying. Again, need to charge that multimeter and re-check.


later again

Power on with no heatsink, the processor doesn't even warm to the touch. CPU, GPU, and other test points around the board pulse to 1-2V and then turn off fast.

Can't help but think it's related to the very low impedance between ground and positive on the V rails for the CPU/GPU. Is that normal?

USB port is charging the multimeter image

So that 5V rail from the southbridge is working.

Lots of 12V test points are consistently 12V (11.94V)


So...

Does any one have a diagram of the test points around the motherboard? What voltages / values should I be seeing? What are some likely culprits?

Thanks in advance! You're all wonderful!

 

This is the original XBOX One. Similar, but not exactly what I need. I can still maybe work from it.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago in reply to lilithelotor +5 suggested
    Sorry - I've been quite busy and am at work ... supposing you didn't lift any traces or warp the board significantly, you might well be fine. However, that's not to say that the VRM didn't fail for other…
  • lilithelotor
    lilithelotor over 7 years ago in reply to Gough Lui +4 suggested
    You are so wonderful and I can't thank you enough. I will work patiently from now on and I have learned a lot from this process. It is actually the first time I have ever used my hot air rework station…
  • Gough Lui
    Gough Lui over 7 years ago +3 suggested
    Most of the time, VRM issues are blown MOSFETs which have become shorted - your low resistance measurement is suggestive that the MOSFET on that phase may have gone shorted. Short burst of voltage and…
  • blockaboots
    0 blockaboots over 6 years ago in reply to lilithelotor

    I tried testing the resistors around the mosfet chip on the other 2 phase lines (which had correct readings for the mosfet) to get an idea of what the resistor readings should be and then i tested the resistors on the bad mosfet phase line and they game me the same results as those on the 2 good phase lines, so i dont think its the resistors that are bad. I also doubt its the coil on each of the phase lines (big black box type thing) as essentially there just coils of wire. Im not sure what else to check, if it is a short else where it has to be a component before the mosfet i guess

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 6 years ago in reply to blockaboots

    Yeah this is a super hard one. I put it down a long time ago. Maybe I should fiddle with it again. I have new MSOFET chips but I may have done other damage to my board by messing around and without schematics or an oscilloscope I am really flying blind.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mysticalbacon679
    0 mysticalbacon679 over 6 years ago in reply to lilithelotor

    Hey im having the same issue but mine had a orange soda spilled on it. The edges where the copper is has dark brown spots on it. Same noises and fan situation as yours, even changed power supplies and still the same thing.  What do you think about that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • matey
    0 matey over 6 years ago

    I had a similar issue with an Xbox one s that I was repairing for my son's friend, the Xbox had no display due to bent pins in the hdmi port, I replaced the port , retested and had flashing display with artifacts, so I replaced the hdmi retimer IC.The first IC did nothing,checked my work and found bridged pins on the port, and some connections not making under the chip.All the voltages and grounds were present at the IC accept the operation enable pin will see 3.3volts and then drop to nothing, so I assumed I killed that chip and put another one on.This time the Xbox will power itself off after two seconds.This time I crapped myself thinking I had busted it, when I cleaned the CPU and replaced the thermal grease, I had trouble with the X clamp ,so I thought I must of used to much force and damaged the CPU. I went about checking resistances to ground and found all the caps under the CPU shorted to ground and other caps with low resistance to ground same as what's happening with the above Xbox, the test point for GFCORE read 0.9 ohms and the CPU CORE read 1.8 ohms which I took as a short, I had nothing to reference this board to I had no shorts on the six pins that the power supply connected to. This thing would also stay on for a couple of minutes without the hard drive connected.i gave up and told the misses it's dead I cant help it sorry give it back, she says are you sure so I tried once again I ordered some retimer ic from Digi key.I thought to myself that I didn't really touch anything apart from the port and the retimer IC and I watched people on YouTube hamfisting these clamps on and off.In the end I put on a third retimer module thinking it was a waste of time, but to my surprise it all worked I and my son played a few hours of FIFA football on it to test, then I handed it back. Sorry about the rambling story i hope this  might help someone out there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lukewalker67
    0 lukewalker67 over 6 years ago

    I bought a Xbox One S with the same exact problem. Interestingly though when I plug in the power adapter I get a fan twitch 3 or 4 times then it just stops. When I try to turn it on the light comes on but then goes straight off. I checked all the mosfets and they are all reading correctly and as far as I can see there are no shorts on the board. I am thinking that the problem is the APU. I tried turning it on again but this time I put a significant amount of pressure on the APU and then I got fanspin for a few seconds before it shut off again. I think the APU needs to be reflowed but I have no where near the experience or hardware to perform such a task. If you guys have any ideas let me know! Hope all is well and stay safe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • zt88
    0 zt88 over 6 years ago

    Hello, I have a similar problem... Mine is a little different however. Finding the test points on the board show all voltages are ok. nothing shorted. i am also getting vcore and gpucore voltages around .8 to 1.0. which would indicate that the fets on mine are not shorted and are working properly. The original fan will not spin under any conditions except for if the pwm pin (Pin 4) is disconnected. then i get full fan speed. Using an after market 4 pin case fan i can get controlled fan speeds and works fine with another xb fan. just not the original. also tested the original fan on other console and works just fine. I also notice that on initial plug in the aftermarket fan starts, gets to normal speed, shuts down and repeats 4 times. During this time i cannot power on the console and get power led. after the 4 intervals i can power on and get power led. The console only stays on for exactly 10 seconds. Does not matter if hdd is connected or not... 10 seconds on then off WITH sounds i might add. both power on and power off sounds. No display at any time in the testing. Not even a blip on a tv/PC monitor. Any suggestions or comments are apreciated. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 5 years ago

    I am having the same issue with my xbox one s, powers on then off.  I checked the power supply, re-imaged the hard drive, check voltages... etc.   nothing seems to be bad.  so i decided to follow the voltage from the power button specially from the power button card into the main board.  I have found that pin number one from left to right its off until i press the button, then its energized sending 2.1 volts to a resistor which it showing 100k omhs.   I compared the reading with another xbox one s and its showing 9.0k omhs for those resistors.  so its my belief that resistors R5F20, R6F13, R6F14, R6F15, R6F16, R6F17 should all be alike resistors and these resistors should all read around 9.0k omhs.   Can someone check your resistors R5F20, R6F13, R6F14, R6F15, R6F16, R6F17 and let me know if your resistors read 9.0k omhs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<