Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Low-level to High-level signal
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 314 subscribers
  • Views 1576 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Low-level to High-level signal

jimmyhu78
jimmyhu78 over 7 years ago

Hi all.

 

I tried to find the magic component on all famous retaillers but no way.

I'm looking for a solution which able to switching between a 28Vcc (state 1) and an open output (state 0), by a command signal of 200mV

 

When U>200mV is applied, that energize a relay which permit to supplied a 28V or let a 28V goes through itself.

When U<200mv is applied, relay is OFF, output is open.

 

I think it's possible to amplify the source signal before be able to command a relay.

But i'm completly lost in datasheets.

 

Does someone is able to help me for finfing an efficient solution?

 

Many thanks.

 

 

Jimmy

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +3 suggested
    You could do this with a 30V rail-to-rail op-amp like an OPA171 or an LT1637. If the current needs to be higher than the op-amp can supply, you can use a FET on the output.
  • dougw
    dougw over 7 years ago in reply to jimmyhu78 +3 suggested
    Diagram:
  • jw0752
    jw0752 over 7 years ago +2 suggested
    Hi Jimmy, I think a comparator circuit like I just used in my recent Interface Build might work. You will have to use a better comparator than the LM 393 or you could use a rail to rail op amp. Don't forget…
Parents
  • dougw
    0 dougw over 7 years ago

    You could do this with a 30V rail-to-rail op-amp like an OPA171 or an LT1637.

    If the current needs to be higher than the op-amp can supply, you can use a FET on the output.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 7 years ago

    You could do this with a 30V rail-to-rail op-amp like an OPA171 or an LT1637.

    If the current needs to be higher than the op-amp can supply, you can use a FET on the output.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer