Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My pin crimping tips -- what are yours?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 14 answers
  • Subscribers 341 subscribers
  • Views 17907 views
  • Users 0 members are here
  • pins
  • crimping
  • crimper
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My pin crimping tips -- what are yours?

Sean_Miller
Sean_Miller over 7 years ago

I am a self taught pin crimper.  Sounds like a personal problem, I know.

 

I have a crimper tool that looks like this:

imageimage

I use it to crimp pins for proto board soldered wire-to-board connectors that look like this:

 

image

 

At first, I was unhappy with the results due to the following results:

  • The wires would stab through the hole blocking the male end
  • I’d lose the pin from it falling off the cable before I could crimp it
  • the pins are hard to seat into the connector
  • the pins back out of the connector when connected to the male end
  • the wire breaks off at the base of the pin
  • the male pins would not want to stab into the female after everything was crimped and ready

 

<EDIT:  See this post below for the crowd improved troubleshooting guide:  https://www.element14.com/community/message/284233/l/re-my-pin-crimping-tips-what-are-yours#284233 >

Here's how I adjusted my approach:

IssueSolution
Wires stabbing through the holeI bend the wires back over the insulation
Dropping the pinI’d pre crimp the bottom with just my fingers to hold it in place.
Hard to seatAfter crimping the bottom of the crimp pin to the cable sheathing, I take a small plier to shape the female tip to remove any parts sticking out impeding entry into the plastic connector housing.
pins back outAfter adjusting the pin shape in the previous step, I pull up the tab that will catch inside the connector to prevent it from backing out.
the wire breaks offI stopped using jumper cables as the donor wire.  Instead, I use ribbon cable.
Male pins not fittingI use a single jumper male pin to pre stab in the female pins I just inserted into the connector to open it back up.

 

 

I now get reasonable results, but what bothers me is that I have to do all this.  I would think I could just crimp and insert and be done.

 

So, my question is, what are the community members experiences, steps, and tricks for using crimp pins?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to fmilburn +6 suggested
    That's a good link , Frank. @Sean As you'll see from Frank's link, bending the inner back over the insulation is wrong. It sounds to me as if you are using the wrong tool for the crimp, and stripping off…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to fmilburn +6 suggested
    Thanks for linking that thread, Frank. All that shop talk was happening on my birthday. Funny thing was, I was probably trying to crimp pins and missed it. Looks like the one twist I had from Shabaz's…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Sean, My experience is similar to yours. There is a good discussion here: https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825. Several people give…
Parents
  • koudelad
    0 koudelad over 7 years ago

    I personally tried about 3 types of crimp tools (mentioned above and in the linked discussion) in addition to just small pliers. However, I don't always have original DuPont connectors and even small differences mean crimping might go wrong. Or the crimp looks OK, but the connector can't be inserted to the housing.

     

    I haven't seen anyone recommending Engineer's crimp tools: ENGINEER INC. - PRECISION CONNECTOR CRIMPING PLIERS FOR NARROW-PITCH AND UNIVERSAL CRIMPING

    It is a universal tool, have a look at the application guide: ENGINEER INC. - PRECISION CONNECTOR CRIMPING PLIERS FOR NARROW-PITCH AND UNIVERSAL CRIMPING

     

    image

     

    It costs about €60. I use it for 2.54 mm connectors, but also made great crimps of JST 1.5 mm, 2.0 mm, 2.5 mm connectors. Specialized crimp tools for just one or two types were offered to us at work for about € 300.

    The downside is, you need to crimp every connector twice, the inner conductor first, the insulated part second.

     

    David

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • IanJeffray
    0 IanJeffray over 7 years ago in reply to koudelad

    I bought these Engineers tools.  I make just as much of a hash of crimping things with htese as with any other tools to be honest.   My best tip for crimping is -- don't bother, buy pre-crimped wires.   At least, specifically, I do a lot of work with Molex PicoBlade stuff and these pins are absolutely minute.  The pre-crimped wires are eyewaterinly expensive, but worrk out efficient when I consider my time and annoyance level at trying to crimp these myself.

     

    Getting just the correct length of conductor exposed appears to be incredibly important too.  With very much sub-millimetre precision.  If the conductor is too long, it'll sit inside the crimp contact and cause issues when inserting the resultant crimped pin in to the mating connector.

     

    Getting the force correct is also incredibly difficult -- insufficient crimping forrce means the thing falls apart, obviously.   Too much force can easily mangle the crimp pin and it either immediately breaks in half, or fails quckly in use.

     

    The whole crimping game is a total nightmare as far as I'm concerned.  Buy pre-crimped leads.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to IanJeffray

    That's good advice, especially with PicoBlade, where the pre-crimped wires are easily available.  Similarly for hobby use, there's cheap 0.1" pre-crimped cables and I buy them too.

    Sometimes I do want custom cables though, and especially when they are the larger ones (like 0.1" pin headers) then the crimp tools (at least the ratcheting one mentioned above) can perform a reliable job just as good or better than ready-crimped 0.1" header wires. I find it satisfying making nicer perfect-length cables and then using heat-shrink than those single 0.1" shells - admittedly not a very productive thing to do though!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago in reply to IanJeffray

    That's good advice, especially with PicoBlade, where the pre-crimped wires are easily available.  Similarly for hobby use, there's cheap 0.1" pre-crimped cables and I buy them too.

    Sometimes I do want custom cables though, and especially when they are the larger ones (like 0.1" pin headers) then the crimp tools (at least the ratcheting one mentioned above) can perform a reliable job just as good or better than ready-crimped 0.1" header wires. I find it satisfying making nicer perfect-length cables and then using heat-shrink than those single 0.1" shells - admittedly not a very productive thing to do though!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • koudelad
    0 koudelad over 7 years ago in reply to shabaz

    Same here. I create custom length cables and also use different wire colors to distinguish between power and various signal wires.

    However, I am talking about only a few cables a month (both privately and at work). When manufacturing some quantities, it is better to get cables crimped by a machine.