Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My pin crimping tips -- what are yours?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 14 answers
  • Subscribers 341 subscribers
  • Views 17896 views
  • Users 0 members are here
  • pins
  • crimping
  • crimper
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My pin crimping tips -- what are yours?

Sean_Miller
Sean_Miller over 7 years ago

I am a self taught pin crimper.  Sounds like a personal problem, I know.

 

I have a crimper tool that looks like this:

imageimage

I use it to crimp pins for proto board soldered wire-to-board connectors that look like this:

 

image

 

At first, I was unhappy with the results due to the following results:

  • The wires would stab through the hole blocking the male end
  • I’d lose the pin from it falling off the cable before I could crimp it
  • the pins are hard to seat into the connector
  • the pins back out of the connector when connected to the male end
  • the wire breaks off at the base of the pin
  • the male pins would not want to stab into the female after everything was crimped and ready

 

<EDIT:  See this post below for the crowd improved troubleshooting guide:  https://www.element14.com/community/message/284233/l/re-my-pin-crimping-tips-what-are-yours#284233 >

Here's how I adjusted my approach:

IssueSolution
Wires stabbing through the holeI bend the wires back over the insulation
Dropping the pinI’d pre crimp the bottom with just my fingers to hold it in place.
Hard to seatAfter crimping the bottom of the crimp pin to the cable sheathing, I take a small plier to shape the female tip to remove any parts sticking out impeding entry into the plastic connector housing.
pins back outAfter adjusting the pin shape in the previous step, I pull up the tab that will catch inside the connector to prevent it from backing out.
the wire breaks offI stopped using jumper cables as the donor wire.  Instead, I use ribbon cable.
Male pins not fittingI use a single jumper male pin to pre stab in the female pins I just inserted into the connector to open it back up.

 

 

I now get reasonable results, but what bothers me is that I have to do all this.  I would think I could just crimp and insert and be done.

 

So, my question is, what are the community members experiences, steps, and tricks for using crimp pins?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to fmilburn +6 suggested
    That's a good link , Frank. @Sean As you'll see from Frank's link, bending the inner back over the insulation is wrong. It sounds to me as if you are using the wrong tool for the crimp, and stripping off…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to fmilburn +6 suggested
    Thanks for linking that thread, Frank. All that shop talk was happening on my birthday. Funny thing was, I was probably trying to crimp pins and missed it. Looks like the one twist I had from Shabaz's…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Sean, My experience is similar to yours. There is a good discussion here: https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825. Several people give…
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Sean,

     

    I've not found a universal tool, but I've got about three different ones, and between them I've so far got repeatable results for a good range of crimps. I'm sure there's other low-cost tools that are just as good or better, these are merely the ones I'm using:

    For the 0.1" pitch header pin sockets or pins, I'm at 100% repeatable results (unless I'm extremely careless) with the HT-225DHT-225D tool (some photos of how to use the tool, and the results on 0.1" crimps are in that other thread that Frank mentioned).

    It's also fine for other similarly-sized, and larger pins or sockets - it gives superb results with MATE'N'LOK crimps too (again 100% repeatable, with what looks to me like a great crimp and grip on the insulation; see photo below), which are intended for up to 19A.

    image

     

     

    For smaller than 0.1" pitch, e.g. JST ZH (as used on the BeagleBone-AI serial connector) then I had to resort to a PA-09 tool. That's a fairly low-cost tool, which is useful for the extremely small crimps (like 2mm pitch). It can do 0.1" pitch too, but HT-225DHT-225D is better for those since that has a proper ratchet action and simultaneously does the insulation as well as the conductor. With the PA-09, they have to be done separately.

     

    Finally from Fry's I've got this crimp tool: https://www.frys.com/product/1922790 which is sometimes handy if there's some unusual connector. It is intended for D-sub connectors but works with other stuff. I prefer the HT-225DHT-225D overall though.

     

    Here's how I try to resolve the issues you mention:

    1. Better accuracy with wire strip length, so that the wire doesn't go into the wrong area. Something like the Stripmaster LiteStripmaster Lite is great for thinner wires, or the Knipex tool here: Knipex Precision Wire Insulation Strippers Review - Model 12 12 06  because they strip the insulation fairly square, and repeatably. The Knipex tool has a depth stop, and I think the Stripmaster Lite may have that as an optional extra (otherwise it should be easy to 3D-print an attachment for it). The photo above shows a wire that was stripped with the Knipex tool, and the insulation is cut very square. I didn't set the depth stop correctly since the wire is protruding by about 1mm into the space where it shouldn't, but I don't think that has an impact for this particular connector. If the wire is extremely thin, then I may fold back and double the wire, but not over the insulation.

    2. I have no real solution to this, except either crimping the ratchet by one or two clicks so that the crimp is held in place and then I only need one hand on the tool and one hand guiding in the wire, or putting light pressure on the tool so that the crimp is held in place. In other words, the crimp is solely held by the tool, and that leaves me with one hand free to then insert the wire. With the HT-225DHT-225D, I can tell when the wire is inserted in to the correct depth, because I hold the tool at an angle and guide in the wire until I see a glint of the wire from the other side. Somehow that's quite repeatable, although it sounds like it shouldn't be : )

    3. I use your solution. It does sometimes happen, if the wire insulation is thicker than will easily fit into the plastic housing.

    4. This doesn't happen much, but your solution seems good (or push the latching plastic on the shell in slightly, if the shell has that feature.

    5. So far I don't see this issue too often, but for single jumper wires I like using heatshrink.

    6. So far I've not encountered this much (usually the crimp tool won't affect the working end of the crimp) but the solutions you mention seem good.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi Sean,

     

    I've not found a universal tool, but I've got about three different ones, and between them I've so far got repeatable results for a good range of crimps. I'm sure there's other low-cost tools that are just as good or better, these are merely the ones I'm using:

    For the 0.1" pitch header pin sockets or pins, I'm at 100% repeatable results (unless I'm extremely careless) with the HT-225DHT-225D tool (some photos of how to use the tool, and the results on 0.1" crimps are in that other thread that Frank mentioned).

    It's also fine for other similarly-sized, and larger pins or sockets - it gives superb results with MATE'N'LOK crimps too (again 100% repeatable, with what looks to me like a great crimp and grip on the insulation; see photo below), which are intended for up to 19A.

    image

     

     

    For smaller than 0.1" pitch, e.g. JST ZH (as used on the BeagleBone-AI serial connector) then I had to resort to a PA-09 tool. That's a fairly low-cost tool, which is useful for the extremely small crimps (like 2mm pitch). It can do 0.1" pitch too, but HT-225DHT-225D is better for those since that has a proper ratchet action and simultaneously does the insulation as well as the conductor. With the PA-09, they have to be done separately.

     

    Finally from Fry's I've got this crimp tool: https://www.frys.com/product/1922790 which is sometimes handy if there's some unusual connector. It is intended for D-sub connectors but works with other stuff. I prefer the HT-225DHT-225D overall though.

     

    Here's how I try to resolve the issues you mention:

    1. Better accuracy with wire strip length, so that the wire doesn't go into the wrong area. Something like the Stripmaster LiteStripmaster Lite is great for thinner wires, or the Knipex tool here: Knipex Precision Wire Insulation Strippers Review - Model 12 12 06  because they strip the insulation fairly square, and repeatably. The Knipex tool has a depth stop, and I think the Stripmaster Lite may have that as an optional extra (otherwise it should be easy to 3D-print an attachment for it). The photo above shows a wire that was stripped with the Knipex tool, and the insulation is cut very square. I didn't set the depth stop correctly since the wire is protruding by about 1mm into the space where it shouldn't, but I don't think that has an impact for this particular connector. If the wire is extremely thin, then I may fold back and double the wire, but not over the insulation.

    2. I have no real solution to this, except either crimping the ratchet by one or two clicks so that the crimp is held in place and then I only need one hand on the tool and one hand guiding in the wire, or putting light pressure on the tool so that the crimp is held in place. In other words, the crimp is solely held by the tool, and that leaves me with one hand free to then insert the wire. With the HT-225DHT-225D, I can tell when the wire is inserted in to the correct depth, because I hold the tool at an angle and guide in the wire until I see a glint of the wire from the other side. Somehow that's quite repeatable, although it sounds like it shouldn't be : )

    3. I use your solution. It does sometimes happen, if the wire insulation is thicker than will easily fit into the plastic housing.

    4. This doesn't happen much, but your solution seems good (or push the latching plastic on the shell in slightly, if the shell has that feature.

    5. So far I don't see this issue too often, but for single jumper wires I like using heatshrink.

    6. So far I've not encountered this much (usually the crimp tool won't affect the working end of the crimp) but the solutions you mention seem good.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer