Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My pin crimping tips -- what are yours?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 14 answers
  • Subscribers 341 subscribers
  • Views 17907 views
  • Users 0 members are here
  • pins
  • crimping
  • crimper
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My pin crimping tips -- what are yours?

Sean_Miller
Sean_Miller over 7 years ago

I am a self taught pin crimper.  Sounds like a personal problem, I know.

 

I have a crimper tool that looks like this:

imageimage

I use it to crimp pins for proto board soldered wire-to-board connectors that look like this:

 

image

 

At first, I was unhappy with the results due to the following results:

  • The wires would stab through the hole blocking the male end
  • I’d lose the pin from it falling off the cable before I could crimp it
  • the pins are hard to seat into the connector
  • the pins back out of the connector when connected to the male end
  • the wire breaks off at the base of the pin
  • the male pins would not want to stab into the female after everything was crimped and ready

 

<EDIT:  See this post below for the crowd improved troubleshooting guide:  https://www.element14.com/community/message/284233/l/re-my-pin-crimping-tips-what-are-yours#284233 >

Here's how I adjusted my approach:

IssueSolution
Wires stabbing through the holeI bend the wires back over the insulation
Dropping the pinI’d pre crimp the bottom with just my fingers to hold it in place.
Hard to seatAfter crimping the bottom of the crimp pin to the cable sheathing, I take a small plier to shape the female tip to remove any parts sticking out impeding entry into the plastic connector housing.
pins back outAfter adjusting the pin shape in the previous step, I pull up the tab that will catch inside the connector to prevent it from backing out.
the wire breaks offI stopped using jumper cables as the donor wire.  Instead, I use ribbon cable.
Male pins not fittingI use a single jumper male pin to pre stab in the female pins I just inserted into the connector to open it back up.

 

 

I now get reasonable results, but what bothers me is that I have to do all this.  I would think I could just crimp and insert and be done.

 

So, my question is, what are the community members experiences, steps, and tricks for using crimp pins?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to fmilburn +6 suggested
    That's a good link , Frank. @Sean As you'll see from Frank's link, bending the inner back over the insulation is wrong. It sounds to me as if you are using the wrong tool for the crimp, and stripping off…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to fmilburn +6 suggested
    Thanks for linking that thread, Frank. All that shop talk was happening on my birthday. Funny thing was, I was probably trying to crimp pins and missed it. Looks like the one twist I had from Shabaz's…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Sean, My experience is similar to yours. There is a good discussion here: https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825. Several people give…
Parents
  • fmilburn
    0 fmilburn over 7 years ago

    Hi Sean,

     

    My experience is similar to yours.  There is a good discussion here:  https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825.  Several people give their experience including me.  Andreas Spiess has a youtube channel and has quite a bit on them as well.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to fmilburn

    That's a good link , Frank.

     

    @Sean As you'll see from Frank's link, bending the inner back over the insulation is wrong. It sounds to me as if you are using the wrong tool for the crimp, and stripping off too much insulation.

     

    The long stripped section is why you are poking the wire in too far.

    I suspect that backing out is caused by deforming the whole crimp, usually due to using the wrong tool.

     

    Having said all that, some crimps are just plain difficult, and unless you can afford a real tool (typically over £200 for once from the connector manufacturer) best left alone.

     

    I've had reasonable results with Molex KK types and Amp using cheapo tools.

     

    08-50-0032 -

    Contact, KKRegistered 254, KK 254 4809 Series, Socket, Crimp, 22 AWG, Tin Plated Contacts 

     

      image 

     

     

        Add to compare 

     

    Image is for illustrative purposes only. Please refer to product description.

    MOLEX

     

    Manufacturer:
    MOLEX 

     

     

    Manufacturer Part No:
    08-50-003

     

     

    TE Connectivity AMPMODU MOD II Female Crimp Terminal Contact 22AWG 181270-2181270-2

    • RS Stock No. 233-0038
    • Mfr. Part No. 181270-2181270-2 
    • Brand  TE Connectivity

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • abrain
    0 abrain over 7 years ago in reply to michaelkellett

    I know a chap who used to solder those Molex crimps.... I just bought the Molex crimp tool and it saved me both a ton of time making the connections in the first place, and the connections were reliable too! Those friction lock KK housings are pretty secure too, good enough for applications on the railway!

     

    A

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • abrain
    0 abrain over 7 years ago in reply to michaelkellett

    I know a chap who used to solder those Molex crimps.... I just bought the Molex crimp tool and it saved me both a ton of time making the connections in the first place, and the connections were reliable too! Those friction lock KK housings are pretty secure too, good enough for applications on the railway!

     

    A

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer