Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My pin crimping tips -- what are yours?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 14 answers
  • Subscribers 341 subscribers
  • Views 17907 views
  • Users 0 members are here
  • pins
  • crimping
  • crimper
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My pin crimping tips -- what are yours?

Sean_Miller
Sean_Miller over 7 years ago

I am a self taught pin crimper.  Sounds like a personal problem, I know.

 

I have a crimper tool that looks like this:

imageimage

I use it to crimp pins for proto board soldered wire-to-board connectors that look like this:

 

image

 

At first, I was unhappy with the results due to the following results:

  • The wires would stab through the hole blocking the male end
  • I’d lose the pin from it falling off the cable before I could crimp it
  • the pins are hard to seat into the connector
  • the pins back out of the connector when connected to the male end
  • the wire breaks off at the base of the pin
  • the male pins would not want to stab into the female after everything was crimped and ready

 

<EDIT:  See this post below for the crowd improved troubleshooting guide:  https://www.element14.com/community/message/284233/l/re-my-pin-crimping-tips-what-are-yours#284233 >

Here's how I adjusted my approach:

IssueSolution
Wires stabbing through the holeI bend the wires back over the insulation
Dropping the pinI’d pre crimp the bottom with just my fingers to hold it in place.
Hard to seatAfter crimping the bottom of the crimp pin to the cable sheathing, I take a small plier to shape the female tip to remove any parts sticking out impeding entry into the plastic connector housing.
pins back outAfter adjusting the pin shape in the previous step, I pull up the tab that will catch inside the connector to prevent it from backing out.
the wire breaks offI stopped using jumper cables as the donor wire.  Instead, I use ribbon cable.
Male pins not fittingI use a single jumper male pin to pre stab in the female pins I just inserted into the connector to open it back up.

 

 

I now get reasonable results, but what bothers me is that I have to do all this.  I would think I could just crimp and insert and be done.

 

So, my question is, what are the community members experiences, steps, and tricks for using crimp pins?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to fmilburn +6 suggested
    That's a good link , Frank. @Sean As you'll see from Frank's link, bending the inner back over the insulation is wrong. It sounds to me as if you are using the wrong tool for the crimp, and stripping off…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to fmilburn +6 suggested
    Thanks for linking that thread, Frank. All that shop talk was happening on my birthday. Funny thing was, I was probably trying to crimp pins and missed it. Looks like the one twist I had from Shabaz's…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Sean, My experience is similar to yours. There is a good discussion here: https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825. Several people give…
Parents
  • dougw
    0 dougw over 7 years ago

    Good crimpers are expensive and many pins require a specialized crimper to do an optimal job. It gets very expensive to acquire enough crimpers to cover all connectors.

    I have to make do with a low-cost crimper which covers numerous sizes and I use it for many different connectors:

    image

    In order to achieve decent crimps for a variety of connectors, it is necessary to figure out a process for each type. For example on some connectors I have to crimp the wire first and the insulation in a second pass with a different jaw. It also requires close inspection of every crimp to ensure it is done well. I generally place the pin in the crimper jaw and hold it in position while closing the jaw until the pin is held securely. Then I slide the wire in to the proper depth before completing the crimp.

    Those small JST pins are particularly difficult with this crimper.

    In better crimpers, the pin fits the jaw with no ambiguity.

    Of course I would like better crimpers, but so far have not been able to justify their price. Needless to say, I only crimp when absolutely necessary. I use solder or insulation displacement whenever possible.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to dougw

    dougw  wrote:

     

    Good crimpers are expensive

    Eeek - too true - I just decided that these were the optimum for a power supply I need to build

     

    08-70-1031 -

    Contact, SPOXTm BMI, SPOX 5194 Series, Socket, Crimp, 18 AWG, Tin Plated Contacts

     

      08-70-1031 - Contact, SPOX&trade; BMI, SPOX 5194 Series, Socket, Crimp, 18 AWG, Tin Plated Contacts

     

     


    https://uk.farnell.com/b/molex

     

    And this is the official crimp tool, at £347

    63811-650063811-6500 -

    Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series 

     

      63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series 

     

     

    63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series

     

     

      63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series 

     

    63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series

        Add to compare 

    Image is for illustrative purposes only. Please refer to product description.

    MOLEX

     

    Manufacturer:  MOLEX 

     

     

    Manufacturer Part No:  63811-650063811-6500

     

     

    Order Code:  2668374

     

     

    Product Range    207129 Series

     

    Needless to say I'll be using one out of the collection of oldies and cheapies !
    MK

     

      

     

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to dougw

    dougw  wrote:

     

    Good crimpers are expensive

    Eeek - too true - I just decided that these were the optimum for a power supply I need to build

     

    08-70-1031 -

    Contact, SPOXTm BMI, SPOX 5194 Series, Socket, Crimp, 18 AWG, Tin Plated Contacts

     

      08-70-1031 - Contact, SPOX&trade; BMI, SPOX 5194 Series, Socket, Crimp, 18 AWG, Tin Plated Contacts

     

     


    https://uk.farnell.com/b/molex

     

    And this is the official crimp tool, at £347

    63811-650063811-6500 -

    Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series 

     

      63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series 

     

     

    63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series

     

     

      63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series 

     

    63811-6500 - Crimp Tool, Ratchet, Molex SPOX 5194 Series 24-18AWG Contacts, 207129 Series

        Add to compare 

    Image is for illustrative purposes only. Please refer to product description.

    MOLEX

     

    Manufacturer:  MOLEX 

     

     

    Manufacturer Part No:  63811-650063811-6500

     

     

    Order Code:  2668374

     

     

    Product Range    207129 Series

     

    Needless to say I'll be using one out of the collection of oldies and cheapies !
    MK

     

      

     

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • neilk
    0 neilk over 7 years ago in reply to michaelkellett

    image  image