Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum My pin crimping tips -- what are yours?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 14 answers
  • Subscribers 341 subscribers
  • Views 17907 views
  • Users 0 members are here
  • pins
  • crimping
  • crimper
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

My pin crimping tips -- what are yours?

Sean_Miller
Sean_Miller over 7 years ago

I am a self taught pin crimper.  Sounds like a personal problem, I know.

 

I have a crimper tool that looks like this:

imageimage

I use it to crimp pins for proto board soldered wire-to-board connectors that look like this:

 

image

 

At first, I was unhappy with the results due to the following results:

  • The wires would stab through the hole blocking the male end
  • I’d lose the pin from it falling off the cable before I could crimp it
  • the pins are hard to seat into the connector
  • the pins back out of the connector when connected to the male end
  • the wire breaks off at the base of the pin
  • the male pins would not want to stab into the female after everything was crimped and ready

 

<EDIT:  See this post below for the crowd improved troubleshooting guide:  https://www.element14.com/community/message/284233/l/re-my-pin-crimping-tips-what-are-yours#284233 >

Here's how I adjusted my approach:

IssueSolution
Wires stabbing through the holeI bend the wires back over the insulation
Dropping the pinI’d pre crimp the bottom with just my fingers to hold it in place.
Hard to seatAfter crimping the bottom of the crimp pin to the cable sheathing, I take a small plier to shape the female tip to remove any parts sticking out impeding entry into the plastic connector housing.
pins back outAfter adjusting the pin shape in the previous step, I pull up the tab that will catch inside the connector to prevent it from backing out.
the wire breaks offI stopped using jumper cables as the donor wire.  Instead, I use ribbon cable.
Male pins not fittingI use a single jumper male pin to pre stab in the female pins I just inserted into the connector to open it back up.

 

 

I now get reasonable results, but what bothers me is that I have to do all this.  I would think I could just crimp and insert and be done.

 

So, my question is, what are the community members experiences, steps, and tricks for using crimp pins?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to fmilburn +6 suggested
    That's a good link , Frank. @Sean As you'll see from Frank's link, bending the inner back over the insulation is wrong. It sounds to me as if you are using the wrong tool for the crimp, and stripping off…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to fmilburn +6 suggested
    Thanks for linking that thread, Frank. All that shop talk was happening on my birthday. Funny thing was, I was probably trying to crimp pins and missed it. Looks like the one twist I had from Shabaz's…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Sean, My experience is similar to yours. There is a good discussion here: https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825. Several people give…
Parents
  • fmilburn
    0 fmilburn over 7 years ago

    Hi Sean,

     

    My experience is similar to yours.  There is a good discussion here:  https://www.element14.com/community/message/276825/l/re-creating-dupont-equivalent-crimp-terminal#276825.  Several people give their experience including me.  Andreas Spiess has a youtube channel and has quite a bit on them as well.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 7 years ago in reply to fmilburn

    Thanks for linking that thread, Frank.  All that shop talk was happening on my birthday.  Funny thing was, I was probably trying to crimp pins and missed it.

     

    Looks like the one twist I had from Shabaz's guide is how to use the second crimp zone.  I had evolved to bend the bare wire back on the insulation and use both crimp zones to grab the insulation to prevent the wire from breaking and to get more copper surface area contacted.  To see how they are mass produced, I just destroyed a store bought cable and did indeed find that the second crimp zone should be nothing but raw copper wire.  So, I updated my troubleshooting chart below.  Note, its not just for DuPont pins in mind, but variations.

     

    Pin Crimping Troubleshooting Guide

    Issue

    Solution

    Wires stabbing through the holeCut off enough insulation such that the cable insulation will sit at the base (outer) crimp zone and raw copper will be crimped in the next zone. If you have excess, "Double up" the excess to the raw copper zone or trim it to fit.  See next issue to prevent it from slipping forward prior to crimping.
    Dropping the pinPaying close attention to orientation of the pin in the jaws (it's designed to fit only one way), squeeze the pin by itself until one ratchet click.  Then, insert the wire.  Make sure the copper isn't too long, then squeeze all the way.
    Hard to seat in the housing

    The standard crimping tool is designed to go one way.  It has a recess on one so that the lower section of the pin crimps with a bigger diameter to accomodate for the insulation.  The upper section of the crimper jaw has a smaller diameter to grab the bare wire.  So, its imperative that you place the pin in the crimper such that each section is aligned with the tool correctly and no pin section overlap occurs in the center.  If not, you'll deform the pin such that it will give unpredictable results when trying to slide in the housing.

     

    If the pin is so small that it fits inside the width of the crimper, then you need to switch to a different style crimper such as the PA-09.  That style crimper doesn't have the offset and is designed to first squeeze the base of the pin at the insulation and then squeeze again at the next crimp section that is at the bare wire.

     

    After crimping, gently push the pin into its housing observing where any clearance issues may be.  If needed, take a small plier to shape any parts sticking out impeding entry.  This may be the case for the smaller pins or if your tool is slightly oversized than the pin your crimping.

    pins back out when making final connectionDepending on the pin, there may or may not be a tab that will click into an opening visible of its connector housing.  That needs pulled out a little if you did not get a confirmational click.  Other problems could be you simply have not inserted it all the way in so that the catch mechanism has had a chance to click into place.  Use a small flat tipped screwdriver to push the pin at its base into the housing further.  You may need to put the pin under a microscope to fully understand the latching design.  Note, most pins are designed to be oriented one way in the housing.  Getting this backwards will definitely cause it to push back out.
    the wire breaks off

    Some cables are designed to be very flexible, but require pins that provide substantial crimp contact area as well as a connector housing that provides stress relief (example, DuPont pins on jumper cable).  Such cables do poorly for pins that have tiny crimp contact area and no stress relief.  For these, try ribbon cable instead or provide stress relief using heat shrink over the crimp zone of each pin and outward at least 1/2".

    In general, don't over squeeze or squeeze too quickly as it can snap the insulation section.

    Male pins not fittingFor connectors used on 0.1" pitch headers, such as the Raspberry Pi, you may use a single jumper male pin to pre stab in the female pins prior to final assembly of the connector.  This will correct any distortions that may have occurred in the crimping process.  For other connectors, try a single male header pin to work each female pin individually.
    All otherPractice, Practice, Practice!

     

    After reading the other thread, coupled to my own experiences, I now feel confident I'm on the right track.  I had a good project yesterday that gave me plenty of practice on an assortment of the cheap chinese pins.  The results were custom sized, strong wire-to-board connectors that cleaned up the inside of the enclosure and are ready for the field.  The project will measure vessel growth due to thermal expansion over a 30 hour operational cycle.  This will allow me to locate vessel attachments without concern of clearance issues with its surroundings.

     

    Thanks!

    Sean

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dpenny
    0 dpenny over 5 years ago in reply to Sean_Miller

    Am new to using molex pins/sockets. Am hobbist doing 5-10 pins per year manually - oh well. Bought pins and housing from Amazon. Pins come attached to a "carrier strip." (dont know what else to call it)

     

    Am having probs getting pins to seat into the housing. Using 093 2-pin sockets with 18 ga lamp wire. My crimps on wire and insulation look good but cannot push into housing cause of "flaps" from carrier strip. If I trim flaps same as body width of pin, then the pin pulls out forward as I connect/disconnect housing pairs. If I leave trim flaps from carrier strip, I cannot push pin into housing.

     

    I have seen lots of stuff on web about crimps to wire and its insulation, but NOTHING about how to trim these carrier strip flaps.

     

    Advice needed.  I am having a 30% failure rate.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to dpenny

    Pictures might help but when I cut a pin off the carrier strip, I cut the carrier strip leaving a small 'tab' on the end of the pin.  After crimping, I cut this 'tab' off at the top of the pin and don't leave any of the carrier strip attached to the pin at all.  It's not really clear what you mean by 'flaps', perhaps you could post some pictures.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to dpenny

    The carrier strips are for machine feed, but should be totally removed, as Andrew mentions.

    If the crimping action using your tool has left the wire grip portion too wide to fit the housing, then it can be gently re-shaped after crimping using needle-nosed pliers. For insertion into the housing, 18 gauge wire is so thick it should be almost effortless to push the wire and terminal into the housing.

    It needs photos, otherwise there's not a lot to go on.

     

    Also, those .093" crimp pins/sockets use a Molex-specific tool, and a lot of generic ratchet crimp tools will not do a good job on them. But at a pinch, I've had success with various tools for the few times I've used .093" crimps.

    I just used a non-insulated terminal crimp tool like HT-230CHT-230C (it is cheap, but totally the wrong tool, it is intended for uninsulated blade and ring crimps) and it crimps the wire portion just fine, but doesn't do a great job on the insulation grip portion, it leaves that too loose. So I redo the insulation portion using a non-ratchet tool (those are even cheaper). The end result works for me, and it pushes into the housing with no issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago in reply to dpenny

    The carrier strips are for machine feed, but should be totally removed, as Andrew mentions.

    If the crimping action using your tool has left the wire grip portion too wide to fit the housing, then it can be gently re-shaped after crimping using needle-nosed pliers. For insertion into the housing, 18 gauge wire is so thick it should be almost effortless to push the wire and terminal into the housing.

    It needs photos, otherwise there's not a lot to go on.

     

    Also, those .093" crimp pins/sockets use a Molex-specific tool, and a lot of generic ratchet crimp tools will not do a good job on them. But at a pinch, I've had success with various tools for the few times I've used .093" crimps.

    I just used a non-insulated terminal crimp tool like HT-230CHT-230C (it is cheap, but totally the wrong tool, it is intended for uninsulated blade and ring crimps) and it crimps the wire portion just fine, but doesn't do a great job on the insulation grip portion, it leaves that too loose. So I redo the insulation portion using a non-ratchet tool (those are even cheaper). The end result works for me, and it pushes into the housing with no issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dpenny
    0 dpenny over 5 years ago in reply to shabaz

    Hope I can figure how to add photo herein. First image comments.

    A. shows good crimp and flaps folded otherwise I cannot insert pin.

    B. shows flaps trimmed not yet folded. Tried 2 ways: without folding cannot insert pin, with folding pin pulls out of FRONT as I take apart male/female connectors.

    C. shows pins as purchased.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to dpenny

    The crimp terminals are also available individually, and they have that flap portion sticking out by about 0.5mm. So, by looking at your photo A, you're doing the right thing by manually trimming that flap and if you cannot cut it so closely, then folding in any remainder so that it's not contributing to the width of the terminal any more than 0.5-1mm max overall. In my photo in my other comment, you can see that the flaps are just slightly wider than the rest of the crimp terminal (measured even after crimping to be about 3.6 mm according to my calipers) and it slid in fine into the housing, and I heard the click when it locked.

    It looks like your photo A crimp should easily fully slide into the housing, and lock itself in permanently using the two side wings. If it comes back out, then examining the wings should reveal if the metal is buckling or not.

    There's a chance the Amazon crimps or housings are not genuine Molex (there's plenty of clones of electronic parts and connectors on Amazon and eBay) and might not be made to the same tolerances or of the same materials as genuine Molex.

     

    (By the way, you seem to have done a fine job with the crimp tool, just a small point is that the bare conductor length should be slightly longer than shown in the photo A, so that it's slightly visible egressing from the crimped portion, and also the wire insulation should be slightly visible from beyond the wire grip portion of the crimp terminal. But that's unrelated to the issue you're experiencing, it was just a minor comment).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer