Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need Help Interpreting Schematic and circuit design for L4971 DC to DC Switching Regulator
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 337 subscribers
  • Views 2402 views
  • Users 0 members are here
  • l4971_switching_regulator
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need Help Interpreting Schematic and circuit design for L4971 DC to DC Switching Regulator

jw0752
jw0752 over 6 years ago

I have recently been experimenting with the L4971 DC to DC Buck Switching Regulator IC.

 

http://www.farnell.com/datasheets/1689801.pdf?_ga=2.69477264.1687415617.1589140235-732132915.1579132131://

 

I discovered this IC chip when a number of them were salvaged from a power supply board. My question involves the interpretation of the unusual way that the schematic for a test circuit is drawn in the manufacturer's data sheet. (see above link) and the reason for this peculiar design feature.

 

Here is the schematic as drawn on page one of the L4971 data sheet:

 

image

 

As you can see the negative rail enters the schematic at the bottom left as is conventional and carries across the page to the bottom right. There are three components that connect directly to the negative rail and then a secondary negative rail is drawn from a connection at the bottom right and back towards the left onto which the ground connections from the chip itself as well as a couple of other components are attached.

 

The Data Sheet also provides a template for a circuit board:

 

image

 

The board does reflect the drawing of the schematic as it has two large negative rail pads on the upper and lower sections of the circuit board with a narrower, though still substantial, trace between them.

 

How does this particular design help the function of this switching regulator and why is it important enough to require the unusual reflection in the drawing of the schematic?

 

The Data sheet doesn't seem to cover this intricacy of the design. Any insights that anyone might have will be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +7 suggested
    As I mentioned I have built the circuit on a piece of perf-board this evening and here is what it looks like: The performance, compared to the bread board of last night, was excellent. Last night I was…
  • shabaz
    shabaz over 6 years ago +6 suggested
    Hi John, Usually that style schematic is done just to provide a signal to the PCB designer (since that person will be different to the electronics design engineer who will have drawn the schematic) to…
  • Andrew J
    Andrew J over 6 years ago in reply to jw0752 +4 suggested
    Hi John, pin7 is for frequency compensation at the error amplifier to try and stabilise the response during changes of external influences (input voltage, load changes etc.) good explanation here - the…
Parents
  • jw0752
    0 jw0752 over 6 years ago

    As I mentioned I have built the circuit on a piece of perf-board this evening and here is what it looks like:

     

    imageimage

     

    The performance, compared to the bread board of last night, was excellent. Last night I was very disappointed with the ability of the circuit to regulate as the load was increased. Tonight however the perf-board version was very stable. I began with the voltage set at 10.01 Volts and no load. When I got to 750 mA of load the voltage had only dropped by 30 millivolts. With the input voltage at 20 volts and the output set to 10 volts and 750 mA load I found that the efficiency was 90%.

     

    I have installed a resistive trimmer so that I can adjust the voltage output (Blue Trimmer in lower left corner). The trimmer gives me the ability to adjust the output from 3.3 volts up to about 21 volts as long as the input voltage is 400 mV above the output voltage. I was really surprised to find that there is only 0.4 volts dropout.

     

    I have one more question if anyone can help. The schematic doesn't show capacitor C3 but the board layout shows C3 between pin 7 of the L4971 and Ground. Pin 7 is used for external adjustment of the frequency of the switch. My board is currently running at about 100 kHz. What would be the purpose of C3 if they have left it off the schematic but included a place for it on the circuit board template?

     

    Thanks John

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to jw0752

    Hi John,

     

    pin7 is for frequency compensation at the error amplifier to try and stabilise the response during changes of external influences (input voltage, load changes etc.)

     

    good explanation here - the set up on the board is described towards the end.  It’s to help deal with noise on the output from just having the RC connection.  https://www.digikey.co.uk/en/articles/designing-compensator-networks-to-improve-switching-regulator-frequency-response

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Thank you very much for finding and linking the article on compensator networks. It will help me understand what is going on.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Thank you very much for finding and linking the article on compensator networks. It will help me understand what is going on.

     

    John

    • Cancel
    • Vote Up +3 Vote Down