I have a control panel for a fire suppression system and on the firing circuit output there is an LED with a .68k resistor
in parallel for testing. 24V when activated. What specs would the LED be?
Be sure to click 'more' and select 'suggest as answer'!
If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!
I have a control panel for a fire suppression system and on the firing circuit output there is an LED with a .68k resistor
in parallel for testing. 24V when activated. What specs would the LED be?
Typical LEDs turn on at a forward voltage around 2V and have a maximum current that they can tolerate without failing which is specified in the data sheet. Are you sure the resistor is in parallel? In a simple circuit where the current is controlled by a resistor they will be in series. Is it a single panel mounted LED? Please confirm the LED / resistor arrangement. Assuming the issue is the LED no longer lights was there something that occurred that might explain the failure?
EDIT: I have concerns about repairs on a safety system without understanding the circuit or cause of failure.
The LED when lit shows the circuit is working for test purposes and I believe that in both in parallel are also a dummy load as the circuit is monitored for faults.
The LED when lit shows the circuit is working for test purposes and I believe that in both in parallel are also a dummy load as the circuit is monitored for faults.