Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum LED
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 7 answers
  • Subscribers 302 subscribers
  • Views 1559 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

LED

vapyro
vapyro over 5 years ago

I have a control panel for a fire suppression system and on the firing circuit output there is an LED with a .68k resistor

in parallel for testing. 24V when activated. What specs would the LED be?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago in reply to vapyro +2
    If that resistor is really in parallel to present a load, the LED may have a built-in resistor. This would be the case if the voltage stays at 24V even with the LED in place. Such LEDs may be substituted…
  • shabaz
    shabaz over 5 years ago in reply to vapyro +1 suggested
    Hi Harry, There's not enough information, but I suspect it could be a current loop? If so, that's important information that was omitted. If the current system used an LED and resistor in parallel, then…
  • shabaz
    shabaz over 5 years ago in reply to shabaz +1
    Also, those photos were really unusable. Sharp, in-focus, showing color bands is important. Any mobile phone can do that, as long as there is decent lighting. Appreciate it may be hard to do that when…
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    Typical LEDs turn on at a forward voltage around 2V and have a maximum current that they can tolerate without failing which is specified in the data sheet.  Are you sure the resistor is in parallel?  In a simple circuit where the current is controlled by a resistor they will be in series.  Is it a single panel mounted LED? Please confirm the LED / resistor arrangement.  Assuming the issue is the LED no longer lights was there something that occurred that might explain the failure?

    EDIT:  I have concerns about repairs on a safety system without understanding the circuit or cause of failure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vapyro
    0 vapyro over 5 years ago in reply to fmilburn

    Try this photo. The bias is 2.7V and I tried a blue one with 2.6 bias that failed immediately.

     

     

     

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to vapyro

    I think the other comments are correct - the LED needs to be in series with the resistor.

    A 6.8K resistor would put about 3 mA through any LED if they were in series across 24V - which will illuminate most LEDs (fairly dimly).

    If you want to protect the LED from being inserted backwards, put a regular diode in series with both the LED and the resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 5 years ago in reply to vapyro

    I think the other comments are correct - the LED needs to be in series with the resistor.

    A 6.8K resistor would put about 3 mA through any LED if they were in series across 24V - which will illuminate most LEDs (fairly dimly).

    If you want to protect the LED from being inserted backwards, put a regular diode in series with both the LED and the resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer