Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Unorthodox application for small fans
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 11 answers
  • Subscribers 338 subscribers
  • Views 2264 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Unorthodox application for small fans

grlassin
grlassin over 5 years ago

Would appreciate some help for an unorthodox application of small fans. Was looking at small Delta Fans and found my way here.

The problem:

Condensation on a full, clear face shield on an ice hockey helmet due to warm air inside the shield (from breathing) and cooler air in the rink.

Plan is to use 2 small (30 mm or smaller) fans to create air flow inside the helmet with full face shield.

The shield has open vents for ventilation, some of which I covered on the inside with breathable N95 filter material (I can send photos).

Questions:

1. If the fans are placed against the breathable N95 material, will this strain the fan being directly against the N95 material?

2. Would it be better if the N95 material is repositioned on the outside of the shield, which would put the fan on the inside approx 5 mm - 6 mm away from the material?

3. What battery(ies) can power the fans?

As background, I am a 67 year old who plays regularly in a few ice hockey leagues.

One is over age 40, another over age 50 and another is all ages.

All hockey stopped in March due to Covid and restarted in June with various restrictions.

With 5 grandchildren, 3 who are under 1 years old, I did not play until this week and had to take extra precautions to mitigate the risk.

I played last weekend with the lower vents on the shield covered with breathable N95 material.

The shield is anti fog, and it didn't fog but it did build up water droplets of condensation on the inside due to my hot breathing and the colder rink air.

Same as fog, I could not see well.

My goal is to use the small fans to prevent condensation.

Greatly appreciate feedback as I am ready to buy some fans and fix this issue.

Thanks for all help.

image

 

image

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago in reply to jw0752 +5 suggested
    We had a mask design contest at work, so I experimented with a design that wouldn't fog glasses up. It turns out, it isn't that hard to achieve. The design conforms to the face under the glasses and all…
  • jw0752
    jw0752 over 5 years ago +4 suggested
    Hi Gary, I am very interested in what you work out. I walk everyday and here in Wisconsin in the Winter it gets cold enough so that I have to use a face covering and ski mask. The problem is I wear glasses…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to dougw +4 suggested
    dougw wrote: ... The design conforms to the face under the glasses and all the way up the bridge of the nose. And there is a slightly larger gap around the chin, which essentially provides a lower impedance…
Parents
  • dougw
    0 dougw over 5 years ago

    I am in a similar boat, except it is my glasses that fog up when playing hockey. My helmet face shield is a wire grid to help keep my glasses from fogging.

    I have tried many things over the years to combat the problem. Some work, some don't, none are perfect.

    I tried using fans, and they do work, but there are lots of drawbacks - size, weight, power supply, ducting, mounting, flow rates, ruggedness, etc.

    Our rules right now require a Covid mask be worn until the helmet has to be donned. A couple of players keep their Covid masks on during the game, but it really restricts the amount of oxygen you get.

    You might try a small blower instead of a fan - they generally produce higher pressure which is needed if you want to overcome the restriction of mask material.

    At work we make high end helmets with visors (not for hockey) and use a high tech permanent coating to eliminate fogging. This stuff works very well, way better than anything you can buy in a retail store, but is also very expensive. I wish I could afford to coat my glasses with it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 5 years ago

    I am in a similar boat, except it is my glasses that fog up when playing hockey. My helmet face shield is a wire grid to help keep my glasses from fogging.

    I have tried many things over the years to combat the problem. Some work, some don't, none are perfect.

    I tried using fans, and they do work, but there are lots of drawbacks - size, weight, power supply, ducting, mounting, flow rates, ruggedness, etc.

    Our rules right now require a Covid mask be worn until the helmet has to be donned. A couple of players keep their Covid masks on during the game, but it really restricts the amount of oxygen you get.

    You might try a small blower instead of a fan - they generally produce higher pressure which is needed if you want to overcome the restriction of mask material.

    At work we make high end helmets with visors (not for hockey) and use a high tech permanent coating to eliminate fogging. This stuff works very well, way better than anything you can buy in a retail store, but is also very expensive. I wish I could afford to coat my glasses with it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • grlassin
    0 grlassin over 5 years ago in reply to dougw

    Doug, In April, a few rinks reopened here with restrictions and players put masks on the outside of their mask or cage. I had a cage and did that and thought it was a great way to play and mitigate the risk. I tried wearing a mask and that was not possible. After playing 4 games, they could not find enough players who'd continue to wear any covering on the ice, but they still had to in the building. I stopped then until last Sunday night. I like the blower idea but will probably start with small fans and see how that works.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer