Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Unorthodox application for small fans
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 11 answers
  • Subscribers 338 subscribers
  • Views 2259 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Unorthodox application for small fans

grlassin
grlassin over 5 years ago

Would appreciate some help for an unorthodox application of small fans. Was looking at small Delta Fans and found my way here.

The problem:

Condensation on a full, clear face shield on an ice hockey helmet due to warm air inside the shield (from breathing) and cooler air in the rink.

Plan is to use 2 small (30 mm or smaller) fans to create air flow inside the helmet with full face shield.

The shield has open vents for ventilation, some of which I covered on the inside with breathable N95 filter material (I can send photos).

Questions:

1. If the fans are placed against the breathable N95 material, will this strain the fan being directly against the N95 material?

2. Would it be better if the N95 material is repositioned on the outside of the shield, which would put the fan on the inside approx 5 mm - 6 mm away from the material?

3. What battery(ies) can power the fans?

As background, I am a 67 year old who plays regularly in a few ice hockey leagues.

One is over age 40, another over age 50 and another is all ages.

All hockey stopped in March due to Covid and restarted in June with various restrictions.

With 5 grandchildren, 3 who are under 1 years old, I did not play until this week and had to take extra precautions to mitigate the risk.

I played last weekend with the lower vents on the shield covered with breathable N95 material.

The shield is anti fog, and it didn't fog but it did build up water droplets of condensation on the inside due to my hot breathing and the colder rink air.

Same as fog, I could not see well.

My goal is to use the small fans to prevent condensation.

Greatly appreciate feedback as I am ready to buy some fans and fix this issue.

Thanks for all help.

image

 

image

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago in reply to jw0752 +5 suggested
    We had a mask design contest at work, so I experimented with a design that wouldn't fog glasses up. It turns out, it isn't that hard to achieve. The design conforms to the face under the glasses and all…
  • jw0752
    jw0752 over 5 years ago +4 suggested
    Hi Gary, I am very interested in what you work out. I walk everyday and here in Wisconsin in the Winter it gets cold enough so that I have to use a face covering and ski mask. The problem is I wear glasses…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to dougw +4 suggested
    dougw wrote: ... The design conforms to the face under the glasses and all the way up the bridge of the nose. And there is a slightly larger gap around the chin, which essentially provides a lower impedance…
Parents
  • jw0752
    0 jw0752 over 5 years ago

    Hi Gary,

     

    I am very interested in what you work out. I walk everyday and here in Wisconsin in the Winter it gets cold enough so that I have to use a face covering and ski mask. The problem is I wear glasses and warm air from perspiration or a leak of exhaled air near the mask will fog the glasses or the mask shield. I have worked with pumps, pipes and all sorts of attempts to fix this problem. At this time I have a special breathing device that I have built where I inhale normally but then exhale into a tube that goes over my shoulders and out my back. I in effect have a tail pipe. In addition I have a small vacuum pump that I wear that can draw air out of the mask itself which is replaced with the very cold low humidity outside air. This system will work for me down to Zero Fahrenheit for about an hour. Winter will be here again in a couple months and I have started to try to come up with some improvements.

     

    I know what you are trying to do is different from my problem but there are enough similarities that I will share a couple things that I have learned. Adding technology to clothing and masks is cumbersome and uncomfortable. Fans consume power. You can look at the voltage and amperage rating of the fan that you hope to use. Divide the amperage rating of the fan into the Amp Hour rating of the battery you hope to use and you will have a rough idea of how long the fan will run. To work well the fan will either have to have a fresh air feed so that you are not just circulating more moist air. The other option is to heat the air or dry the air both of which have high energy costs or material costs. I can't imagine that the technology,(Fans, Wires, Batteries, Heaters, & etc) won't be more distracting than the loss of visibility.

     

    Since you are skating and moving with hockey I wonder if you could come up with some sort of air scope on the face shield that would direct air through the mask, though any filter would drastically cut the flow.  It would be nice if one could find some transparent wicking material that could carry the moisture away. In your situation you probably don't have to deal with frost or ice like I do but even a layer of water on an anti fog surface can distort and mess with your sight.

     

    I will be watching what others respond and I will continue to try to come up with some suggestions. I am hoping someone on the forum has some experience and suggestions beyond what I have come up with.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to jw0752

    We had a mask design contest at work, so I experimented with a design that wouldn't fog glasses up. It turns out, it isn't that hard to achieve. The design conforms to the face under the glasses and all the way up the bridge of the nose. And there is a slightly larger gap around the chin, which essentially provides a lower impedance for air flow down onto the neck than up to the glasses.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to dougw

    dougw  wrote:

     

    ... The design conforms to the face under the glasses and all the way up the bridge of the nose. And there is a slightly larger gap around the chin, which essentially provides a lower impedance for air flow down onto the neck than up to the glasses.

    Yes. One of my daughters wears glasses and has made a nose-contour fitting mask for herself. No more fogged glasses, even when cycling.

    Another temporary trick is to wash windshield or glasses in dishwash water. Then let them dry or shake dry without wiping.

    The detergent film that stays behind takes care that the damp does not create a blur on the surface. The moisture is still there but is transparant.

    With a good formula and some practice you can get by for a few hours. When sporting you may want to repeat the exercise during half-time.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to dougw

    Hi Doug,

     

    That sounds interesting. Do I have the resources to make one?

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to jw0752

    The glasses mask...

    You will need a needle and thread and your choice of cloth. The design does not need straps, so you don't need any elastic.

    The mask is held on with sleeves for the arms of the glasses and button holes for the nose pads on the glasses.

    I tried to make the colors look like Ironman, but my skills as a seamstress are below rudimentary.

    image

    The theme was "Even Ironman wears a mask".....

    image

    The red hoodie didn't help.

    Here is a rough (half-mask) template to get started, but it may need alterations for your face and more room at the chin equals less fogging .....

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to dougw

    Hi Doug,

     

    Thanks for the information. I believe I can put it together. The picture and the half pattern are good enough as I will have to measure to make it fit me properly anyway.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 5 years ago in reply to dougw

    Hi Doug,

     

    Thanks for the information. I believe I can put it together. The picture and the half pattern are good enough as I will have to measure to make it fit me properly anyway.

     

    John