Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using Heatsink to cool large volume of water
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 16 answers
  • Subscribers 338 subscribers
  • Views 13546 views
  • Users 0 members are here
  • heatsink
  • copper pipe
  • water
  • aluminium
  • radiator
  • cooling
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using Heatsink to cool large volume of water

sporkeh
sporkeh over 5 years ago

Hi everybody,

 

I'm currently trying to upgrade a cold water tank at my work.

We use this to cool down hot wax parts quickly.

Currently, its a plastic box with a large household radiator thrown in and copper pipes connecting to a constant flowing cold water source.

 

It works, however, a household radiator wasn't meant to be submerged and is quickly turning into a pile of rust.

 

So I'm looking into a variety of things, including making a whole new one. (new one will have insulated sides and top to try and keep the temp)

- one suggestion I had was to build a radiator into the skin of the tank, and then put some insulation on the outside, all of which would be a massive faf to make, and I'm not a radiator designer/engineer so I currently have no idea if that would work ether.

 

This tank is ~800 x 600 x 300mm and should hold ~140 liters of water, the current radiator is around 2200 BTU.

The room is kept at a constant 21 degrees, and the water comes in at about ~10 degrees iirc.

 

I've found a heatsink on farnell and wondered if it or something similar could be used (considering its just ally and copper, I could probably get a custom sized one made), but I have no idea if it would be suitable for this application.

 

I was originally thinking of just having copper pipe run around the inside of the tank, but a colleague mentioned that they tried to do a similar thing for a project at home and found that the copper pipes didn't do too much.

I'm not sure if there is something with the aluminium block along with the copper pipe that might work better, or if I can even get enough copper pipe in there for that kind of volume.

 

Is there anyone with a better understanding of thermal conductivity or any experience that could give me some advice?

Or maybe someone who has a spare one of these who might be able to do a simple/rough test? image

 

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago in reply to sporkeh +5 suggested
    Hi Henri, Here are the physics of your system. Thermal energy (heat) moves from warmer to colder. It can do this is three ways (1) by conduction where a hot area makes physical contact with a colder area…
  • dougw
    dougw over 5 years ago +4 suggested
    Those radiators are designed for liquid-to-air heat transfer where you need a large surface area on the air side. For liquid-to-liquid heat transfer I would expect simple copper tubing provides about the…
  • jw0752
    jw0752 over 5 years ago +4 suggested
    One other idea is to put a metal box within an outer box. Cold water is pumped into the outer box and surrounds the inner box. If you can elongate the shape of the box you will increase outer surface area…
Parents
  • sporkeh
    0 sporkeh over 5 years ago

    Thanks dougw and jw0752 for your replies;

     

    These wax parts get cast in metal, and can have very delicate sections, so they are easily damaged.

    Unfortunately, the water in the tank needs to be isolated, for a similar reason to having circulation, as there is a worry that too strong a blast of water could push the wax parts around the tank and damage them (some of them float, some are in metal setters which make them sink). This also could be an issue if any bits get sucked out causing a blockage, even with a filter on there I can guarantee someone won't notice and we'll end up flooding the shop-floor.

     

    I'm not too worried about keeping the tank circulated, as when in use, the water will be disturbed every couple of minutes from someone putting/removing something.

    -I've got a hot water tank as well without circulation, and that seems to be okay. I can always add circulation at a later date if its not enough though.

     

    I was thinking of pretty much a box inside a box to allow water to run around the outside, but I wasn't sure if it would work.

    My idea was to have the tank made from sheet metal, with the walls made up of 3 layers with a gap in between to allow the cold water to flow around;

    It would have an aluminium inner skin which contacts the water, thinking this will act like a heat storage, and then a copper skin outside of that which will be in contact with the aluminium and the cold water, thinking the copper will transfer the cold from the cold water and into the ally skin which will then disperse into the tank water. Finally a stainless steel outer skin which will protect it all.

    Hopefully the image below gives a decent idea of what I was thinking.

    We may also put some insulation on the outside of the tank to help reflect the cold into the tank.

    image

     

    The next idea would be to use copper piping to go around the sides of the tank, but actually in the water, and then have a 2-layer wall with a gap for insulation in the walls.

     

    The last idea would be to have some kind of heat sink or cooling device actually in the water to chill it that way, and still having an insulated wall.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • sporkeh
    0 sporkeh over 5 years ago

    Thanks dougw and jw0752 for your replies;

     

    These wax parts get cast in metal, and can have very delicate sections, so they are easily damaged.

    Unfortunately, the water in the tank needs to be isolated, for a similar reason to having circulation, as there is a worry that too strong a blast of water could push the wax parts around the tank and damage them (some of them float, some are in metal setters which make them sink). This also could be an issue if any bits get sucked out causing a blockage, even with a filter on there I can guarantee someone won't notice and we'll end up flooding the shop-floor.

     

    I'm not too worried about keeping the tank circulated, as when in use, the water will be disturbed every couple of minutes from someone putting/removing something.

    -I've got a hot water tank as well without circulation, and that seems to be okay. I can always add circulation at a later date if its not enough though.

     

    I was thinking of pretty much a box inside a box to allow water to run around the outside, but I wasn't sure if it would work.

    My idea was to have the tank made from sheet metal, with the walls made up of 3 layers with a gap in between to allow the cold water to flow around;

    It would have an aluminium inner skin which contacts the water, thinking this will act like a heat storage, and then a copper skin outside of that which will be in contact with the aluminium and the cold water, thinking the copper will transfer the cold from the cold water and into the ally skin which will then disperse into the tank water. Finally a stainless steel outer skin which will protect it all.

    Hopefully the image below gives a decent idea of what I was thinking.

    We may also put some insulation on the outside of the tank to help reflect the cold into the tank.

    image

     

    The next idea would be to use copper piping to go around the sides of the tank, but actually in the water, and then have a 2-layer wall with a gap for insulation in the walls.

     

    The last idea would be to have some kind of heat sink or cooling device actually in the water to chill it that way, and still having an insulated wall.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dougw
    0 dougw over 5 years ago in reply to sporkeh

    Your first idea is okay, but you don't need the extra copper layer - it actually reduces heat transfer. If you can't have water circulation, make the tank as skinny as possible so the heat has a minimum distance to travel to get to a cold wall. Also put feet on the inner tank so cold water can flow under it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to sporkeh

    Hi Henri,

     

    Here are the physics of your system. Thermal energy (heat) moves from warmer to colder. It can do this is three ways (1) by conduction where a hot area makes physical contact with a colder area. (2) by radiation where the Infrared radiation from a warm area escapes and is reabsorbed by a colder area. (3) Convection where differences in density caused by the relative temperatures causes fluids to move relative to each other in the Earth's gravitational field. From what you describe I think your best bet will be for the inner tank and outer tank to be made of the same metal. This will help to prevent any "galvanic" activity which can cause corrosion and deterioration of the metal of one of the tanks. The water between the tank should be kept moving so that the metal of the inner tank is constantly in contact with water that is colder than the water of the inner tank or at the desired equilibrium temperature. Heat will always flow from warmer to cooler. How quickly this happens depends on the difference in temperature  and the thermal resistance between the two areas. Left long enough the temperature of the warm area will nearly match the temperature of the cooler area. If there is no removal of heat from the outer layer they will meet at a temperature between the warm area temperature and the cold area temperature. Our replenishment and flowing of the water in the outer layer ensures that the final temperature of the water in the inner tank will approach the temperature of the water in the outer layer. The specific heat of wax is fairly low so it doesn't carry too much energy into the water. There is no way to reflect cold or to improve the flow of heat by introducing layers of metal between the warm area and the cold area. This would only likely introduce layers of still water which would act as an insulator and defeat your intention of moving heat energy from inside the water of the inner tank to the water of the outer tank. If there isn't a lower limit on the temperature of the water that you can use (other than the temperature of freezing) the colder that you can make the outer water relative to the temperature of the wax parts the quicker they will loose their thermal energy to the water. Many of the ideas that you mentioned are aimed at creating a greater temperature difference between the outer layer of water and the inner tank water. Don't forget that two different metals and an electrolyte (water and contaminates) can produce electricity and corrode one of the metals (galvanic effect). I learned this the hard way once and had a system where parts were miraculously dissolving on a regular schedule until I made all the parts of the same metal. One more thought, I understand that the wax forms are delicate but even a minuscule movement of the water in the inner tank will have a serious effect on the efficiency of the heat transfer.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sporkeh
    0 sporkeh over 5 years ago in reply to sporkeh

    Thanks for your input dougw, jw0752 & rstone

     

    Interesting about removing the extra copper layer, but what you say makes sense.

    Also interesting to hear about your galvanic experiences, there are electrics on the tank frame and so everything is grounded, however, I would imagine this would make that effect worse? in which case I will probably stick to Stainless Steel.

    I was planning on having the cold water flowing around the 4 sides + base and then there would be a lid for when its not in use.

    I can't make the sizing much smaller, as some of the parts we have only just fit, so I know I may struggle with a hot spot in the middle of the tank when the water is undisturbed, but if it becomes an issue, I can look into putting an eductor to add some movement.

     

    As for using parts from an AC or fridge, its been a while since I've looked at the back of my fridge, but I would imagine a fair few of the parts would rust, whether or not I could strip enough away whilst leaving the useful stuff is something I'd have to look at.

     

    The cold water around the tank will be constantly moving, it feeds straight from our water line, currently goes around the radiator, and goes back out, so its always fresh cold water, however I don't have any control over making it colder.

     

     

    I'll read this again in the morning after I've some time to think about it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to sporkeh

    I think you would do much better and simpler with a coil of copper pipe in the water. Run the cold water through the copper pipe. It will be well worth using some gentle pumping action to stir up the water in the tank, otherise you will tend to get a cold layer at the bottom (where I assume the copper coil would be.) Pretty much every domestic hot water system uses an indirectly heated water tank with a copper coil inside, through which hot water flows to heat up the water in the tank. The tank water comes out of the taps and the boiler water never mixes with it.

    Copper tube is easy to get from plumbing merchants, 25m of 8mm tube costs less than £50.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to sporkeh

    jw0752 is right, stainless steel will eventually galvanically erode the aluminum.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer