Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using Heatsink to cool large volume of water
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 16 answers
  • Subscribers 338 subscribers
  • Views 13541 views
  • Users 0 members are here
  • heatsink
  • copper pipe
  • water
  • aluminium
  • radiator
  • cooling
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using Heatsink to cool large volume of water

sporkeh
sporkeh over 5 years ago

Hi everybody,

 

I'm currently trying to upgrade a cold water tank at my work.

We use this to cool down hot wax parts quickly.

Currently, its a plastic box with a large household radiator thrown in and copper pipes connecting to a constant flowing cold water source.

 

It works, however, a household radiator wasn't meant to be submerged and is quickly turning into a pile of rust.

 

So I'm looking into a variety of things, including making a whole new one. (new one will have insulated sides and top to try and keep the temp)

- one suggestion I had was to build a radiator into the skin of the tank, and then put some insulation on the outside, all of which would be a massive faf to make, and I'm not a radiator designer/engineer so I currently have no idea if that would work ether.

 

This tank is ~800 x 600 x 300mm and should hold ~140 liters of water, the current radiator is around 2200 BTU.

The room is kept at a constant 21 degrees, and the water comes in at about ~10 degrees iirc.

 

I've found a heatsink on farnell and wondered if it or something similar could be used (considering its just ally and copper, I could probably get a custom sized one made), but I have no idea if it would be suitable for this application.

 

I was originally thinking of just having copper pipe run around the inside of the tank, but a colleague mentioned that they tried to do a similar thing for a project at home and found that the copper pipes didn't do too much.

I'm not sure if there is something with the aluminium block along with the copper pipe that might work better, or if I can even get enough copper pipe in there for that kind of volume.

 

Is there anyone with a better understanding of thermal conductivity or any experience that could give me some advice?

Or maybe someone who has a spare one of these who might be able to do a simple/rough test? image

 

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago in reply to sporkeh +5 suggested
    Hi Henri, Here are the physics of your system. Thermal energy (heat) moves from warmer to colder. It can do this is three ways (1) by conduction where a hot area makes physical contact with a colder area…
  • dougw
    dougw over 5 years ago +4 suggested
    Those radiators are designed for liquid-to-air heat transfer where you need a large surface area on the air side. For liquid-to-liquid heat transfer I would expect simple copper tubing provides about the…
  • jw0752
    jw0752 over 5 years ago +4 suggested
    One other idea is to put a metal box within an outer box. Cold water is pumped into the outer box and surrounds the inner box. If you can elongate the shape of the box you will increase outer surface area…
Parents
  • jw0752
    0 jw0752 over 5 years ago

    One other idea is to put a metal box within an outer box. Cold water is pumped into the outer box and surrounds the inner box. If you can elongate the shape of the box you will increase outer surface area for a given volume thus improving heat transfer. Water itself is a fairly good insulator of heat with a thermal conductivity of 0.6 W/m dot K. This means that if you put your heated wax in the center of the pool of water the heat will not quickly move to the cold sink. It will be a good idea to use a stirring mechanism as recommended by dougw as this will help a lot with the transfer of heated water to the colder sink. If you must put a radiator or heat sink in the water tank place it towards the top of the water surface so that the cold water produced will sink to the bottom and produce a convection current. Placing the radiator at the bottom will produce a stable cold to warm gradient from the bottom of the tank to the top.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 5 years ago

    One other idea is to put a metal box within an outer box. Cold water is pumped into the outer box and surrounds the inner box. If you can elongate the shape of the box you will increase outer surface area for a given volume thus improving heat transfer. Water itself is a fairly good insulator of heat with a thermal conductivity of 0.6 W/m dot K. This means that if you put your heated wax in the center of the pool of water the heat will not quickly move to the cold sink. It will be a good idea to use a stirring mechanism as recommended by dougw as this will help a lot with the transfer of heated water to the colder sink. If you must put a radiator or heat sink in the water tank place it towards the top of the water surface so that the cold water produced will sink to the bottom and produce a convection current. Placing the radiator at the bottom will produce a stable cold to warm gradient from the bottom of the tank to the top.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer