Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the best choice of LED to build a large (400mm) outdoor 7-segment display?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 339 subscribers
  • Views 5898 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the best choice of LED to build a large (400mm) outdoor 7-segment display?

line
line over 5 years ago

Having done a reasonable amount of research (clearly not enough) I'd value some assistance in selecting LEDs to make large 7-segment displays for outdoor use.

The application is for clocks/timers, with a viewing distance of 100m, reasonable viewing angle (ideally two displays at 90 degrees to provide near 180 degree viewing angle), for a product to run from mains (240Vac) or portable (12Vdc). Using two 7-segment characters for each display module.

Can anyone suggest either some suitable 7-segment displays (ready made - I can't find any) or LEDs suitable for making some bespoke displays?

Considerations include:

Brightness: How many lumens/mcd per segment are required for 100m visibility outdoors (full sunlight)?

Forward voltage: I expect to require higher than a 12V supply for the LED segment (daisy chain), using a boost converter to achieve the required voltages from a 12Vdc power source (battery) but it (Vf) needs to be reasonable.

Forward current: anticipate using constant current drivers to drive the LED segments, again needs to be reasonable (1w max).

Cost: each 7-segment display needs to be under £50 if buying and under £25 component cost if building, for the overall product cost to be viable.

Power: a consideration for the batteries - spec is four 7-segment displays (2 modules with 2 characters each) running for 6 hours of operation.

Heat: heat sink / heat management to avoid the LED junctions overheating (eg high power LEDs)

Viewing angles: In theory 90 degrees viewing angle per segment/display but in practice would the LED viewing angle need to be this high to achieve good/acceptable results across 180 degrees with two displays fixed 90 degrees to each other?

Quantity and arrangement of LEDs per segment?

If it helps (not much) a decimal point is not required - just the 7-segment characters.

 

If anyone has experience in this area and can offer some assistance\guidance it would be greatly appreciated.

With so many LEDs to choose from - you could save me a lot of pain and headache. Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 5 years ago +4 suggested
    Hello Matthew, Have you looked at using WS2812 strips also sometimes called Neopixels? I have seen several large 7 segment displays made from them - for example these made for a clock. There may be 12…
  • shabaz
    shabaz over 5 years ago +4 suggested
    Hi Matthew, Another option maybe worth considering is 'jumbotron' type panels. They are available from Aliexpress for under £25 each (google search for something like 'aliexpress P8 LED panel') and each…
  • fmilburn
    fmilburn over 5 years ago in reply to line +4 suggested
    I think the segments that are lit will be visible if there is sufficient contrast in color and / or brightness compared to the unlit ones. I have some and will try and do an experiment and capture the…
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    Hello Matthew,

     

    Have you looked at using WS2812 strips also sometimes called Neopixels?   I have seen several large 7 segment displays made from them - for example these made for a clock.  There may be 12 V versions, if not then a switching buck converter could be used to get 5 V

     

    edit: here is another one https://learn.adafruit.com/ninja-timer-giant-7-segment-display/overview

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • line
    0 line over 5 years ago in reply to fmilburn

    Hi Frank

    Thank you for the suggestion and a beautiful solution for indoor use but are these bright enough to be visible outdoors?

    Example: https://www.ukled.co.uk/led-strip-4-8w-m.html

    Spec quotes lumens per meter at 240lm.

    To construct a 400mm character, each segment would be 200mm long which is just 48lm.

    Sadly I don't think it would be visible in bright daylight from more than a few meters.

    I had come across the Ninja timer in my research - I think it's great (for indoors).

    I have been looking for suitable SMD devices - the viewing angles are great - but I haven't found the right combination of quantity, cost, power and brightness yet.

    What do you think?

    Regards Matthew

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to line

    I think the segments that are lit will be visible if there is sufficient contrast in color and / or brightness compared to the unlit ones.  I have some and will try and do an experiment and capture the results outdoors on my phone - but it is raining here at the moment and it may be a day or so before we get good weather.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 5 years ago in reply to line

    I think the segments that are lit will be visible if there is sufficient contrast in color and / or brightness compared to the unlit ones.  I have some and will try and do an experiment and capture the results outdoors on my phone - but it is raining here at the moment and it may be a day or so before we get good weather.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer