Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Is my 74HC08 bad?  (Weird results in Make: Electronics experiment 21)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 9 answers
  • Subscribers 337 subscribers
  • Views 5208 views
  • Users 0 members are here
  • make electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Is my 74HC08 bad?  (Weird results in Make: Electronics experiment 21)

opalko
opalko over 5 years ago

So I have built the "combination lock" from Charles Platt's Make: Electronics experiment 21 a couple of times now without getting it working correctly.  The schematic for the lock is below. The experiment is supposed to take a combination (pressing buttons E, F, G, H in order) to unlock the lock and provide power at the leads marked "to computer".  The buttons E, F, G, H are tied to a 74HC08 Quad AND chip with each button tied to an AND gate.  Each gate is unlocked in series by providing logical high as input from the previous button.  That is how it is supposed to work, but mine does not!  Using a logic probe, mine always has logic high on both inputs of button E so it seems to have no effect.  Pressing buttons F and G then unlock the circuit (sending high to H) which does not appear to need be pressed at all. One other weird thing is that I can occasionally start with a logical low at AND gate E if I disconnect and reconnect the green jumper tied to pin 2 on the 74HC08 from the 10K resistor to the same AND gate input, but not always.

 

I have taken the 74HC08 out and tried each AND gate separately and they all appear to work correctly independent of experiment 21.  But put it back into my circuit and logic high is always present on both inputs of the gate button E is attached to before I ever get started.  Do I just need another chip to try this with (I don't have one)?  Any help on how to troubleshoot further is appreciated!!  Note: I have removed switch A in mine as it was too much trouble to keep it pressed while troubleshooting and just substituted a jumper.

 

Regards,
Robert Opalko

Schematic

Circuit as built

Platt's image of how to build circuit

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +2 suggested
    Hi Robert, Check the voltage to ground on both sides of the 10K resistor that ties pin one to ground. This resistor should pull pin one low unless the E button is pushed. If it doesn't you probably have…
  • DAB
    DAB over 5 years ago +2 suggested
    The HC logic is very sensitive to levels so make sure each input has a pull up resistor so that they have a well defined state transition. It looked to me like there were some inputs directly attached…
  • dougw
    dougw over 5 years ago +2 suggested
    Logic gates can be unpredictable or undefined as power is applied to the circuit. If the gate output is even momentarily high during power up, it will latch up the gate in the high state. Pushing switch…
Parents
  • jw0752
    0 jw0752 over 5 years ago

    Hi Robert,

     

    Check the voltage to ground on both sides of the 10K resistor that ties pin one to ground. This resistor should pull pin one low unless the E button is pushed. If it doesn't you probably have a bad connection on the bread board.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • opalko
    0 opalko over 5 years ago in reply to jw0752

    John, thank you for this.  I checked the voltage to ground on both sides of the 10K resistor that ties pin one to ground and it read 5V on both ends!  I rebuilt this circuit a third time on a new & different mfr breadboard and still get the same result!  If that is not confusing enough,  if I remove the 1N4148 diode that ties pin 3 to pin 1 the +5V on pin one disappears and goes to 0!   What is going on?  I swapped out this diode with 3 others and still get +5V at pin 1.  This does not occur with the 1N4148 diode between pins 4 and 6.  I am soooo confused now!

     

    Boolean algebra is no sweat to me so I could move on to the next experiment but I really want to know why the diode is causing the +5V/logic high on pin 1!

    Thank you for any enlightenment!
    Robert Opalko

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • opalko
    0 opalko over 5 years ago in reply to jw0752

    John, thank you for this.  I checked the voltage to ground on both sides of the 10K resistor that ties pin one to ground and it read 5V on both ends!  I rebuilt this circuit a third time on a new & different mfr breadboard and still get the same result!  If that is not confusing enough,  if I remove the 1N4148 diode that ties pin 3 to pin 1 the +5V on pin one disappears and goes to 0!   What is going on?  I swapped out this diode with 3 others and still get +5V at pin 1.  This does not occur with the 1N4148 diode between pins 4 and 6.  I am soooo confused now!

     

    Boolean algebra is no sweat to me so I could move on to the next experiment but I really want to know why the diode is causing the +5V/logic high on pin 1!

    Thank you for any enlightenment!
    Robert Opalko

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 5 years ago in reply to opalko

    Hi Robert,

     

    Your experiment where you measured the voltage on both sides of the resistor that runs between Pin one and Pin seven shows that there is something wrong with your connection. The Blue wire in your picture that ties pin seven to the ground rail should also tie the 10 K resistor to ground. This would mean that this side of the resistor should read 0 volts with respect to ground. When key E is not pressed this path to ground should also pull Pin one low even if there is a small leakage through the diode. The diode looks to me like it is there to latch the gate that is tied to pins 1-2-3. Your problem from what we have discussed is that the side of the 10 K resistor that should be grounded just as pin 7 of the 74HC08 should be grounded is not or you would not have been able to read +5V on it.

     

    Take a deep breath and check everything again paying close attention to everything that is attached to the pin seven of the IC. These things that don't work are a much better learning experience than the situations where everything works. These are the challenges that actually teach electronics and not just how to plug things into a breadboard following a map. I like to buy cheap electronic kits from China and when they don't work which happens once in a while I have a lot more fun because then I get to troubleshoot and occasionally redesign a circuit.

     

    Keep trying and let me know what you find.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • opalko
    0 opalko over 5 years ago in reply to jw0752

    Ok, I am a little closer now but not quite there yet.  See my reply to Douglas Wong below! Thanks