Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Boosting a Frequency Generator Output
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 6 answers
  • Subscribers 337 subscribers
  • Views 7076 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Boosting a Frequency Generator Output

Andrew J
Andrew J over 5 years ago

My generator will output a 20Vp-p sine wave, resulting in a 7Vrms AC voltage (10V * 0.7)  I want to boost this to >=12Vrms AC and I thought an Op Amp would do that; if I use a gain of x2 that would suffice for my purpose.  The problem is I can't get it to work and I suspect I'm doing something stupid that I just can't see.  The Op Amp I have is a TI UA741

 

image

I don't care about quality nor if the signal is clipped - common mode input voltage range is +-13V at 15Vin and I could increase Vin to +-18V.  At the moment, I'm getting a wholly unexpected output which makes me think I'm doing something wrong.  I originally thought it was because I'd got the ground wrong but when I change the ground point of the Op Amp output to the Ground of the Function Generator, it still doesn't work AND channel 1 of the PSU oscillates between 0V and 32V! 

 

Is there a better way that I can do this with parts that I might have at hand?  Ultimately, I want to be able to variably alter the output voltage level to amounts < 12Vac and alter the frequency (hence why I thought using my frequency generator was a good idea)

  • Sign in to reply
  • Cancel

Top Replies

  • three-phase
    three-phase over 5 years ago +5 verified
    Hello Andrew, Some of my thoughts for you. Do you have the ground from the waveform generator connected to the ground for the op-amp? I would have thought all the grounds should be connected together,…
  • Andrew J
    Andrew J over 5 years ago in reply to shabaz +4
    Donald, Ralph: yes you were both right: 1K was too much of a load and it needed the generator -ve connecting to GNDREF. I'd wrongly assumed that would cause problems given that they belonged to two different…
  • michaelkellett
    michaelkellett over 5 years ago in reply to phoenixcomm +3 suggested
    phoenixcomm You're aiming for 115 * 5 = 575W minimum with a hope for double that. When I needed to do this last I bought a no name mega disco audio amplifier for about £200. It can manage about 1500W out…
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Andrew, the 741 (and some other old op-amps like TL0x1 series) behave weirdly enough outside their (often quite limited) specifications personally I try not to use them when experimenting, although they have their advantages like ultra-low cost.

    What frequency range do you want to work at?

    Another option (don't know if it is relevant though, depends on if you can find the part or not), is to find a transformer. It will solve any ground issues too, since the output will then be floating.

    If you're in the audio frequency range then if you can find a audio transformer (vintage equipment! maybe something from some NMOC stash?) that could be usable.

    Otherwise (say) R/Z1606 will work for about 500Hz upward in the audio range. It is 1:1, but with a centre tap secondary, so the secondary can be used as the primary, using half of the winding, so that it becomes 1:2 ratio.

    You won't be able to load it very much though. I think an audio transformer can be a great problem-solver for working with signal generators.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago in reply to shabaz

    Donald, Ralph: yes you were both right: 1K was too much of a load and it needed the generator -ve connecting to GNDREF.  I'd wrongly assumed that would cause problems given that they belonged to two different voltage sources.   By upping the PSU to +17V and -17V I can get 12.4Vac out of the op amp which is enough for my purposes.

     

    Shabaz: I'm not doing anything fancy, I literally want to be able to generate a 12Vac, 50Hz output and then reduce that voltage down and change the frequency, which is why I went with what I had to hand.  I do have some SMD op amps but those are +5V/-5V input so I was keeping my fingers crossed for the venerable UA741!  I keep getting warned off them but they're little troopers and always pull through in the end image  I want to test the specification of something that works at 12Vac and 50Hz.

     

    Thanks guys

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 5 years ago in reply to shabaz

    Donald, Ralph: yes you were both right: 1K was too much of a load and it needed the generator -ve connecting to GNDREF.  I'd wrongly assumed that would cause problems given that they belonged to two different voltage sources.   By upping the PSU to +17V and -17V I can get 12.4Vac out of the op amp which is enough for my purposes.

     

    Shabaz: I'm not doing anything fancy, I literally want to be able to generate a 12Vac, 50Hz output and then reduce that voltage down and change the frequency, which is why I went with what I had to hand.  I do have some SMD op amps but those are +5V/-5V input so I was keeping my fingers crossed for the venerable UA741!  I keep getting warned off them but they're little troopers and always pull through in the end image  I want to test the specification of something that works at 12Vac and 50Hz.

     

    Thanks guys

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • three-phase
    0 three-phase over 5 years ago in reply to Andrew J

    Good to hear you have to working. I believe that the resistor on the output of the amplifier should be in series with the load and is there to limit current if someone shorts out the output of the amplifier.

     

    Commoning out the ground references is usually required. As far the the electronics end is concerned, it isn't usually a problem. At the power end, it can be an issue if there is no isolation from the mains to the DC. When I built my high power AC PSU, I used some switchmode PSU boards to provide the DC rails, and of course they aren't isolated. So when I hooked up my waveform generator to the amplifier input, a not so nice current circulated around the waveform generator and PSUs.

     

    As MK has pointed out above, the easiest way to do this is to by a power amplifier, but not if you want to cut costs or build the circuit yourself.

     

    I guess the uA741 isn't the best, but as long as it can power the load and you aren't looking for any finesse, then I don't see any issues.

     

    Kind regards.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer