Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Flipping out on flip-flop basics
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 338 subscribers
  • Views 7962 views
  • Users 0 members are here
  • flipflop
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Flipping out on flip-flop basics

opalko
opalko over 5 years ago

Hey folks, I am working my way through Forrest Mims' Digital Logic Projects Workbook 2 and stumbling on understanding basic D-type flip-flop operations.  I hope someone can help me understand where I am getting lost.

 

Mims presents this explanation of a 4013 D-type flip flop:

image

which, as I understand it, on the rising edge of a clock pulse Q1 gets set when D is set.  (By the way, why does he use Q1 and Q2 in the truth table and Q and ~Q (I don't know how to write a Q with a line over it) in the schematic??).  He presents a basic flip flop circuit to demonstrate this :

image

Ok I get when you set D in this circuit with the toggle switch manually, Q1 gets set high (1) with the rising clock pulse!

 

Now the circuit I am working on:

image

The circuit works as it should, lighting up LED's 1,2,3,4 in sequence.  Ok.  However, when I put a logic probe on pin 5 of the 4013 (D1) with the rising clock pulse starting from 0, D1 is 0 (low) but Q1 is 1 (high). I don't understand why Q1 is set when D1 is low.  Here is the truth table I came up with but it seems to me from the truth table in the image at the top of this post, on rising clock pulse when D1 is 0, ~Q should get set to 1 (high).  I feel like I am missing the sequence of how the outputs get changed but I don't know what...  Help!

 

image

 

Thanks!

Robert Opalko

 

Message was edited by: Robert Opalko

 

Message was edited by: Robert Opalko

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago +7 verified
    The short answer is, that the ~Q output (pin2) is connected to the D input (pin5). When the rising edge happens and after the propagation delay of the flipflop the outputs toggle according to the D input…
  • gdstew
    gdstew over 5 years ago in reply to opalko +6 suggested
    Propagation delay, the amount of time an output (Q or ~Q) takes to change after a change in an input (D and clock) for 4000 series ICs is measured in 10s to 100s of nanoseconds depending on the operating…
  • dougw
    dougw over 5 years ago in reply to opalko +6 suggested
    As wolfgangfriedrich points out the FF is operating as it should. When the clock rising edge occurs whatever is at D gets latched to Q. In this case /Q gets latched as the inverse of Q, and it is connected…
Parents
  • wolfgangfriedrich
    0 wolfgangfriedrich over 5 years ago

    The short answer is, that the ~Q output (pin2) is connected to the D input (pin5). When the rising edge happens and after the propagation delay of the flipflop the outputs toggle according to the D input. When D is high, Q goes high and ~Q goes low, which loops back to the D input.

    The logic probe would not show this relationship as the prop delay is only some nanoseconds.

    The long answer would require a timing diagram.

    If you have an oscilloscope, look at the clock, D and Q,~Q signals and trigger on the clock.

    - W.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • opalko
    0 opalko over 5 years ago in reply to wolfgangfriedrich

    So D is going high before Q is getting set and I can't see that with the logic probe? If that is the case, is the truth table I constructed incorrect then?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 5 years ago in reply to opalko

    Propagation delay, the amount of time an output (Q or ~Q) takes to change after a change in an input (D and clock) for 4000 series ICs is measured in 10s to 100s of nanoseconds depending on the operating voltage. So without an

    oscilloscope or logic analyzer you will not be able to see any difference. There is also something called set up time which is the amount of time that the D input must be stable before the clock input makes a low to high transition

    and clocks in what is on the D pin. Also just a bit of clarification the D pin is not actually connected to the Q or ~Q pin, there are several logic gates in between that form the flip-flop. You might want to google CD4013 and look at

    the data sheet to get a better idea of what it takes to make a D type flip-flop.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 5 years ago in reply to opalko

    Propagation delay, the amount of time an output (Q or ~Q) takes to change after a change in an input (D and clock) for 4000 series ICs is measured in 10s to 100s of nanoseconds depending on the operating voltage. So without an

    oscilloscope or logic analyzer you will not be able to see any difference. There is also something called set up time which is the amount of time that the D input must be stable before the clock input makes a low to high transition

    and clocks in what is on the D pin. Also just a bit of clarification the D pin is not actually connected to the Q or ~Q pin, there are several logic gates in between that form the flip-flop. You might want to google CD4013 and look at

    the data sheet to get a better idea of what it takes to make a D type flip-flop.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer