Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum would it be possible to build a crt driver board from scratch or would the parts and information be to hard to source ?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 338 subscribers
  • Views 6495 views
  • Users 0 members are here
  • crt monitor
  • vintage crt repair
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

would it be possible to build a crt driver board from scratch or would the parts and information be to hard to source ?

retrofusion35
retrofusion35 over 5 years ago

hi i dont know much about crt tubes at all but im looking to build a crt arcade unit but alot of crt tvs and screens i find seem to be completly useless i was hoping there might allready be an option but would there be any point in trying to create a crt driver board or the deflector circut ? (to controll the yolk and electron gun )that accepts av and rgb inputs.

hoping this isnt a fools idea

  • Sign in to reply
  • Cancel

Top Replies

  • geralds
    geralds over 5 years ago +2 suggested
    I don't know your experience in electronics. The old CRT monitor has been obsolete for decades. There is no single chip in which you can build everything in one. Such a CRT monitor needs some 1000V, starting…
  • retrofusion35
    retrofusion35 over 5 years ago in reply to dougw +1
    hi yes i have seen people ad rgb to a standard crt tv but i think id rather go down the route of making a pcb for an existing jungle chip
  • retrofusion35
    retrofusion35 over 5 years ago in reply to wolfgangfriedrich +1
    hey thanks for the input but i have messed around with some lcds and emulators and to me at least it doesn't compare to original crt and hardware(plus that would be easy and a good project wont be easy…
  • vmate
    0 vmate over 5 years ago

    It is certainly possible, but I don't think it's worth the time, effort, and money put into it. An FPGA can easily handle the task of converting an input signal into the necessary outputs for the CRT, but you will need to build a bunch of high voltage logic as well that controls the CRT based on the FPGA's outputs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • retrofusion35
    0 retrofusion35 over 5 years ago in reply to vmate

    i like the thought but i think fpga programming lies outside my current abilities

    it probably would be one of the better options but it might not be the most pocket friendly option i think ill stick to reutilizing a chip from a crt and revise the pcb its mounted to

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 5 years ago

    I don't know your experience in electronics. The old CRT monitor has been obsolete for decades. There is no single chip in which you can build everything in one.

    Such a CRT monitor needs some 1000V, starting with R-G-B 12kV, so that the electron beam can be drawn onto the screen.

    Can you control that?

    Do you have the right knowledge? Have you measuring devices to set the various parameters?

    e.g. Black level, white level, geometry, anode current at 25kV, synchronization, etc ..?

    Building a VGA graphics card yourself is similarly complex.

    There used to be a VGA controller, the timing components, the memory and the power amplifier drivers were mounted around this controller.

    Then the software, etc.

    Now it's an ASIC and the memory with power amplifier ...

     

    Ok...

    Here is a little inspire, the video amplifier and the block diagram of an 17 inch RGB CRT monitor:

     

    Video amplifier:

    image

     

    Block diagram:

    image

     

    You can see, for that you need the x, y HV generator for the power deflection as well as the video data synchronisation.

    It is not easy to build it by "do it yourself".

    I wish you the best.

     

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<