Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Capacitor basics question(s)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 7 answers
  • Subscribers 339 subscribers
  • Views 4371 views
  • Users 0 members are here
  • oscillator
  • capacitor;
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Capacitor basics question(s)

opalko
opalko over 5 years ago

Hey again folks, just when I think I am getting somewhere I find something that makes me reevaluate if I have been learning image! So I am back with yet another question!

I was looking at making a "Simon" type toy from scratch using an Arduino and other components. I got the idea reading an early Ciarcia's Circuit Cellar circa 1980-81 where he made one of these and was thinking of doing it with more recent components.

 

Anyway, in the article he presents a schematic of the hardware tone generator he built for the game and I thought "Cool I can understand this!"... or so I thought lol!  What I am lost on is the charging of the capacitor in the oscillator circuit (below, and then a detailed view below that):

image

image

 

I studied this quite a while and realized I had seen it before in Forrest Mims' Digital Logic Projects:

image

and his explanation:

image

 

Where I am lost is how C1 (C in Ciarcia's circuit) is charging.  So two questions:

 

1) I would think the positive side of C1 would be accumulating positive charge, but if pin 4 is low then nothing is going to the positive side of C1?

 

2) The first answer in this discussion I found of this very circuit says "C1 will get charged through R1.By "charged" i mean lower terminal of C1 will get increasingly positive."  However, the "lower terminal" is the negative polarity side of the capacitor - so how is it accumulating a positive charge? Isn't putting a positive charge on the negative side of a capacitor a Very Bad Thing?

 

 

I know I am (again) missing something very basic here!  I have looked at this for 3 days now and not made progress...Thanks for any help on this!

Robert Opalko

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 5 years ago +6 suggested
    The two extremes of the circuit are shown below. For this capacitor, it must be non-polarized, that is, able to hold electrons or holes on either plate. Look at the top circuit, when the output of the…
  • jc2048
    jc2048 over 5 years ago in reply to opalko +5 suggested
    Here are a few examples of capacitor symbols from old books. This is from Troubleshooting Analog circuits by Robert Pease [1991]. The circuit is a simple voltage regulator. He uses a curved plate to denote…
  • gdstew
    gdstew over 5 years ago +4 suggested
    Hi, First these are non-polarized capacitors so they don't have positive or negative terminals. Polarized capacitors like electrolytic and tantalum do have positive and negative terminals and applying…
Parents
  • colporteur
    0 colporteur over 5 years ago

    I think I can see where the explanation and schematic could be confusing. Is the indication that capacitor C1 is a polarized introducing the confusion?

     

    However, the "lower terminal" is the negative polarity side of the capacitor - so how is it accumulating a positive charge?

     

    Are you interpreting the capacitor polarity as you would a battery? If a non-polarized capacitor symbol was used would you feel more at ease?

     

    If you view the polarization of a capacitor as a manufactures means to and ends would that help? The ratio of physical size to capacity is different in polarized and non-polarized capacitors. Polarized capacitors provide more capacity in a smaller size.

     

    MW's michaelwylie explanation of the function of the capacitor in the circuit is more appropriate. It ignores the capacitors polarization and views it just as a charge device. First the capacitor charges in one direction from a positive source and then in the alternate direction for a different positive source. That charge time is dependent on the capacitance and resistance in the circuit. You have a polarized capacitor here because it provides the charge capacity in a small size.

     

    That is not to say you ignore polarity on a polarized capacitor. Install them backwards in a power supply for example and they can explode launching them across a room [image I have done this].

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 5 years ago

    I think I can see where the explanation and schematic could be confusing. Is the indication that capacitor C1 is a polarized introducing the confusion?

     

    However, the "lower terminal" is the negative polarity side of the capacitor - so how is it accumulating a positive charge?

     

    Are you interpreting the capacitor polarity as you would a battery? If a non-polarized capacitor symbol was used would you feel more at ease?

     

    If you view the polarization of a capacitor as a manufactures means to and ends would that help? The ratio of physical size to capacity is different in polarized and non-polarized capacitors. Polarized capacitors provide more capacity in a smaller size.

     

    MW's michaelwylie explanation of the function of the capacitor in the circuit is more appropriate. It ignores the capacitors polarization and views it just as a charge device. First the capacitor charges in one direction from a positive source and then in the alternate direction for a different positive source. That charge time is dependent on the capacitance and resistance in the circuit. You have a polarized capacitor here because it provides the charge capacity in a small size.

     

    That is not to say you ignore polarity on a polarized capacitor. Install them backwards in a power supply for example and they can explode launching them across a room [image I have done this].

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer