Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for NPNs Array
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 304 subscribers
  • Views 561 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for NPNs Array

Former Member
Former Member over 15 years ago

Hello everybody.

 

I used NPN (BC817-25      from NXP) but i have now 15 NPN to only one board, i'd like to regroup every NPNs by NPN arrays.

 

My NPN pilot relays.

 

So, in fact, MCU drives NPN' base, there is each relay on rach collecter and all the emitter are connected to the ground.

 

Do you know what can i choose ? Because i don't find anything.

 

Thank you;

Regards,

 

Florent

  • Sign in to reply
  • Cancel
Parents
  • nickgray
    0 nickgray over 15 years ago

    I would suggest one of the MMPQ3904 or the MMPQ2222AMMPQ2222A. However, I offer some cautions. These devices may or may not work in your circuit because collector breakdown voltage on these is 40V compared with 45V for the BC317-25 and the forward current gain (beta) is a minimum of 100 (no maximum stated) at 10 mA for these compared with 160 to 400 at 100 mA for the BC317-25. You will have to make the evaluation for yourself as to whether these devices are satisfactory for your application.

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nickgray
    0 nickgray over 15 years ago

    I would suggest one of the MMPQ3904 or the MMPQ2222AMMPQ2222A. However, I offer some cautions. These devices may or may not work in your circuit because collector breakdown voltage on these is 40V compared with 45V for the BC317-25 and the forward current gain (beta) is a minimum of 100 (no maximum stated) at 10 mA for these compared with 160 to 400 at 100 mA for the BC317-25. You will have to make the evaluation for yourself as to whether these devices are satisfactory for your application.

    Good luck!