Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Remote Current Sensing
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 337 subscribers
  • Views 1372 views
  • Users 0 members are here
  • avr
  • current
  • sense
  • xbee
  • solenoid
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Remote Current Sensing

e14 Contributor
e14 Contributor over 14 years ago

I have all of a silly home project functional except for one piece of the puzzle. I'm over-building a remote doorbell for fun for our house. On the back patio, we can never hear the doorbell ring inside the house when guests come over, so I wanted to overdo it by putting a cool 6" brass bell on the back patio wall with a solenoid inside that would ding the bell when the doorbell was run. At first I was just going to hack apart an off-the-shelf setup, but that's just not as fun as using parts I have lying around.

 

I have set up two Xbee radios to do the wireless part. Works great. Simple. Not so cheap, but simple and they were available on my bench. I'm an AVR fan, so I used a couple of ATtiny24's I had sitting in the drawer for each end to make sure the communications was reliable and that the brass bell doesn't just randomly fire at all hours of the night. image

 

The part that I'm theorizing about is the sensor for the doorbell. I don't want to hack apart the actual button. Space is limited and I want the front door area to not look like the entrance to a mad scientist's lair. I'd like to do something more non-intrusive, like a current sensor. I want to use one of these to sense the current on the solenoid lines for the actual doorbell on the wall inside the house:

 

http://www.newark.com/allegro-microsystems/acs756kca-050b-pff-t/ic-linear-current-sensor-10ma-pff/dp/97M3899?in_merch=Popular%20Sensors

 

Does anyone who knows more about this amazing world of electronics fun (unlike me, the hobbyist hacker) know if this is a reasonable solution or if it would work well at all? It seems really cool to do it this way. It would also be kosher with my wife, whose only rule for me on this project (aside from the usual, "Don't burn down the house.") was (paraphrasing): "Do not destroy our doorbell." image

 

Recommendations or suggestions or a, "sure, that should do the trick" would be greatly appreciated!

 

Andy

  • Sign in to reply
  • Cancel
Parents
  • nlarson
    0 nlarson over 14 years ago

    This sounds really cool - I'm not technically inclined to answer if it will work or not with that part - but I'd love to see a video demo of the finished product! image

     

    Good luck!

    Nicole

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nlarson
    0 nlarson over 14 years ago

    This sounds really cool - I'm not technically inclined to answer if it will work or not with that part - but I'd love to see a video demo of the finished product! image

     

    Good luck!

    Nicole

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to nlarson

    Thanks! I always post articles (usually with videos and at least with photos) on my blog of all of the projects I build, no matter how silly they are. image I'll post a link to this discussion when the project is completed. Certain pieces of it are already posted on the blog and I think they reference this project.

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer