Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Student looking to create an energy harvesting circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 339 subscribers
  • Views 502 views
  • Users 0 members are here
  • harvesting
  • school
  • energy
  • sensor
  • beginner
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Student looking to create an energy harvesting circuit

e14 Contributor
e14 Contributor over 14 years ago
I am a student who is researching methods of "harvesting energy" through the means of a few electrical effects.  These include the piezoelectric effect, current generated in certain materials in response to pressure, and the thermoelectric effect, current generated in certain materials in response to a temperature differential.  I am looking to create some type of circuit that uses these principles to power something (a light or a small fan).  Can anyone suggest how I could go about doing this? I am looking at this (http://us.element14.com/peltier-elements) page for possible Peltier Elements to base the circuit around.  I am guessing from my limited knowledge on the subject that I will need something to translate the changing energy output of the thermoelectric device to a more constant (DC?) supply.  What do you think would be something reasonable to run off the Peltier Element?  Do you have suggestions as to what else I need to create a well running circuit to demonstrate the Thermoelectric Effect?
  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 14 years ago

    Josh,

     

    Where do you plan on using this Peltier energy harvester?

     

    Here is a circuit that is powered by a Peltier and senses temperature. Low power sensor applications would be a good use of the effect. The more of a difference in between two surfaces the better your project will work.

    image

    See more about this fully worked out project at Linear's site.

    Here is another.

     

    First of all, I recommend learning as much as you can about the Peltier. Build some projects that are already worked out, like the two above. Then, I would say, you know enough to venture out to build your unique project.

     

    I have a project idea for you to try in the future:

    Use the heat source from your furnace or water-heater to detect moisture on the basement floor. (If you live in a house.)

    Or a similar heat source for detecting window condensation. (For high-rise apartments, window moisture is an issue.)

     

    Cabe

    http://twitter.com/Cabe_e14
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 14 years ago

    Josh,

     

    Where do you plan on using this Peltier energy harvester?

     

    Here is a circuit that is powered by a Peltier and senses temperature. Low power sensor applications would be a good use of the effect. The more of a difference in between two surfaces the better your project will work.

    image

    See more about this fully worked out project at Linear's site.

    Here is another.

     

    First of all, I recommend learning as much as you can about the Peltier. Build some projects that are already worked out, like the two above. Then, I would say, you know enough to venture out to build your unique project.

     

    I have a project idea for you to try in the future:

    Use the heat source from your furnace or water-heater to detect moisture on the basement floor. (If you live in a house.)

    Or a similar heat source for detecting window condensation. (For high-rise apartments, window moisture is an issue.)

     

    Cabe

    http://twitter.com/Cabe_e14