Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Output Selector for a Bench Top Power Supply
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 317 subscribers
  • Views 607 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Output Selector for a Bench Top Power Supply

Former Member
Former Member over 13 years ago

Hi,

 

As one of my first build, I would like to build a power supply based on an ATX power supply. The output voltages are 3.3V, 5V, 12V and -12V. I was thinking of using two binding posts, one for ground and the other one for the voltage. I thought of using a rotary switch with 4 positions to select what type of current I want to output, is this a good idea?  Most seem to either support very low current (I guess I would need to go for an heavy duty one?) or have a ton of pins, I thought that 4 positions would only require something like 5 pins, 4 inputs and 1 output?

 

Thank you in advance

 

Eric

 

PS.: this is also my first post, so I hope it's in the right forum and I follow the guidelines image

  • Sign in to reply
  • Cancel
Parents
  • nermash
    0 nermash over 13 years ago

    IMHO it would be better to add separate binding posts for every voltage. Why? Because then you can use all 4 outputs at the same time or powering the same project. For example, 5V for some logic, 3.3V for microcontroller, +12 and -12 for opamp. Just be carefull, these psus can pump out some serious currents. It likely won't kill you but it can burn you badly...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nermash
    0 nermash over 13 years ago

    IMHO it would be better to add separate binding posts for every voltage. Why? Because then you can use all 4 outputs at the same time or powering the same project. For example, 5V for some logic, 3.3V for microcontroller, +12 and -12 for opamp. Just be carefull, these psus can pump out some serious currents. It likely won't kill you but it can burn you badly...