Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Converting a rotisserie oven into a coffee roaster
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 339 subscribers
  • Views 1574 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Converting a rotisserie oven into a coffee roaster

e14 Contributor
e14 Contributor over 13 years ago

I want to add a PID Temp controller to a Hamilton Beach rotisserie (toaster) oven to get better temperature control and thus get best possible coffee bean roast. I am not an engineer of any sort by I know some of the basics and how to solder AND I know how to follow directions. I want to be sure I wire this PID correctly. the closest example I found was the website here: http://www.die4laser.com/toaster/index.html

 

Would it be as simple as inserting the PID in place of the timer? Is there a need for an SSR? What other things should I consider? I do intend on adding some insulation to lower heat loss.

Any help greatly appreciated. Thank you.image

 

I tinker with a lot of things but sadly not an expert at anything.

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 13 years ago

    Randall,

     

    How do you foresee using a PID controller to handle temperature?

    What is ideal for a coffee bean?

    Depending on the variety of answers, a simple temperature sensor and relay/switch may be all you need.

     

    Otherwise,  may have to suggest moving towards a different option. A small microcontroller may be a better bet. And it is easy to setup, don't worry.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Catwell

    The temp setting only goes up to 450. I need to better regulate that temp as well as see what the temp actually is so I can keep track of each roast and hopefully get a better roast. In my original post I found that die4laser site where the guy used the PID in the toaster oven. I thought since the rotisserie is similar maybe I could do the same thing. I already ordered one (with thermocouple). I also intend on adding some insulation to cut down on heat loss. In ideal cooking situation for a coffee bean, it needs to reach an internal temp of about 425-430 degrees F. The roast cycle should be in about 20-30 minutes. Right now it takes about 50-60. Let's just say this doesn't make the coffee right now.

     

    Anyway, I could just insert the PID into the circuit in place of the timer like the other guy did with his toaster oven. I wanted another opinion. As far as I know, it could work but maybe I need to do something a little different like add a solid state relay like int the mod done on element 14. If there is something else I should do, I'm open. Thank you for your help.

     

    Message was edited by: Randall Bowman

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Catwell

    The temp setting only goes up to 450. I need to better regulate that temp as well as see what the temp actually is so I can keep track of each roast and hopefully get a better roast. In my original post I found that die4laser site where the guy used the PID in the toaster oven. I thought since the rotisserie is similar maybe I could do the same thing. I already ordered one (with thermocouple). I also intend on adding some insulation to cut down on heat loss. In ideal cooking situation for a coffee bean, it needs to reach an internal temp of about 425-430 degrees F. The roast cycle should be in about 20-30 minutes. Right now it takes about 50-60. Let's just say this doesn't make the coffee right now.

     

    Anyway, I could just insert the PID into the circuit in place of the timer like the other guy did with his toaster oven. I wanted another opinion. As far as I know, it could work but maybe I need to do something a little different like add a solid state relay like int the mod done on element 14. If there is something else I should do, I'm open. Thank you for your help.

     

    Message was edited by: Randall Bowman

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    *bump*