Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Multiplexer for Pi Camera Module
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 302 subscribers
  • Views 694 views
  • Users 0 members are here
  • video_switching
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Multiplexer for Pi Camera Module

rboone2020
rboone2020 over 12 years ago

Hello,

 

I am new to element14, and appreciate your help.   I am a wildlife ecologist interested in surveying wildlife and livestock.   I am experimenting with a Raspberry Pi with a camera and a stepper motor to take panoramic images every minute or so.  Enjoying the process, but ...

 

Ideally I would prefer a solid state solution.   I would like to connect 8 Pi cameras to a single computer.   **I do not need signal from all of them at the same time**   I just need to pole each camera in turn.   I think I need a multiplexer, but a design ... or even the chip in question ... is beyond me.   Do you have any pointers?   Are there places on the web where I might contract with a designer for an embarrassingly small amount of money to help out?

 

As I say, new to the community.  If this post is misplaced, pardon.

 

Thanks,

Randy

  • Sign in to reply
  • Cancel
Parents
  • rboone2020
    0 rboone2020 over 12 years ago

    Hi,

     

    It seems I've stumped folks.   The technical question aside, is there a good place on the web to post requests for design assistance?

     

    Thanks,

    Randy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to rboone2020

    Hi Randall,

     

    This is quite some work, because the cameras operate at high speed, and without a lot of knowledge of what is going on, perhaps an FPGA or CPLD might be the route you may want to pursue - just guessing though, I am not knowledgeable on the camera. It may be LVDS interface to the camera, so then you need a device with LVDS capability. It would need a custom board made too (you couldn't use prototyping board). So, it is a fair amount of work for an Engineer, maybe several weeks : ( I'm not sure there is anything existing that could be re-used to reduce the amount of development. I don't know if the circuit diags are published for the camera - if they are, that may help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago in reply to rboone2020

    Hi Randall,

     

    This is quite some work, because the cameras operate at high speed, and without a lot of knowledge of what is going on, perhaps an FPGA or CPLD might be the route you may want to pursue - just guessing though, I am not knowledgeable on the camera. It may be LVDS interface to the camera, so then you need a device with LVDS capability. It would need a custom board made too (you couldn't use prototyping board). So, it is a fair amount of work for an Engineer, maybe several weeks : ( I'm not sure there is anything existing that could be re-used to reduce the amount of development. I don't know if the circuit diags are published for the camera - if they are, that may help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • rboone2020
    0 rboone2020 over 12 years ago in reply to shabaz

    Ah, I see.   Thank you for the reply and information, Shabaz.   The camera uses a standard format (CSI) and schematics are available, but it sounds like, for the time being, that my experiments with stepper motors are the way to proceed.  That said, hope springs eternal!   Perhaps something will become available that I and others may use.

     

    Thanks again,

    Randy