Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum power LED's
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Subscribers 342 subscribers
  • Views 2914 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

power LED's

greenwald1818
greenwald1818 over 12 years ago

hi,

     I was wondering, im building a raspberry pi laptop, and I need a way to tell if the battery is low. so, what part would I need to get if I get 2 LED'S, and I want the blue one to be on if the battery is full and the amber one to be on if it gets below 4.5 volts (with a 7.5 volt battery) OR if I have a multi-colored one how would I do it if the same thing applies except with a multi colored one. thx in advanced.

  • Sign in to reply
  • Cancel

Top Replies

  • saurocksall
    saurocksall over 12 years ago +1 verified
    Hi Alex, I have found the circuit that will help you , it uses The LM 3914 it has ten comparators, which are internally assembled in the voltage divider network based on the current-division rule. So it…
  • greenwald1818
    greenwald1818 over 12 years ago in reply to saurocksall +1
    what is the ic1 LM3914
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Alex,

     

    This type of thing is possible to implement using comparator ICs and a voltage reference. For example, see the datasheet for LM3915 which has a block diagram of the type of circuitry that would do what you need. Another alternative - if you're using something like an Arduino as part of your build - would be to use one of the ADC channels to monitor a fraction of the supply voltage and control the LEDs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago

    Hi Alex,

     

    This type of thing is possible to implement using comparator ICs and a voltage reference. For example, see the datasheet for LM3915 which has a block diagram of the type of circuitry that would do what you need. Another alternative - if you're using something like an Arduino as part of your build - would be to use one of the ADC channels to monitor a fraction of the supply voltage and control the LEDs.