Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Polarity Switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 305 subscribers
  • Views 1249 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Polarity Switch

Former Member
Former Member over 11 years ago

Dear All,

 

I am in searching for a solution which switches input power polarities.

 

Story: My car window regulator (together with the driving motor and the control module) is broken and I've ordered a new one which is a bit different than the original one. The new regulator has no control module, only a motor with 2 power cable (+/-); the car provides a wiring harness has one +12v output and two grounds, depending on the button you pulled or pushed, either of the grounds closed to complete the circuit. The original regulator control module will automatically switch the polarity to drive the motor up or down accordingly. However, the new one has no control module to do this.

 

Current Planning Solution: I am planning to utilize two relays and two MOSFETs to make such 'Polarity Switch' and here is the circuit diagram I've drawn. I haven't tested it yet (components are on their way from Element14 to me).

 

Question 1: Could anyone examine my circuit to find out whether it will work? If it does, will it still work if I replace the relay with straight wire?

 

Question 2: because of the relays, I am really not too confident about the reliability. Is there any other way to complete this 'polarity switching' purpose?

 

If it helps, the max voltage supplied is 15v (when the alternator is running), the fuse that is used for front window is 30A (maybe it's for both front window), so I assume that the max current draw is less than 30A.

 

Thanks for any input!

 

psw

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago

    image

    How about this circuit. It would allow your switches to run relays which in turn would power the window up or down. This assumes that there are limit switches in the motor unit that will stop the window at top and bottom of travel. This way we eliminate the MOSFETs that were just confusing things.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    image

    How about this circuit. It would allow your switches to run relays which in turn would power the window up or down. This assumes that there are limit switches in the motor unit that will stop the window at top and bottom of travel. This way we eliminate the MOSFETs that were just confusing things.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to jw0752

    It's Perfect! It's simple and effective!

     

    Although I haven't try it yet, I have strong feeling that this will work.

     

    Just ordered the some new relays. I will post back when I test this.

     

    Thanks!