Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum USB Scanner
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 302 subscribers
  • Views 560 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

USB Scanner

Former Member
Former Member over 11 years ago

I am currently doing a project with opticard 821 (Scanner). I want to include a external switch to Arduino. When the switch is press, the scanner will then operate and then save the image in a SD card. Both the scanner and the Arduino are connected to computer. The scanner appear under imaging device while Arduino is under port at the device manager.  Is there a way I can control it using Arduino board and how can I go about doing it?

  • Sign in to reply
  • Cancel
Parents
  • hawkeyethehacker
    0 hawkeyethehacker over 11 years ago

    Arduino - ArduinoUSBHostShield should solve the issue of getting a USB Port for the scanner to connect to, however I am unsure about how you would read the input, as it likely requires proprietary drivers which wont function on an Arduino.

    In this case, a Raspberry Pi might be better as there is more chance of a working driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hawkeyethehacker
    0 hawkeyethehacker over 11 years ago

    Arduino - ArduinoUSBHostShield should solve the issue of getting a USB Port for the scanner to connect to, however I am unsure about how you would read the input, as it likely requires proprietary drivers which wont function on an Arduino.

    In this case, a Raspberry Pi might be better as there is more chance of a working driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to hawkeyethehacker

    What if both the scanner and Arduino is connected to the same computer, is there a sample code for Arduino such that it can command the scanner to scan?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hawkeyethehacker
    0 hawkeyethehacker over 11 years ago in reply to Former Member

    Oh, you wish for a computer in between the two? The way I would do it is write an application for the PC that checks SPI (Serial) data from the Arduino. The Arduino application can write to serial whenever the button is pushed, the PC application reads it and does whatever it needs to do to make the scanner scan.

     

    I do not believe there is sample code but if you have a look at Serial examples for the Arduino it may point you in the right direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to hawkeyethehacker

    Yes both the computer and arduino is connected to the same computer. Below is a sample code I have done. I am not sure what is the code for the scan function. Is there also any header for me to include? Please help me with the coding.

     

    -------------------------------------------------------------------------------------------------------------------------------------------

                                                                                                                                              

    void setup(){                                                                                                                         

      Serial.begin(9600);

      pinMode(10,INPUT);//connect switch to pin 10 of arduino

    }

    void loop(){

      if (digitalRead(10) == HIGH){

        scan()://call the function to scan

      }

      else{

      }

      delay(1000); //delay for 1ms

    }

     

    void scan(){

      /*

      This is the part where I am unsure. Both the scanner and arduino is

      connected to the same computer. How can I ask the device to do the

      scanning

      */

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hawkeyethehacker
    0 hawkeyethehacker over 11 years ago in reply to Former Member

    I'll see what I can do.