Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum led driver circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 320 subscribers
  • Views 4312 views
  • Users 0 members are here
  • led
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

led driver circuit

terrenone
terrenone over 11 years ago

I need some help with a circuit I need to drive 10 white leds from a 3.7v 2200mAh lipo battery it sounds simple but it has to be able to fit in a small container aproximity 1inch square and not produce a lot of heat,  its for my son's night im making.


Any help is welcome

Thanks

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    In this case I would be tempted to replace the 10 LEDs with a single 1 or 3W LED, it will fit easier and can be driven from the 3.7V LIPO with a simple constant current generator with minimal power loss…
  • jw0752
    jw0752 over 11 years ago in reply to terrenone +1
    That sounds good Dave. The battery and charging question is resolved. Let me know how your testing of the 5mm LEDs go on the 3.7Volt source. Since you are going to be dealing with relatively low mA I do…
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes +1
    Hi Peter - Whenever I try to answer one of these questions I am always pleased when one of the fellows, like yourself, with more knowledge and experience add their insight. I have come back to your recommendation…
Parents
  • terrenone
    0 terrenone over 11 years ago

    I have a basic multi meter, bread board, soldering iron and perf board.

    I have a led work lamp which has a broken case like this, https://www.torchstar.biz/detail.php?id=820 it has a battery cut off and charge circuit built on to the control board could this be used??

    and i was hoping to replace the led bar with individual leds

     

    i was going to build a car shaped night light out of an old rc car

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to terrenone


    Hi Dave - I do not have enough information to tell you. The LiPo battery that you mentioned, does it come from the work lamp so that it is matched to the charge circuit? You will have to perform the experiments on the individual LEDs or go with the single brighter LED as outlined by Peter. Are you replacing the work lamp LED strip as it is too bright and concentrated to make a good night light? I hope you can make this work as it seems like a project your son will really like.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terrenone
    0 terrenone over 11 years ago in reply to jw0752

    Hi John, yes the Lipo came from the work lamp i fingered it would be better to use the circuit and battery together than use the battery on it own and charge it separately.

    your right about the Led bar when it tested it, it practically lit up the entire bedroom

    so i decided to go with the 5mm white leds, just so they will fit in to the car

     

    thanks

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to terrenone


    That sounds good Dave. The battery and charging question is resolved. Let me know how your testing of the 5mm LEDs go on the 3.7Volt source.  Since you are going to be dealing with relatively low mA I do not think there will be any problems with heat or a large impact from using resistors to limit the current as opposed to using the current generator circuit that Peter mentioned. It just depends how fancy you want to get.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to terrenone


    That sounds good Dave. The battery and charging question is resolved. Let me know how your testing of the 5mm LEDs go on the 3.7Volt source.  Since you are going to be dealing with relatively low mA I do not think there will be any problems with heat or a large impact from using resistors to limit the current as opposed to using the current generator circuit that Peter mentioned. It just depends how fancy you want to get.

    John