Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help Using WS2811 to drive 12v RGB LED strip
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 41 replies
  • Answers 11 answers
  • Subscribers 345 subscribers
  • Views 12971 views
  • Users 0 members are here
  • driver
  • mosfet
  • strip
  • led
  • ws2811
  • rgb
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help Using WS2811 to drive 12v RGB LED strip

dmilton2004
dmilton2004 over 11 years ago

Greetings all,

 

I am creating a lighting project that I want to have a wall display with large (15" x 20") panels and each panel acts as its own "pixel" (controlled by one WS2811).

 

I had purchased 12v RGB LED strips with 30 LEDs per meter. What I want do is control a section of the RGB strip (about 15 LEDs). I have been scouring the web for possible solutions. One avenue I was looking at was using MOSFETs to drive the strip from the PWM outputs from the WS2811. There is an example in the WS2811 datasheet that shows using 3 LEDs per color with 12v. I do know that the WS2811 is a constant current source device. My thought was to use a logic level N-channel MOSFET to drive the LED strip. This is just based upon the research that I have done. What I have not found was any schematic to go from. I am looking at possible 3 MOSFETs per WS2811.

 

Any help and schematics would greatly help!

 

Thanks in advance!

 

Don

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +3 suggested
    I was able to make this work by using a simple NOT gate between the WS2811 chip and the mosfet. I believe this works because it is using TTL (transistor based logic). The WS2811 requires some kind of load…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to michaelkellett +2
    More LEDS in series means less current, thinner wires and a single switch, so 12V = 3-4 LEDS per channel, using a chip like ULN2003 will provide all the drive for a single board probably Using logic levels…
  • dmilton2004
    dmilton2004 over 11 years ago in reply to dragonstyne +2 suggested
    Thanks Steve. I have not tried to trigger the MOSFETs yet, but that was my next plan. I should be able to do that by applying +5v to the Gate and connecting the Source to GND. I should see voltage flow…
Parents
  • ipdotsetaf
    0 ipdotsetaf over 6 years ago

    hey there

     

    i know this question was on 2014 but i'll answer any wayimage

    the thing is that i had the same idea and wanted to do some thing like this cuple of weeks ago BUT i actually knew that it is imposible to connect the ws2811 ic directly to mosfets

    and thats because the pwm input signals of the mosfet (0-5v usually) are different from the output pwm signal of a ws2811

    to fix that you can basically use a rgb amplifier witch are preaty cheap OR you can make your own rgb amplifier

    i found a picture taken from one of these amplifiers and its basicaly a inverting op-amp (LM324 witch has 4 op-amps inside) and three n-channel mosfets (in this case A2sHB)

    the op amp translates the pwm signal and the mosfets amplify each r, g and b channels

     

     

    link to the rgb ampifier page ::

    https://perso.aquilenet.fr/~sven337/english/2015/01/19/Tearing-down-a-RGB-LED-strip-amplifier.html

     

    i'am also planning to create something similar so i'd be happy to know that if you could completed the project ? if so, how was the results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • theriddler
    0 theriddler over 6 years ago in reply to ipdotsetaf

    You can use a ws2811 with either a fet or Darlington ic. You need to replace the led with pull up resistors ,10k on a 5 volt setup will work

    run the output from the rgb of the ws2811 into a 74ls04 hex inverter .. you can then drive a fet ( make sure you have a 1k resistor on the output of the hex inverter to limit current ) or drive a Darlington IC .. no current limiting resistor required

    for this.. the trick to get the output of the ws2811 to swing logic high and low when it uses current limiting to drive the LED ( in this case about 18.5 mA) is to use  pull up resistors on the rgb output . Otherwise the output of the 2811 floats

    I have assembled a 11 channel board to drive standard RGB strips

    ws2811. —-> 74ls04 —> uln2003

    its is limited to 500mA per colour which was s fine for what my use was for ( about 1 m of rgb led strip )

     

    https://ibb.co/tYFWf4y

    https://ibb.co/G9gYxyx

     

    I did design and build the board without any prototyping when I decided to read the ws2811 data sheet to find that the output was current limiting .. the design does work without the pull up resistors , however if you want to keep the input a clean square wave for the hex inverter I will be fitting them into the led footprints instead of the LED .. installing the LEDs on the control board does stuff things up as I over looked the vcc to the led needs to have the current draw limited with a 100ohm resistor .. either way I dont need the led onboard as a reference but instead putting 10k resistors in place

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • theriddler
    0 theriddler over 6 years ago in reply to ipdotsetaf

    You can use a ws2811 with either a fet or Darlington ic. You need to replace the led with pull up resistors ,10k on a 5 volt setup will work

    run the output from the rgb of the ws2811 into a 74ls04 hex inverter .. you can then drive a fet ( make sure you have a 1k resistor on the output of the hex inverter to limit current ) or drive a Darlington IC .. no current limiting resistor required

    for this.. the trick to get the output of the ws2811 to swing logic high and low when it uses current limiting to drive the LED ( in this case about 18.5 mA) is to use  pull up resistors on the rgb output . Otherwise the output of the 2811 floats

    I have assembled a 11 channel board to drive standard RGB strips

    ws2811. —-> 74ls04 —> uln2003

    its is limited to 500mA per colour which was s fine for what my use was for ( about 1 m of rgb led strip )

     

    https://ibb.co/tYFWf4y

    https://ibb.co/G9gYxyx

     

    I did design and build the board without any prototyping when I decided to read the ws2811 data sheet to find that the output was current limiting .. the design does work without the pull up resistors , however if you want to keep the input a clean square wave for the hex inverter I will be fitting them into the led footprints instead of the LED .. installing the LEDs on the control board does stuff things up as I over looked the vcc to the led needs to have the current draw limited with a 100ohm resistor .. either way I dont need the led onboard as a reference but instead putting 10k resistors in place

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer