Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help Using WS2811 to drive 12v RGB LED strip
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 41 replies
  • Answers 11 answers
  • Subscribers 345 subscribers
  • Views 12951 views
  • Users 0 members are here
  • driver
  • mosfet
  • strip
  • led
  • ws2811
  • rgb
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help Using WS2811 to drive 12v RGB LED strip

dmilton2004
dmilton2004 over 11 years ago

Greetings all,

 

I am creating a lighting project that I want to have a wall display with large (15" x 20") panels and each panel acts as its own "pixel" (controlled by one WS2811).

 

I had purchased 12v RGB LED strips with 30 LEDs per meter. What I want do is control a section of the RGB strip (about 15 LEDs). I have been scouring the web for possible solutions. One avenue I was looking at was using MOSFETs to drive the strip from the PWM outputs from the WS2811. There is an example in the WS2811 datasheet that shows using 3 LEDs per color with 12v. I do know that the WS2811 is a constant current source device. My thought was to use a logic level N-channel MOSFET to drive the LED strip. This is just based upon the research that I have done. What I have not found was any schematic to go from. I am looking at possible 3 MOSFETs per WS2811.

 

Any help and schematics would greatly help!

 

Thanks in advance!

 

Don

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +3 suggested
    I was able to make this work by using a simple NOT gate between the WS2811 chip and the mosfet. I believe this works because it is using TTL (transistor based logic). The WS2811 requires some kind of load…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to michaelkellett +2
    More LEDS in series means less current, thinner wires and a single switch, so 12V = 3-4 LEDS per channel, using a chip like ULN2003 will provide all the drive for a single board probably Using logic levels…
  • dmilton2004
    dmilton2004 over 11 years ago in reply to dragonstyne +2 suggested
    Thanks Steve. I have not tried to trigger the MOSFETs yet, but that was my next plan. I should be able to do that by applying +5v to the Gate and connecting the Source to GND. I should see voltage flow…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you need to be careful about current for a starter, each LED at full brightness is 60mA (3 LEDs per pixel at 20mA each), running from a 5V supply

    1000 LEDs  = 1000x0.06 = 60 Amps

    using 12V and 3 LEDs in series will reduce it by 1/3 so you're still looking at about 20Amps. you would have to feed power to the strips every so often so the current draw does not diminish the voltage too much along the strip

     

    The timing requirements I think may also limit you to 1024 devices in series, technically this may mean 3000 LED's if there the 12V strips with 3 in series per chip

     

    i would suggest you simply use a separate data line for each 500 or so LEDs to keep the single strip current down and the refresh rate up

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you need to be careful about current for a starter, each LED at full brightness is 60mA (3 LEDs per pixel at 20mA each), running from a 5V supply

    1000 LEDs  = 1000x0.06 = 60 Amps

    using 12V and 3 LEDs in series will reduce it by 1/3 so you're still looking at about 20Amps. you would have to feed power to the strips every so often so the current draw does not diminish the voltage too much along the strip

     

    The timing requirements I think may also limit you to 1024 devices in series, technically this may mean 3000 LED's if there the 12V strips with 3 in series per chip

     

    i would suggest you simply use a separate data line for each 500 or so LEDs to keep the single strip current down and the refresh rate up

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer