Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help Using WS2811 to drive 12v RGB LED strip
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 41 replies
  • Answers 11 answers
  • Subscribers 345 subscribers
  • Views 12951 views
  • Users 0 members are here
  • driver
  • mosfet
  • strip
  • led
  • ws2811
  • rgb
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help Using WS2811 to drive 12v RGB LED strip

dmilton2004
dmilton2004 over 11 years ago

Greetings all,

 

I am creating a lighting project that I want to have a wall display with large (15" x 20") panels and each panel acts as its own "pixel" (controlled by one WS2811).

 

I had purchased 12v RGB LED strips with 30 LEDs per meter. What I want do is control a section of the RGB strip (about 15 LEDs). I have been scouring the web for possible solutions. One avenue I was looking at was using MOSFETs to drive the strip from the PWM outputs from the WS2811. There is an example in the WS2811 datasheet that shows using 3 LEDs per color with 12v. I do know that the WS2811 is a constant current source device. My thought was to use a logic level N-channel MOSFET to drive the LED strip. This is just based upon the research that I have done. What I have not found was any schematic to go from. I am looking at possible 3 MOSFETs per WS2811.

 

Any help and schematics would greatly help!

 

Thanks in advance!

 

Don

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +3 suggested
    I was able to make this work by using a simple NOT gate between the WS2811 chip and the mosfet. I believe this works because it is using TTL (transistor based logic). The WS2811 requires some kind of load…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to michaelkellett +2
    More LEDS in series means less current, thinner wires and a single switch, so 12V = 3-4 LEDS per channel, using a chip like ULN2003 will provide all the drive for a single board probably Using logic levels…
  • dmilton2004
    dmilton2004 over 11 years ago in reply to dragonstyne +2 suggested
    Thanks Steve. I have not tried to trigger the MOSFETs yet, but that was my next plan. I should be able to do that by applying +5v to the Gate and connecting the Source to GND. I should see voltage flow…
Parents
  • dragonstyne
    0 dragonstyne over 11 years ago

    The WS2811 is a specialized RGB driver. If you want individual controllable RGB pixels in a multi circuit array, no matter what size (limited by the current capability), this is the device for you.

     

    If you look at the data sheet on Adafruit's site, you see this is not a just a constant current LED driver.  You don't feed it with PWM. You feed it with data and it provides the PWM to the LED's to give you the color and intensity you command.


    If you wanted to build your own jumbotron TV, albeit expensive,  this would be a good choice. I use devices such as this in my lighting for holidays.


    I do agree with Peter and Shabaz, there are more efficient and easier ways to drive LED's if that's what you are trying to do.


    -Steve

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dragonstyne

    Hi Steve,

     

    I'm about to make a big order of these and would like to drive >1000 with a single data stream. Do you think I would run into issues with this?

     

    I suppose I could buy a couple thousand and do some stress tests, but asking seems less expensive.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago in reply to e14 Contributor

    Have you checked out the awesome project by COMPACT A Very Compact Christmas Display - Presentation Video

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 10 years ago in reply to e14 Contributor

    Have you checked out the awesome project by COMPACT A Very Compact Christmas Display - Presentation Video