Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Un-grounded protection design
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 341 subscribers
  • Views 1204 views
  • Users 0 members are here
  • surge_protection
  • israel
  • newbie
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Un-grounded protection design

btfarmer94
btfarmer94 over 11 years ago

Hello,

I am currently working on a project where I need to design a simple and effective protection circuit to prevent from voltage spikes and current surges into our product, as well as brown-outs. This particular product will be used overseas where the power plugs are not grounded. My first question is: will a varistor work without a ground if I connect it between line and neutral on 230v @ 50Hz power? My next question is, can anyone provide me with some resources or advice on this type of circuit design? I am studying engineering at school, but have little electrical experience so far and am just starting my career. Thank you all for your assistance!

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 11 years ago in reply to btfarmer94 +1
    Perhaps a transformer and relay could act as a brown out shut off. Once the voltage drops below a certain level then the relay would drop out. You'd need to match your transformer and relay well (or perhaps…
  • gdstew
    gdstew over 11 years ago in reply to Workshopshed +1
    Another solution is what is called a line stabilizer. Basically it is a 1 to 1 isolation transformer that also senses when the line voltage drops below certain thresholds and uses a relays to kick windings…
Parents
  • btfarmer94
    0 btfarmer94 over 11 years ago

    Thank you all for the advice!

     

    I should specify further. In short, we are controlling a Universal 2-stage Motor at one speed (full power) and a smaller universal motor, again at only 1 speed.  Our testing showed insufficient power damaged these motors. Will the 1:1 isolation transformer still be a suitable solution? This product will be running on 240v @ 50Hz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to btfarmer94

    An isolation transformer is different from a line conditioner/stabilizer in that they do not adjust the output voltage, they simply use a transformer to isolate the AC input

    from the AC output and this will not stop a brownout. A line conditioner/stabilizer made for 240v @ 50Hz (they should be available) may help as long as the motors can

    handle a brief (~ 1/2 to 1 cycle) voltage drop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 11 years ago in reply to btfarmer94

    An isolation transformer is different from a line conditioner/stabilizer in that they do not adjust the output voltage, they simply use a transformer to isolate the AC input

    from the AC output and this will not stop a brownout. A line conditioner/stabilizer made for 240v @ 50Hz (they should be available) may help as long as the motors can

    handle a brief (~ 1/2 to 1 cycle) voltage drop.