Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need suggestions for a good soldering iron
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 316 subscribers
  • Views 5421 views
  • Users 0 members are here
  • pcb soldering
  • soldering tips
  • soldering
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need suggestions for a good soldering iron

rsjawale24
rsjawale24 over 4 years ago

I'm looking to buy a good soldering iron preferably with a fine needle tip that can last long. Power - 25W-35 W

 

I checked online and there are two types of irons available - Ceramic heater and coil heater type.

 

I use this one from Soldron (A popular brand in India) but the tips don't last longer esp. if you keep the iron on for longer times. The entire soldering bit starts to give off flakes (some kind of coating comes off).

The only plus point is that the tips are easy to replace and not very expensive.

imageimage

I found another one from Stanley the tip is tightened using a screw on the side. Probably uses a different heating element too as compared to the above one.

image

Please suggest good soldering irons to buy (brand, models, etc) which can last longer with power rating of 25W to 35 W. Also, which heating element is better? Coil type or ceramic type?

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 4 years ago +6
    I am not an expert in soldering irons but what I have noticed over the years is that the tips are very damaged if you do not have temperature regulation and some function for the soldering iron to detect…
  • shabaz
    shabaz over 4 years ago +4
    Hi Rushiraj, I think both could be ok for general through-hole work if nothing else is available, but both look pretty bad for surface-mount. This is just from general experience from similar-looking tools…
  • shabaz
    shabaz over 4 years ago in reply to rsjawale24 +3
    Hi Rushiraj, There's a Multicomp soldering station but is just slightly higher than your budget (it is ~ 100 USD). Personally with $70 budget, I think I would try to buy a used soldering station, but that…
Parents
  • hugohu
    hugohu over 4 years ago

    I have a 30 dollar Atten iron from adafruit, it has temp control and uses standard 900-M-T tips. I used to have a weller SP25 which had (more) expensive tips and was prone to oxidation(it literally wouldn't tin, not with lead or lead free) but my atten is really nice, i bought 12 tips for 5 dollars and only 2 have oxidized and that's because I didn't tin them properly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hugohu
    hugohu over 4 years ago

    I have a 30 dollar Atten iron from adafruit, it has temp control and uses standard 900-M-T tips. I used to have a weller SP25 which had (more) expensive tips and was prone to oxidation(it literally wouldn't tin, not with lead or lead free) but my atten is really nice, i bought 12 tips for 5 dollars and only 2 have oxidized and that's because I didn't tin them properly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to hugohu

    hugohu  wrote:

    I used to have a weller SP25 which had (more) expensive tips and was prone to oxidation(it literally wouldn't tin, not with lead or lead free) ...

    The tips for the SP25 are plated and shouldn't oxidise fast. They aren't special, but they are decent.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hugohu
    hugohu over 4 years ago in reply to Jan Cumps

    They are electroplated, certainly. I didn't tin the tips that came originally correctly, but my official replacement tips failed to tin with any solder i had, yet it was easily tinned with the 900m-t tips(from PCBway bazaar, one that came with atten, and a mechanic tip) with my cheapest solder, as well as the "better" ones.