Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need suggestions for a good soldering iron
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 316 subscribers
  • Views 5444 views
  • Users 0 members are here
  • pcb soldering
  • soldering tips
  • soldering
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need suggestions for a good soldering iron

rsjawale24
rsjawale24 over 4 years ago

I'm looking to buy a good soldering iron preferably with a fine needle tip that can last long. Power - 25W-35 W

 

I checked online and there are two types of irons available - Ceramic heater and coil heater type.

 

I use this one from Soldron (A popular brand in India) but the tips don't last longer esp. if you keep the iron on for longer times. The entire soldering bit starts to give off flakes (some kind of coating comes off).

The only plus point is that the tips are easy to replace and not very expensive.

imageimage

I found another one from Stanley the tip is tightened using a screw on the side. Probably uses a different heating element too as compared to the above one.

image

Please suggest good soldering irons to buy (brand, models, etc) which can last longer with power rating of 25W to 35 W. Also, which heating element is better? Coil type or ceramic type?

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 4 years ago +6
    I am not an expert in soldering irons but what I have noticed over the years is that the tips are very damaged if you do not have temperature regulation and some function for the soldering iron to detect…
  • shabaz
    shabaz over 4 years ago +4
    Hi Rushiraj, I think both could be ok for general through-hole work if nothing else is available, but both look pretty bad for surface-mount. This is just from general experience from similar-looking tools…
  • shabaz
    shabaz over 4 years ago in reply to rsjawale24 +3
    Hi Rushiraj, There's a Multicomp soldering station but is just slightly higher than your budget (it is ~ 100 USD). Personally with $70 budget, I think I would try to buy a used soldering station, but that…
Parents
  • colporteur
    colporteur over 4 years ago

    I would encourage you to check out the following soldering stations RoadTest reviews.

    METCAL GT120-HP-T6 Soldering Station

    Weller Soldering Station WT Series

    I think it can provide you with some useful information in making a purchase decision.

    To avoid self-promotion use the links provided and you can examine each review using the Recent Reviews links on the right-hand side.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 4 years ago

    I would encourage you to check out the following soldering stations RoadTest reviews.

    METCAL GT120-HP-T6 Soldering Station

    Weller Soldering Station WT Series

    I think it can provide you with some useful information in making a purchase decision.

    To avoid self-promotion use the links provided and you can examine each review using the Recent Reviews links on the right-hand side.

    • Cancel
    • Vote Up +3 Vote Down