Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum For FET-sake, I keep switching and cannot find a suitable MOSFET (or BJT)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 33 replies
  • Answers 12 answers
  • Subscribers 338 subscribers
  • Views 10972 views
  • Users 0 members are here
  • mosfet relay
  • transistor switch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

For FET-sake, I keep switching and cannot find a suitable MOSFET (or BJT)

BigG
BigG over 5 years ago

I came across this lovely term on Twitter the other day for tablet and laptop battery packs that had seen better days (usually when continuously powered/charged). It's #spicy pillow. LOL.

 

https://twitter.com/hashtag/spicypillow?lang=en

 

Anyway, this reminded me of a little project I had in mind (as shown in schema below).

 

image

As a electronics novice, this appears to be a borderline case as I know that transistors tend to work well for mA switches while MOSFETs tend to be targeted at higher voltages (and say +3A current).

 

So now struggling to choose a suitable component - I'm particularly interested at the 1.5A option as that tends to be the limit for many usb charger adapters:

 

image

 

Having done some prelim research it looks like FET's are the way to go but when working through my design criteria I'm quickly getting bogged down in the detail... In this case I'm not coming up with options as I can see that I need to minimise my resistance losses to reduce voltage drop etc... I'm also looking for a low cost <1$ SMD option.

 

Hence I thought to open this little design challenge to the members as I had to chuckle at aGough Lui status update I found when doing my e14 search...

 

Often we're lazy, choosing to use the same parts over and over. I'm guilty of this when it comes to...

 

 

So, any old favourite FETs you have which could well work here?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago +7 suggested
    Don't have favourites. Always use a part for a reason (usually many reasons). Having a reel of 999 of a part is a good reason if it will work OK ! In your case with 3.3V drive, 5V power supply, a load…
  • colporteur
    colporteur over 5 years ago +3 suggested
    Absolutely loved the title of your post! You have to start writing for British tabloids. I missed the meaning of the hashtag. I have little exposure to the sun or social media from under the bridge I only…
  • BigG
    BigG over 5 years ago in reply to colporteur +3 suggested
    LOL. (British tabloids) I missed the meaning of the hashtag. Batteries look like pillows. As to where "spicy" came from, who knows, so I had to look it up (thanks Google) https://www.urbandictionary.com…
Parents
  • BigG
    0 BigG over 5 years ago

    All thanks to https://oshpark.com/, it cost me about $10 to get 3 boards made up and delivered using their express service. Very impressed.

     

    image

     

    As you can see from the above schematic, the board is designed to be attached to a Nordic Semiconductor nRF52840 dongle - these are great low cost dev boards that can be slotted directly into a USB port. The MOSFET I decided to use was partly based on the fact that it was in stock and is low cost.

     

    https://www.vishay.com/docs/63302/si2342ds.pdf

     

    It works - I verified manually.

     

    Now I'm able to control the power to any device attached, using BLE to remotely switch power on and off. Well that's the theory. Now I just need to get my nRF52840 firmware sorted. Fingers crossed.

     

     

    {gallery:autoplay=false} USBLE Spicy Controller Board

    image

    The underside of my USBLE spicy controller board

    image

    My USBLE Spicy Controller attached to an nRF52840 dongle

    image

    nRF52840 USB dongle inserted into laptop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to BigG

    Hi Colin,

     

    Nice project! One thing you might (or might not) need (can be easily hacked in place hopefully, perhaps with surface mount resistors, is a resistance between the data pins, because the tablet/end device might not draw too much current without it - It's called Dedicated Charging Port (or other options are possible), I don't know the precise details but they should be published, there's some brief information here: SILICON LABS USB-TO-UART Bridge Controller EVM - Review

    (in the 'Battery Charging Negotiation' section)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 5 years ago in reply to shabaz

    Yes, I wondered about that. Thankfully it works with my old Android tablets - see video demo.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    I have a new Android phone, which uses USB C. I suspect that with this phone I'll need to make a few mods. In particular I'd need a better MOSFET as with fast charge you can draw over 2 Amps. Not sure what else will be needed for USB-C regarding data lines. Needs further research.

     

     

     

    EDIT... ah! I see what you mean.

     

    I've just done some further testing and whilst it (sort of) works I can see that the current draw does differ depending on device and whether it is charged by laptop or otherwise.

     

    TEST 1: Charging tablet (Amazon FIRE 7) directly from laptop. Here the current draw is less than shown in the video demo.

    image

     

    TEST 2: Charging tablet directly from a USB charger. Here the current draw is higher.

     

    image

     

    TEST 3: Attaching the USBLE Spicy Controller to USB charger. Here the current draw is less and is similar to the current draw when charging directly from a laptop.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to BigG

    Hi Colin,

     

    I'm in the same situation, many devices with USB-C, so I ordered some connectors - they arrived today - so that I can in future lay out boards with that rather than (in my case for USB peripheral) Micro-USB. From what I read, since the connector works in both orientations, the data pins are replicated so they need to be connected together, and then there is a pin called CC, again replicated, and each of those separately needs to be connected via a resistor, to 0V or to the supply. The computer end (host) connects it high, and the peripheral end (device) connects it low. The diagram below was from a Cypress document but I found it hard to follow so I put some colour-coded annotations on it below.

     

    image

     

    Personally I went with this USB-C connectorthis USB-C connector which is through-hole (I preferred SMD but I didn't see one that looked easy to solder). The through-hole won't be particularly easy to solder either, since the pins are extremely close, but that's life - I've bought enough to last me a while! so I have to go with what I have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to shabaz

    Hi Shabaz,

    That does look like it could be difficult to solder. Some of the less expensive PCB manufacturers may not be able to put solder mask between the pads. I would be interested in your experience as this is something I would like to try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 5 years ago in reply to BigG

    The nRF52840 dongle has test points for the USB data pins, so I decided to use those to allow for pass through by hooking those up to the data pins of the USB-A receptacle connector.

     

    image

     

    image

     

    Whilst it does not give identical results in terms of current draw (with USBLE spicy controller vs without), the hack does appear to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 5 years ago in reply to BigG

    Indeed, it should work just fine with USB-C at least in its USB-A compatible modes by using a regular A-to-C lead.

     

    The resistance values on the CC lines using a USB-A to USB-C cable are usually configured to tell the end device to "fall-back" to other methods of detecting available charge current. Regardless, the connectors themselves shouldn't be used above 3A anyway, most USB-A devices never exceed 2.4A in the best ideal situations. However, in most cases, because of the USB-BCS rules, devices will fold-back their current if they detect the charger is being overloaded - this is done by watching the voltage. This is mainly so that if someone plugs a new phone into an old USB 0.5A charger for example, it doesn't trip the OCP. This fold-back usually works very well, resulting in slower-than-normal charging on long leads, thin leads and/or worn connectors.

     

    I'd probably be more concerned that the Nordic board doesn't have a "proper" USB connector, as the PCB-pad connections do not have the raised ridged profile of proper USB pins and the contact pressure may not be optimal. Drawing so much current this way could lead to "intermittent" resistance changes which may mean downstream devices fold-back and charge a bit slower. Of note is that USB meters also will add additional resistance due to the connectors and sensing shunts - sometimes a small wiggle of the connection and you can see the fold-back in action.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 5 years ago in reply to BigG

    Indeed, it should work just fine with USB-C at least in its USB-A compatible modes by using a regular A-to-C lead.

     

    The resistance values on the CC lines using a USB-A to USB-C cable are usually configured to tell the end device to "fall-back" to other methods of detecting available charge current. Regardless, the connectors themselves shouldn't be used above 3A anyway, most USB-A devices never exceed 2.4A in the best ideal situations. However, in most cases, because of the USB-BCS rules, devices will fold-back their current if they detect the charger is being overloaded - this is done by watching the voltage. This is mainly so that if someone plugs a new phone into an old USB 0.5A charger for example, it doesn't trip the OCP. This fold-back usually works very well, resulting in slower-than-normal charging on long leads, thin leads and/or worn connectors.

     

    I'd probably be more concerned that the Nordic board doesn't have a "proper" USB connector, as the PCB-pad connections do not have the raised ridged profile of proper USB pins and the contact pressure may not be optimal. Drawing so much current this way could lead to "intermittent" resistance changes which may mean downstream devices fold-back and charge a bit slower. Of note is that USB meters also will add additional resistance due to the connectors and sensing shunts - sometimes a small wiggle of the connection and you can see the fold-back in action.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • BigG
    0 BigG over 5 years ago in reply to Gough Lui

    I'd probably be more concerned that the Nordic board doesn't have a "proper" USB connector, as the PCB-pad connections do not have the raised ridged profile of proper USB pins and the contact pressure may not be optimal. Drawing so much current this way could lead to "intermittent" resistance changes which may mean downstream devices fold-back and charge a bit slower.

     

    Yes I have that concern too. As such, I designed the USBLE board to offer some sort of cantilevered type support with the back of the board resting against the side of the charger. I was also thinking of adding some solder on the ends of the outer outer pads to provide a ridge.

     

    In the meantime I'm doing some more testing. I created a quick app using MIT App Inventor for the tablet to update google sheets with battery data... I've started with the standard direct charge method. Then I will wait for battery to discharge and then I will introduce my USBLE device and measure the battery charging data again to learn about difference in charging rates.