Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the advantage of having LET-M connectivity over internet connectivity?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 314 subscribers
  • Views 1573 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the advantage of having LET-M connectivity over internet connectivity?

embeddedguy
embeddedguy over 4 years ago

Hi community,

I have the question while reading about the LTE-M solutions and development kits in the market and normal internet connectivity which one can do on boards such as ESP32 etc.

What is the essential difference between these two? My idea is that LTE-M is that it connects to the service provider and can support the datarate of upto ~2-MBPS. A SIM card and LTE-M module is required for these.

In case of internet and clound connectivity only internet is most needed while it also somehow connects to the network of  a service provide like Vodaphone, Airtel etc. But on the other hand it provides high data rates.

Can someone point me some online resorce to differentiate? talking some key points of each technology?

  • Sign in to reply
  • Cancel

Top Replies

  • navadeepganeshu
    navadeepganeshu over 4 years ago +4
    Hi, you're right about this intuition. LTE modules have 4G connectivity(nothing different than a 4G link in smartphones) and connect to a network via a service provider using SIM card. You can do call…
  • embeddedguy
    embeddedguy over 4 years ago +2
    Thanks, Navadeep for the clerification, I will find time to read through the document...
Parents
  • navadeepganeshu
    0 navadeepganeshu over 4 years ago

    Hi, you're right about this intuition. 

    LTE modules have 4G connectivity(nothing different than a 4G link in smartphones) and connect to a network via a service provider using SIM card. You can do call-dial up + internet + SMS stuff in this. These modules come with a variety of interfaces -- one common of them is UART and using MCU interface, with AT commands(used for MODEMS and networking stuff), its functionality can be controlled. 

    One example which I recently used in one of the IoT design is this SIM7600 module. The advantage with these are that it can be used in systems which are to be deployed in remote locations(unlike WiFi where you need wired internet link to the system and wireless range is limited). GSM, 3G modules are older versions of these. 

    A quick resource here: LTE vs WIFI | Top Most Comapriosn Between LTE vs WIFI (Inofgraphics) (educba.com)

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • navadeepganeshu
    0 navadeepganeshu over 4 years ago

    Hi, you're right about this intuition. 

    LTE modules have 4G connectivity(nothing different than a 4G link in smartphones) and connect to a network via a service provider using SIM card. You can do call-dial up + internet + SMS stuff in this. These modules come with a variety of interfaces -- one common of them is UART and using MCU interface, with AT commands(used for MODEMS and networking stuff), its functionality can be controlled. 

    One example which I recently used in one of the IoT design is this SIM7600 module. The advantage with these are that it can be used in systems which are to be deployed in remote locations(unlike WiFi where you need wired internet link to the system and wireless range is limited). GSM, 3G modules are older versions of these. 

    A quick resource here: LTE vs WIFI | Top Most Comapriosn Between LTE vs WIFI (Inofgraphics) (educba.com)

    • Cancel
    • Vote Up +4 Vote Down