Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Triac 0-10V control
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 304 subscribers
  • Views 3608 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Triac 0-10V control

Pips
Pips over 3 years ago

Hello,

The goal is to control thru a triac a low power 24VAC load, by a 0-10VDC setpoint

Generating a synchronizied ramp and zero crossing detection, comparating and firing the triac is well known.

BUT : is somebody knowing an IC to do that (the goal is space saving) ?

Thank you for your ideas

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +2 verified
    https://www.banggood.com/One-way-Solid-State-Relay-Module-p-979853.html?cur_warehouse=CN https://www.banggood.com/Two-way-Solid-State-Relay-Module-p-979855.html?cur_warehouse=CN https://www.banggood…
  • kkazem
    kkazem over 3 years ago +2
    There are numerous ICs for controlling triacs, typically divided into Zero-crosssing vs non-zero crossing types. Do a Google search for triac control IC.
  • colporteur
    colporteur over 3 years ago in reply to Pips +1
    The terms used added some confusion. You are looking to regulate the AC voltage using a triac? There is a difference between regulate and control. Maybe provide some description of the goal of…
Parents
  • dougw
    0 dougw over 3 years ago

    The application isn't clear to me but here is a way to save space on a duty cycle controller....it doesn't even need a separate power supply.

    https://www.eeworldonline.com/simplifying-solid-state-lighting-control/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Pips
    0 Pips over 3 years ago in reply to dougw

    Hello Doug,

    The application is not the matter, but if you are interested let's explain it :

    80 lamps lighting the audience in a theater.

    The original (35 years old) system was controlled by 4 buttons on several control panels : 100%, 40%, 0%, stop ... value changing from on to another following a ramp. This old system sent the reference to the dimmers as 0-10Vdc.

    I build a new system (8051 based)  keeping these buttons functions, but permetting to switch to Dmx control from the light desk.

    The new system include both set-point outputs : 0-10Vdc and Dmx, to be compatible with various dimmers. Everything works perfectly.

    It include also a curve correction thru a table in the processor.

    And now I want that the light intensity of the 100% button follow the hall intensity. And the bulding wiring is pretty messy. The control power for everything (buttons, relays, contactors, button's lamps,...) is 24Vac, with the 0/24Vac grounded ! That's why I choose to keep the control of this lamp by a regulated 24Vac as it was ...

     Thank for your help. The schematic you mentionned is harware controlled, I need to control via an analog set-point. Integrated !

    Best regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Pips
    0 Pips over 3 years ago in reply to dougw

    Hello Doug,

    The application is not the matter, but if you are interested let's explain it :

    80 lamps lighting the audience in a theater.

    The original (35 years old) system was controlled by 4 buttons on several control panels : 100%, 40%, 0%, stop ... value changing from on to another following a ramp. This old system sent the reference to the dimmers as 0-10Vdc.

    I build a new system (8051 based)  keeping these buttons functions, but permetting to switch to Dmx control from the light desk.

    The new system include both set-point outputs : 0-10Vdc and Dmx, to be compatible with various dimmers. Everything works perfectly.

    It include also a curve correction thru a table in the processor.

    And now I want that the light intensity of the 100% button follow the hall intensity. And the bulding wiring is pretty messy. The control power for everything (buttons, relays, contactors, button's lamps,...) is 24Vac, with the 0/24Vac grounded ! That's why I choose to keep the control of this lamp by a regulated 24Vac as it was ...

     Thank for your help. The schematic you mentionned is harware controlled, I need to control via an analog set-point. Integrated !

    Best regards