Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Rise time measurements counter/timer vs Oscope?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 303 subscribers
  • Views 2538 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Rise time measurements counter/timer vs Oscope?

dc2daylight
dc2daylight over 3 years ago

Hi,

I am trying to measure the rise time of a 10 MHz square wave with a Keysight 53220A universal counter.  The source has a specified rise time at 10 MHz of <3 nS.  This is confirmed to be about 3 nS when measured on a scope.

However, when measured on the counter I am seeing a rise time of around 40 nS (10-90%).

I suspect that either I am not measuring the same thing or I may be setting up the measurement incorrectly on the counter.  (the user manual has very little on this).

Any help or suggestions would be appreciated.

Thanks,

Mark

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +3
    The 53220A isn't a time-stamping or zero-dead-time counter. So there is a minimum delay needed between start and stop triggers on time interval measurements. The rise time of a fast edge wouldn't satisfy…
  • Jan Cumps
    Jan Cumps over 3 years ago +2
    Is the 10/90% on the counter rise time or duty cycle? A sking because the UOM is %, and that's more common for the duty cycle. 2nd check: input impedance of scope vs counter. Are they both 50 Ohm, both…
  • dc2daylight
    dc2daylight over 3 years ago in reply to Jan Cumps +1
    Ok, yes, It's a time interval parameter, not a duty cycle. My understanding is the 10-90% is the time interval it takes the signal to go from 10% to it's final value of 90% of it's final value. It…
  • Jan Cumps
    0 Jan Cumps over 3 years ago

    Is the 10/90% on the counter rise time or duty cycle?A sking because the UOM is %, and that's more common for the duty cycle.

    2nd check: input impedance of scope vs counter. Are they both 50 Ohm, both high impedance, or is one different from the other?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dc2daylight
    0 dc2daylight over 3 years ago in reply to Jan Cumps

    Ok, yes, It's a time interval parameter, not a duty cycle.

    My understanding is the 10-90% is the time interval it takes the signal to go from 10% to it's final value of 90% of it's final value.

    It is an adjustable parameter but I thing the 10/90 is most commonly used.

    Using 50 ohms input impedance on both.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to dc2daylight
    dc2daylight said:
    I thing the 10/90 is most commonly used

    Yes, you are correct.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago

    I didn't think counters measured rise-time. At least mine doesn't but then mine isn't the same instrument. It's unusual (or maybe it is a very modern counter?). 

    Normally a 'scope is used for this as far as I'm aware - there may be specialized equipment in some industries perhaps, but the general instrument would be the 'scope. And the 'scope should be set to 50 ohm usually, as Jan says (at least most signal generators would expect the load to be 50 ohm).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to shabaz

    This one has the rise time functionality. It's a rather advanced (and expensive) instrument.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 3 years ago

    The 53220A isn't a time-stamping or zero-dead-time counter. So there is a minimum delay needed between start and stop triggers on time interval measurements. The rise time of a fast edge wouldn't satisfy the setup time needed by the counter. 

     

    Is the source clock 50% duty cycle? Perhaps the counter is triggering on the next edge (if the source was 40% duty cycle)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Jan Cumps

    Interesting, nice feature. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago

    I suppose one other thing to rule in or out, could be, has it ever worked, or is it in some lab and no-one knows if it works. I only say this because people do end up damaging anything RF related, I've seen several destroyed spectrum analyzers, and my counter came destroyed too, fortunately, that was an easy fix. I think people like plugging in transmitters.

    If there's another way to verify it works (on all channels if it is a multi-channel instrument, or run diagnostics) could be good to confirm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dc2daylight
    0 dc2daylight over 3 years ago in reply to scottiebabe

    Thanks for the response.  I think your on to something there.  I am still finding my way around all the settings on this unit. 

    Yes, the duty cycle is set at 50%. Gate and trigger settings have many options including time and delay settings. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to dc2daylight

    A different path could be to ask the question on EEVBlog: https://www.eevblog.com/forum/testgear/.
    There is always someone who has exactly the same instrument as you. It's where the instrument addicts hang out :).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>