Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Op Amps in Flight Sim
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 313 subscribers
  • Views 3048 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Op Amps in Flight Sim

EAL727Capt
EAL727Capt over 3 years ago

Good day to all.

Long time lurker and first posting; I truly appreciate your patience.

I have been working on constructing a home cockpit representing a Boeing 727-200 using OEM parts/instruments/indicators/gauges I’ve obtained over the years.

Currently, I’m hard-at-work on interfacing these pieces with X-Plane 11.   I have many, many questions and as a relative newcomer to the world of electronics (which is like learning a new foreign language to me most times) I would appreciate some assistance.

I’m working on a Flight Director Indicator (FDI) and a Horizontal Situation Indicator (HSI) which both provide vertical and horizontal guidance to the pilots.  Luckily, I have the pin out assignments and operation manual for the FDI and am having fun hooking-up wires and seeing the dials slowly turn.  The pitch and roll functions are controlled by synchros and motor-generators via 26VAC/400Hz.  The warning flags are powered by 28VDC.

On the topic of op amps—-

There is a ‘needle’ indicator for the glide slope (which provides a ‘path’ to follow when approaching the runway to land).  This needle indicator is biased from view when the glide slope receiver does not detect a glide slope indication.  When approaching the runway and intercepting the glide slope at a specific altitude, the needle will move slowly move down from its hidden view.  When the needle reaches its centered position, you are on the glide slope and continuously descend to the runway, keeping this needle centered.  
This needle requires very little power, both positive and negative.  Full deflection in either direction (above glide path and below glide path)  is minimal; this indicator is extremely sensitive as it is designed to guide the pilot to the runway in very low visibility conditions—precision is paramount.

Given this, an op amp (based upon the reading and research I’ve done) seems the logical choice for operation.  I have been successful in getting the needle to move from full up to full down by switching the leads for positive and negative power, using extremely low amps from my 28VDC bench power supply.  

From the unit’s manual:

”Meter mechanism sensitivity is 150 +/-20 ua in each direction and is biased from view with 1.5 ma maximum and is in view with 500 ua applied.  Meter resistance is 1000 +/- 30 ohms.”

I will be using a Teensy board which provides power of 3.3VDC with PWM.  I’m not concerned with the coding/sketch to drive this instrument as that has already been established.  

How would I apply Ohm’s Law to drive this needle using various values of resistors/diodes or other components, given the tiny amount of amperage (positive and negative) required?  And then the question of which type of op amp to purchase?  I have done some research on the topic of op amps and am still a little unclear to their full capabilities and/or limitations.   I had seen an op amp board available from SparkFun which looked promising but I wanted to first ask as I see many, many friendly, patient and helpful suggestions and advice here.

I certainly appreciate your input.

Jay

Las Vegas, NV

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to EAL727Capt +4
    Hello, you're quite welcome :) The component values were just a rough guess, I choose 100 ohm resistors assuming you wanted to drive upto +- 1.5 mA through the meter movement. You can always use a larger…
  • scottiebabe
    scottiebabe over 3 years ago +2
    Here is a very simple implementation to get you started: Really neat project, btw!
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe +2
    Just wondering, it may be possible to remove the RC filter, although it depends on the movement. On my limited test on a 100 uA movement ( see here: /products/roadtest/rv/roadtest_reviews/509/sensirion_gastemphum…
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    The spec you have given doesn't quite make sense to me.

    On the one hand it says the sensitivty is 150uA, then says you should apply 500uA to keep it in view and 1500uA to bias out of view.

    Its 1000R (ohms) so you get 1000uA per volt.

    If you put a 9000 (use 9100R = 9.1k)  resistor in series with the meter then you will get 500uA for about 5V applied.

    (because the total resistance will be 10000R so you'll get V/10000 * 1000,000 uA)

    Then, if you can tell us where the needle is for currents from 0 to 1500uA going up in 100uA steps.

    I think you may not need an op amp at all - just a resistor and capacitor but there isn't quite enough data to be sure.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to michaelkellett

    I understood that to be 1500uA maximum.  I.e. apply 501uA to 1500uA to keep it out of view, but no more than that.  That implied to me it functionally operates across a range of 0A to 500uA for the purposes of deflecting the needle.  I think you are interpreting it as functionally operating between 500uA and 1500uA which I can also see now you say it!  That 1.5mA max in the manual would seem to indicate it could breakdown above 1.5mA and would go out of view at a value below 1.5mA, but above 500uA.

    There's also mention of positive and negative power - does it run with a positive and negative power rail?  It may well be the case that it operates in view from -500uA to +500uA (climb or descend).  Jay's experiment with his power supply could support this but it wasn't a nuanced enough experiment to be sure.

    Confusing???  Jay: do you have more info to add from your experiments/investigation?

    Given the use of a 3.3V Teensy, an alternative combination would be a 5600 Ohm resistor: 3.3/(5600 + 1000) = 500uA.  It could then still be characterised in steps of 100uA.  I don't suppose it matters, but it may help depending upon parts to hand.

    It would still be useful to understand the operating range though.

    phoenixcomm just in case you miss this post, I daresay you have good experience to add here.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago in reply to michaelkellett

    I understood that to be 1500uA maximum.  I.e. apply 501uA to 1500uA to keep it out of view, but no more than that.  That implied to me it functionally operates across a range of 0A to 500uA for the purposes of deflecting the needle.  I think you are interpreting it as functionally operating between 500uA and 1500uA which I can also see now you say it!  That 1.5mA max in the manual would seem to indicate it could breakdown above 1.5mA and would go out of view at a value below 1.5mA, but above 500uA.

    There's also mention of positive and negative power - does it run with a positive and negative power rail?  It may well be the case that it operates in view from -500uA to +500uA (climb or descend).  Jay's experiment with his power supply could support this but it wasn't a nuanced enough experiment to be sure.

    Confusing???  Jay: do you have more info to add from your experiments/investigation?

    Given the use of a 3.3V Teensy, an alternative combination would be a 5600 Ohm resistor: 3.3/(5600 + 1000) = 500uA.  It could then still be characterised in steps of 100uA.  I don't suppose it matters, but it may help depending upon parts to hand.

    It would still be useful to understand the operating range though.

    phoenixcomm just in case you miss this post, I daresay you have good experience to add here.