Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Op Amps in Flight Sim
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 315 subscribers
  • Views 3152 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Op Amps in Flight Sim

EAL727Capt
EAL727Capt over 3 years ago

Good day to all.

Long time lurker and first posting; I truly appreciate your patience.

I have been working on constructing a home cockpit representing a Boeing 727-200 using OEM parts/instruments/indicators/gauges I’ve obtained over the years.

Currently, I’m hard-at-work on interfacing these pieces with X-Plane 11.   I have many, many questions and as a relative newcomer to the world of electronics (which is like learning a new foreign language to me most times) I would appreciate some assistance.

I’m working on a Flight Director Indicator (FDI) and a Horizontal Situation Indicator (HSI) which both provide vertical and horizontal guidance to the pilots.  Luckily, I have the pin out assignments and operation manual for the FDI and am having fun hooking-up wires and seeing the dials slowly turn.  The pitch and roll functions are controlled by synchros and motor-generators via 26VAC/400Hz.  The warning flags are powered by 28VDC.

On the topic of op amps—-

There is a ‘needle’ indicator for the glide slope (which provides a ‘path’ to follow when approaching the runway to land).  This needle indicator is biased from view when the glide slope receiver does not detect a glide slope indication.  When approaching the runway and intercepting the glide slope at a specific altitude, the needle will move slowly move down from its hidden view.  When the needle reaches its centered position, you are on the glide slope and continuously descend to the runway, keeping this needle centered.  
This needle requires very little power, both positive and negative.  Full deflection in either direction (above glide path and below glide path)  is minimal; this indicator is extremely sensitive as it is designed to guide the pilot to the runway in very low visibility conditions—precision is paramount.

Given this, an op amp (based upon the reading and research I’ve done) seems the logical choice for operation.  I have been successful in getting the needle to move from full up to full down by switching the leads for positive and negative power, using extremely low amps from my 28VDC bench power supply.  

From the unit’s manual:

”Meter mechanism sensitivity is 150 +/-20 ua in each direction and is biased from view with 1.5 ma maximum and is in view with 500 ua applied.  Meter resistance is 1000 +/- 30 ohms.”

I will be using a Teensy board which provides power of 3.3VDC with PWM.  I’m not concerned with the coding/sketch to drive this instrument as that has already been established.  

How would I apply Ohm’s Law to drive this needle using various values of resistors/diodes or other components, given the tiny amount of amperage (positive and negative) required?  And then the question of which type of op amp to purchase?  I have done some research on the topic of op amps and am still a little unclear to their full capabilities and/or limitations.   I had seen an op amp board available from SparkFun which looked promising but I wanted to first ask as I see many, many friendly, patient and helpful suggestions and advice here.

I certainly appreciate your input.

Jay

Las Vegas, NV

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to EAL727Capt +4
    Hello, you're quite welcome :) The component values were just a rough guess, I choose 100 ohm resistors assuming you wanted to drive upto +- 1.5 mA through the meter movement. You can always use a larger…
  • scottiebabe
    scottiebabe over 3 years ago +2
    Here is a very simple implementation to get you started: Really neat project, btw!
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe +2
    Just wondering, it may be possible to remove the RC filter, although it depends on the movement. On my limited test on a 100 uA movement ( see here: /products/roadtest/rv/roadtest_reviews/509/sensirion_gastemphum…
Parents
  • EAL727Capt
    EAL727Capt over 3 years ago

    Thank you all for your replies thus far.

    When I connect the positive power lead to the positive pin on the unit and the negative power lead to the negative pin on the unit, needle deflection is up (indicating flying below the glide path).  A centered needle (flying on the glide path) is obtained at zero volts.

    When I reverse the power leads (e.g., Positive power lead to negative pin, negative power lead to positive pin), needle reflection is down (indicating flying above the glide path).  

    The needle will always indicate where the glide slope beam is, in all cases.


    As little as .2V shoots the needle up (or down, depending on the power lead placement on the unit).

    My assumption here is that very, very, very little voltage is required and the precision of the meter/needle movement is controlled by amps and not volts, hence the op amp question applying either positive or negative amperage for accurate movement.

    As soon as I figure out some way to more accurately control positive and negative amperage, I can then learn the readings with an ammeter and post my findings here.  Again, being new to electronics for testing and practical application with these very old and priceless (to me) instruments, this is currently not in my wheel house!   I fly planes…I don’t usually pull ‘em apart!!!     LOL

    Thank you again.

    Jay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to EAL727Capt

    The circuit supplied by scottiebabe will allow your Teensy PWM output to create a positive and negative voltage and current, where a 50% duty cycle on the PWM would be zero reading or "on glide path indication".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago in reply to EAL727Capt

    The circuit supplied by scottiebabe will allow your Teensy PWM output to create a positive and negative voltage and current, where a 50% duty cycle on the PWM would be zero reading or "on glide path indication".