Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Pool boiling experiment
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 317 subscribers
  • Views 4809 views
  • Users 0 members are here
  • resistance
  • pool boiling experiment
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Pool boiling experiment

brunopserrao
brunopserrao over 3 years ago

Dear community,

My research group is developing a pool boiling experiment. It consists basically by a heater (a Stainless Steel wire in our case) placed in a working fluid and a power supply connected to it. In a pool boiling experiment, different bubble regimes are observed depending on the temperature difference between the heater and the working fluid. Our goal is to measure the voltage across the heater in order to calculate the heater resistance and use the temperature x resistance relation to get its temperature.

Our experimental setup consists of a 5000 Watts DC power supply (0-20V and 0-250A) connected to copper wires and then connected to a 316L Stainless Steel wire (this one stays in a water tank).

We have already run this experiment a few times, but we never got a reliable voltage measurement. Our calculated resistance for the heater in general decreases with increasing the power in the power supply, what is not true for two reasons: (1) we can observe the different regimes using a high speed-camera, and (2) increasing power means increasing the heater temperature that means increasing resistance according to the temperature x resistance relation.

In addition, our power supply display is not reliable, so we measure our system current using a clamp digital ammeter. Our voltage across the heater is measured by a 6 1/2 DMM. Can someone help me to understand what we are doing wrong?

Regards,

Bruno

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +1
    The voltage over the heater is the voltage of your power supply - the voltage drop in your copper wires. The more current you send, the more voltage is dropped in the copper leads, and the less voltage…
  • shabaz
    shabaz over 3 years ago +1
    Also, the current measurement may become inaccurate over time* (this is a guess). It might be better to find an alternate way to measure current, e.g. measuring the voltage across the wires, and the voltage…
  • brunopserrao
    brunopserrao over 3 years ago in reply to Jan Cumps +1
    Jan, Thanks for your help. I will be in the lab tomorrow and I can take some pictures of our setup. Basically we have two 8 AWG stranded copper wires connected to the positive and negative sides of the…
Parents
  • shabaz
    shabaz over 3 years ago

    Also, the current measurement may become inaccurate over time* (this is a guess). It might be better to find an alternate way to measure current, e.g. measuring the voltage across the wires, and the voltage across the heating element, if you know the resistance of the wires (and how that will change as they warm up).

    *I'm thinking of drift, since it's DC you're measuring with the clamp meter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • brunopserrao
    brunopserrao over 3 years ago in reply to shabaz

    Shabaz,

    Thanks for the help. I will keep that in mind. We fist tried to use a shunt resistor in our setup in order to measure the current of the system instead of using the clamp ammeter. Then, I decided to take it out of the system. Then you are saying I should put it back and get the system current based on the voltage drop across it, right? Does a shunt resistor have a fixed resistance or not?

    This is our shunt model by the way:

    www.ohmite.com/.../SH2-200R0005DE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to brunopserrao

    Hi,

    Nothing has a fixed resistance, there will be a change with temperature, and that can be caused by the amount of power loss through the material. The 8 AWG wire will have more resistance than your shunt resistor. You'll need to calculate how much power loss there is in the wire, and see if that's sufficient to raise the temperature enough to make a material difference to the resistance or not. Just 1 metre of 8 AWG copper wire will have 2 mOhm of resistance (if I've calculated that correctly) so you can't ignore the voltage across the wire, as Jan mentions. You don't need the shunt resistor if you consider the wire to be a resistor anyway (which it is), so maybe I'm missing something, but I don't see why you're adding the 0.5 mOhm shunt to the circuit if the wire has comparable resistance.

    You could try to use many wires in parallel to reduce the resistance compared to the shunt, but you should still measure across the wires and the shunt, since the wire resistance and connections may still not be insignificant (I don't know). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to brunopserrao

    Shunts are typically used because they have a lower change with temperature than wire - generally assumed to be fixed value. Yours changes no more than 30ppm/C.

    When you say you have bad readings what does that mean? They are fluctuating or just appear to be inaccurate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • brunopserrao
    brunopserrao over 3 years ago in reply to dougw

    Dougw,

    Thanks for your help. In general, when I increase the power, the resistance decreases. I'm wondering if this is happening because somehow the resistance x temperature relation for the stainless steel wire is being affected by the same relation for the system copper wires.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • brunopserrao
    brunopserrao over 3 years ago in reply to dougw

    Also, do you think I should add the shunt back to the system in order to obtain a reliable system current measurement?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to brunopserrao

    It would help if you show the formula you use, and the input values and measurements for that formula. For several measurements in your range.

    We may spot something then?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to brunopserrao

    Think you need to draw a diagram showing precisely where your wires are connected to which test equipment. Your wire resistance is swamping the shunt. Unless you take the wire resistance into account, it's pointless measuring just across a shunt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    Yes, making measurements when there is a very low resistance in play, needs care.
    My suspicion is that stray resistance, in the wires, is the cause. But it 'll stay a guess until Bruno shows the setup, calculations and measurements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to brunopserrao

    Also, the datasheet of the current clamp (if you're still using it) would be helpful. I doubt it will be effective, but worth examining the datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • brunopserrao
    brunopserrao over 3 years ago in reply to brunopserrao

    All,

    You can find the formula here:

    https://www.sciencelaws.in/2020/12/relation-between-resistance-and-temperature.html#:~:text=The%20formula%20of%20relation%20between,of%20the%20conductor%20also%20increases.

    The coefficient I found online for 316L stainless steel was 9.2x10^-4

    http://en.techinfodepot.shoutwiki.com/wiki/Temperature_Coefficient_of_Resistance

    The initial resistance is calculated using the resistivity given by 7,4x10^-5 at 20 degrees Celsius and the wires characteristics (length and cross-sectional area).

    www.matweb.com/.../datasheet_print.aspx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • brunopserrao
    brunopserrao over 3 years ago in reply to brunopserrao

    All,

    You can find the formula here:

    https://www.sciencelaws.in/2020/12/relation-between-resistance-and-temperature.html#:~:text=The%20formula%20of%20relation%20between,of%20the%20conductor%20also%20increases.

    The coefficient I found online for 316L stainless steel was 9.2x10^-4

    http://en.techinfodepot.shoutwiki.com/wiki/Temperature_Coefficient_of_Resistance

    The initial resistance is calculated using the resistivity given by 7,4x10^-5 at 20 degrees Celsius and the wires characteristics (length and cross-sectional area).

    www.matweb.com/.../datasheet_print.aspx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to brunopserrao

    Better to create a little Excel spreadsheet for yourself, with the formulas, and plug in your variables. Otherwise it's just guesswork, like literally how long is a piece of string/wire...

    Needs a diagram too.